Logout Successful! 




*----------------------------------------------------------------------------*
Attention! The IP Address in Programming was recently changed. In order to
re-establish a connection to the panel you must update your Network Settings
on your PC with a new IP Address in the same group. (For example, if your
new IP Address is 123.456.7.8 you must change your PC IP Address to
123.456.7.x where "x" can be any digit except 8).

You will also need to put the new IP Address of the panel in the address bar
of your internet browser. (In the above example you would type the following
into your internet browser: http://123.456.7.8/ and press Enter.)
*----------------------------------------------------------------------------*