#
# Backlight & LCD drivers configuration
#

menuconfig BACKLIGHT_LCD_SUPPORT
	bool "Backlight & LCD device support"
	help
	  Enable this to be able to choose the drivers for controlling the
	  backlight and the LCD panel on some platforms, for example on PDAs.

config BACKLIGHT_CLASS_DEVICE
        tristate "Lowlevel Backlight controls"
	depends on BACKLIGHT_LCD_SUPPORT
	default m
	help
	  This framework adds support for low-level control of the LCD
          backlight. This includes support for brightness and power.

	  To have support for your specific LCD panel you will have to
	  select the proper drivers which depend on this option.

config LCD_CLASS_DEVICE
        tristate "Lowlevel LCD controls"
	depends on BACKLIGHT_LCD_SUPPORT
	default m
	help
	  This framework adds support for low-level control of LCD.
	  Some framebuffer devices connect to platform-specific LCD modules
	  in order to have a platform-specific way to control the flat panel
	  (contrast and applying power to the LCD (not to the backlight!)).

	  To have support for your specific LCD panel you will have to
	  select the proper drivers which depend on this option.

config BACKLIGHT_CORGI
	tristate "Sharp Corgi Backlight Driver (SL Series)"
	depends on BACKLIGHT_CLASS_DEVICE && PXA_SHARPSL
	default y
	help
	  If you have a Sharp Zaurus SL-C7xx, SL-Cxx00 or SL-6000x say y to enable the
	  backlight driver.

config BACKLIGHT_LOCOMO
	tristate "Sharp LOCOMO LCD/Backlight Driver"
	depends on BACKLIGHT_CLASS_DEVICE && SHARP_LOCOMO
	default y
	help
	  If you have a Sharp Zaurus SL-5500 (Collie) or SL-5600 (Poodle) say y to
	  enable the LCD/backlight driver.

config BACKLIGHT_HP680
	tristate "HP Jornada 680 Backlight Driver"
	depends on BACKLIGHT_CLASS_DEVICE && SH_HP6XX
	default y
	help
	  If you have a HP Jornada 680, say y to enable the
	  backlight driver.

config BACKLIGHT_PROGEAR
	tristate "Frontpath ProGear Backlight Driver"
	depends on BACKLIGHT_CLASS_DEVICE && PCI && X86
	default n
	help
	  If you have a Frontpath ProGear say Y to enable the
	  backlight driver.

config BACKLIGHT_CARILLO_RANCH
	tristate "Intel Carillo Ranch Backlight Driver"
	depends on BACKLIGHT_CLASS_DEVICE && LCD_CLASS_DEVICE && PCI && X86 && FB_LE80578
	default n
	help
	  If you have a Intel LE80578 (Carillo Ranch) say Y to enable the
	  backlight driver.

config BACKLIGHT_KB920x
	tristate "KwikByte KB9202 Backlight Driver"
	depends on BACKLIGHT_CLASS_DEVICE && MACH_KB9200
	default y
	help
	  If you have a KwikByte KB9202 board, say Y to enable the
	  backlight driver.