#
# Video configuration
#

menu "Graphics support"
	depends on HAS_IOMEM

source "drivers/video/backlight/Kconfig"
source "drivers/video/display/Kconfig"

config VGASTATE
       tristate
       default n

config FB
	tristate "Support for frame buffer devices"
	---help---
	  The frame buffer device provides an abstraction for the graphics
	  hardware. It represents the frame buffer of some video hardware and
	  allows application software to access the graphics hardware through
	  a well-defined interface, so the software doesn't need to know
	  anything about the low-level (hardware register) stuff.

	  Frame buffer devices work identically across the different
	  architectures supported by Linux and make the implementation of
	  application programs easier and more portable; at this point, an X
	  server exists which uses the frame buffer device exclusively.
	  On several non-X86 architectures, the frame buffer device is the
	  only way to use the graphics hardware.

	  The device is accessed through special device nodes, usually located
	  in the /dev directory, i.e. /dev/fb*.

	  You need an utility program called fbset to make full use of frame
	  buffer devices. Please read <file:Documentation/fb/framebuffer.txt>
	  and the Framebuffer-HOWTO at
	  <http://www.tahallah.demon.co.uk/programming/prog.html> for more
	  information.

	  Say Y here and to the driver for your graphics board below if you
	  are compiling a kernel for a non-x86 architecture.

	  If you are compiling for the x86 architecture, you can say Y if you
	  want to play with it, but it is not essential. Please note that
	  running graphical applications that directly touch the hardware
	  (e.g. an accelerated X server) and that are not frame buffer
	  device-aware may cause unexpected results. If unsure, say N.

config FIRMWARE_EDID
       bool "Enable firmware EDID"
       depends on FB
       default n
       ---help---
         This enables access to the EDID transferred from the firmware.
	 On the i386, this is from the Video BIOS. Enable this if DDC/I2C
	 transfers do not work for your driver and if you are using
	 nvidiafb, i810fb or savagefb.

	 In general, choosing Y for this option is safe.  If you
	 experience extremely long delays while booting before you get
	 something on your display, try setting this to N.  Matrox cards in
	 combination with certain motherboards and monitors are known to
	 suffer from this problem.

config FB_DDC
       tristate
       depends on FB
       select I2C_ALGOBIT
       select I2C
       default n

config FB_CFB_FILLRECT
	tristate
	depends on FB
	default n
	---help---
	  Include the cfb_fillrect function for generic software rectangle
	  filling. This is used by drivers that don't provide their own
	  (accelerated) version.

config FB_CFB_COPYAREA
	tristate
	depends on FB
	default n
	---help---
	  Include the cfb_copyarea function for generic software area copying.
	  This is used by drivers that don't provide their own (accelerated)
	  version.

config FB_CFB_IMAGEBLIT
	tristate
	depends on FB
	default n
	---help---
	  Include the cfb_imageblit function for generic software image
	  blitting. This is used by drivers that don't provide their own
	  (accelerated) version.

config FB_SYS_FILLRECT
	tristate
	depends on FB
	default n
	---help---
	  Include the sys_fillrect function for generic software rectangle
	  filling. This is used by drivers that don't provide their own
	  (accelerated) version and the framebuffer is in system RAM.

config FB_SYS_COPYAREA
	tristate
	depends on FB
	default n
	---help---
	  Include the sys_copyarea function for generic software area copying.
	  This is used by drivers that don't provide their own (accelerated)
	  version and the framebuffer is in system RAM.

config FB_SYS_IMAGEBLIT
	tristate
	depends on FB
	default n
	---help---
	  Include the sys_imageblit function for generic software image
	  blitting. This is used by drivers that don't provide their own
	  (accelerated) version and the framebuffer is in system RAM.

config FB_SYS_FOPS
       tristate
       depends on FB
       default n

config FB_DEFERRED_IO
	bool
	depends on FB
	default y

config FB_SVGALIB
	tristate
	depends on FB
	default n
	---help---
	  Common utility functions useful to fbdev drivers of VGA-based
	  cards.

config FB_MACMODES
       tristate
       depends on FB
       default n

config FB_BACKLIGHT
	bool
	depends on FB
	select BACKLIGHT_LCD_SUPPORT
	select BACKLIGHT_CLASS_DEVICE
	default n

config FB_MODE_HELPERS
        bool "Enable Video Mode Handling Helpers"
        depends on FB
	default n
	---help---
	  This enables functions for handling video modes using the
	  Generalized Timing Formula and the EDID parser. A few drivers rely
          on this feature such as the radeonfb, rivafb, and the i810fb. If
	  your driver does not take advantage of this feature, choosing Y will
	  just increase the kernel size by about 5K.

config FB_TILEBLITTING
       bool "Enable Tile Blitting Support"
       depends on FB
       default n
       ---help---
         This enables tile blitting.  Tile blitting is a drawing technique
	 where the screen is divided into rectangular sections (tiles), whereas
	 the standard blitting divides the screen into pixels. Because the
	 default drawing element is a tile, drawing functions will be passed
	 parameters in terms of number of tiles instead of number of pixels.
	 For example, to draw a single character, instead of using bitmaps,
	 an index to an array of bitmaps will be used.  To clear or move a
	 rectangular section of a screen, the rectangle will be described in
	 terms of number of tiles in the x- and y-axis.

	 This is particularly important to one driver, matroxfb.  If
	 unsure, say N.

comment "Frame buffer hardware drivers"
	depends on FB

config FB_CIRRUS
	tristate "Cirrus Logic support"
	depends on FB && (ZORRO || PCI)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  This enables support for Cirrus Logic GD542x/543x based boards on
	  Amiga: SD64, Piccolo, Picasso II/II+, Picasso IV, or EGS Spectrum.

	  If you have a PCI-based system, this enables support for these
	  chips: GD-543x, GD-544x, GD-5480.

	  Please read the file <file:Documentation/fb/cirrusfb.txt>.

	  Say N unless you have such a graphics board or plan to get one
	  before you next recompile the kernel.

config FB_PM2
	tristate "Permedia2 support"
	depends on FB && ((AMIGA && BROKEN) || PCI)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Permedia2 AGP frame
	  buffer card from ASK, aka `Graphic Blaster Exxtreme'.  There is a
	  product page at
	  <http://www.ask.com.hk/product/Permedia%202/permedia2.htm>.

config FB_PM2_FIFO_DISCONNECT
	bool "enable FIFO disconnect feature"
	depends on FB_PM2 && PCI
	help
	  Support the Permedia2 FIFO disconnect feature (see CONFIG_FB_PM2).

config FB_ARMCLCD
	tristate "ARM PrimeCell PL110 support"
	depends on FB && ARM && ARM_AMBA
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This framebuffer device driver is for the ARM PrimeCell PL110
	  Colour LCD controller.  ARM PrimeCells provide the building
	  blocks for System on a Chip devices.

	  If you want to compile this as a module (=code which can be
	  inserted into and removed from the running kernel), say M
	  here and read <file:Documentation/kbuild/modules.txt>.  The module
	  will be called amba-clcd.

choice

	depends on FB_ARMCLCD && (ARCH_LH7A40X || ARCH_LH7952X)
	prompt "LCD Panel"
	default FB_ARMCLCD_SHARP_LQ035Q7DB02

config FB_ARMCLCD_SHARP_LQ035Q7DB02_HRTFT
	bool "LogicPD LCD 3.5\" QVGA w/HRTFT IC"
	help
	  This is an implementation of the Sharp LQ035Q7DB02, a 3.5"
	  color QVGA, HRTFT panel.  The LogicPD device includes
	  an integrated HRTFT controller IC.
	  The native resolution is 240x320.

config FB_ARMCLCD_SHARP_LQ057Q3DC02
	bool "LogicPD LCD 5.7\" QVGA"
	help
	  This is an implementation of the Sharp LQ057Q3DC02, a 5.7"
	  color QVGA, TFT panel.  The LogicPD device includes an
	  The native resolution is 320x240.

config FB_ARMCLCD_SHARP_LQ64D343
	bool "LogicPD LCD 6.4\" VGA"
	help
	  This is an implementation of the Sharp LQ64D343, a 6.4"
	  color VGA, TFT panel.  The LogicPD device includes an
	  The native resolution is 640x480.

config FB_ARMCLCD_SHARP_LQ10D368
	bool "LogicPD LCD 10.4\" VGA"
	help
	  This is an implementation of the Sharp LQ10D368, a 10.4"
	  color VGA, TFT panel.  The LogicPD device includes an
	  The native resolution is 640x480.


config FB_ARMCLCD_SHARP_LQ121S1DG41
	bool "LogicPD LCD 12.1\" SVGA"
	help
	  This is an implementation of the Sharp LQ121S1DG41, a 12.1"
	  color SVGA, TFT panel.  The LogicPD device includes an
	  The native resolution is 800x600.

	  This panel requires a clock rate may be an integer fraction
	  of the base LCDCLK frequency.  The driver will select the
	  highest frequency available that is lower than the maximum
	  allowed.  The panel may flicker if the clock rate is
	  slower than the recommended minimum.

config FB_ARMCLCD_AUO_A070VW01_WIDE
	bool "AU Optronics A070VW01 LCD 7.0\" WIDE"
	help
	  This is an implementation of the AU Optronics, a 7.0"
	  WIDE Color.  The native resolution is 234x480.

config FB_ARMCLCD_HITACHI
	bool "Hitachi Wide Screen 800x480"
	help
	  This is an implementation of the Hitachi 800x480.

endchoice


config FB_ACORN
	bool "Acorn VIDC support"
	depends on (FB = y) && ARM && (ARCH_ACORN || ARCH_CLPS7500)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Acorn VIDC graphics
	  hardware found in Acorn RISC PCs and other ARM-based machines.  If
	  unsure, say N.

config FB_CLPS711X
	bool "CLPS711X LCD support"
	depends on (FB = y) && ARM && ARCH_CLPS711X
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Say Y to enable the Framebuffer driver for the CLPS7111 and
	  EP7212 processors.

config FB_SA1100
	bool "SA-1100 LCD support"
	depends on (FB = y) && ARM && ARCH_SA1100
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is a framebuffer device for the SA-1100 LCD Controller.
	  See <http://www.linux-fbdev.org/> for information on framebuffer
	  devices.

	  If you plan to use the LCD display with your SA-1100 system, say
	  Y here.

config FB_IMX
	tristate "Motorola i.MX LCD support"
	depends on FB && ARM && ARCH_IMX
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT

config FB_CYBER2000
	tristate "CyberPro 2000/2010/5000 support"
	depends on FB && PCI && (BROKEN || !SPARC64)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This enables support for the Integraphics CyberPro 20x0 and 5000
	  VGA chips used in the Rebel.com Netwinder and other machines.
	  Say Y if you have a NetWinder or a graphics card containing this
	  device, otherwise say N.

config FB_APOLLO
	bool
	depends on (FB = y) && APOLLO
	default y
	select FB_CFB_FILLRECT
	select FB_CFB_IMAGEBLIT

config FB_Q40
	bool
	depends on (FB = y) && Q40
	default y
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT

config FB_AMIGA
	tristate "Amiga native chipset support"
	depends on FB && AMIGA
	help
	  This is the frame buffer device driver for the builtin graphics
	  chipset found in Amigas.

	  To compile this driver as a module, choose M here: the
	  module will be called amifb.

config FB_AMIGA_OCS
	bool "Amiga OCS chipset support"
	depends on FB_AMIGA
	help
	  This enables support for the original Agnus and Denise video chips,
	  found in the Amiga 1000 and most A500's and A2000's. If you intend
	  to run Linux on any of these systems, say Y; otherwise say N.

config FB_AMIGA_ECS
	bool "Amiga ECS chipset support"
	depends on FB_AMIGA
	help
	  This enables support for the Enhanced Chip Set, found in later
	  A500's, later A2000's, the A600, the A3000, the A3000T and CDTV. If
	  you intend to run Linux on any of these systems, say Y; otherwise
	  say N.

config FB_AMIGA_AGA
	bool "Amiga AGA chipset support"
	depends on FB_AMIGA
	help
	  This enables support for the Advanced Graphics Architecture (also
	  known as the AGA or AA) Chip Set, found in the A1200, A4000, A4000T
	  and CD32. If you intend to run Linux on any of these systems, say Y;
	  otherwise say N.

config FB_FM2
	bool "Amiga FrameMaster II/Rainbow II support"
	depends on (FB = y) && ZORRO
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Amiga FrameMaster
	  card from BSC (exhibited 1992 but not shipped as a CBM product).

config FB_ARC
	tristate "Arc Monochrome LCD board support"
	depends on FB && X86
	select FB_SYS_FILLRECT
	select FB_SYS_COPYAREA
	select FB_SYS_IMAGEBLIT
	select FB_SYS_FOPS
	help
	  This enables support for the Arc Monochrome LCD board. The board
	  is based on the KS-108 lcd controller and is typically a matrix
	  of 2*n chips. This driver was tested with a 128x64 panel. This
	  driver supports it for use with x86 SBCs through a 16 bit GPIO
	  interface (8 bit data, 8 bit control). If you anticipate using
	  this driver, say Y or M; otherwise say N. You must specify the
	  GPIO IO address to be used for setting control and data.

config FB_ATARI
	bool "Atari native chipset support"
	depends on (FB = y) && ATARI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the builtin graphics
	  chipset found in Ataris.

config FB_OF
	bool "Open Firmware frame buffer device support"
	depends on (FB = y) && (PPC64 || PPC_OF) && (!PPC_PSERIES || PCI)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES
	help
	  Say Y if you want support with Open Firmware for your graphics
	  board.

config FB_CONTROL
	bool "Apple \"control\" display support"
	depends on (FB = y) && PPC_PMAC && PPC32
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES
	help
	  This driver supports a frame buffer for the graphics adapter in the
	  Power Macintosh 7300 and others.

config FB_PLATINUM
	bool "Apple \"platinum\" display support"
	depends on (FB = y) && PPC_PMAC && PPC32
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES
	help
	  This driver supports a frame buffer for the "platinum" graphics
	  adapter in some Power Macintoshes.

config FB_VALKYRIE
	bool "Apple \"valkyrie\" display support"
	depends on (FB = y) && (MAC || (PPC_PMAC && PPC32))
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES
	help
	  This driver supports a frame buffer for the "valkyrie" graphics
	  adapter in some Power Macintoshes.

config FB_CT65550
	bool "Chips 65550 display support"
	depends on (FB = y) && PPC32
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Chips & Technologies
	  65550 graphics chip in PowerBooks.

config FB_ASILIANT
	bool "Asiliant (Chips) 69000 display support"
	depends on (FB = y) && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Asiliant 69030 chipset

config FB_IMSTT
	bool "IMS Twin Turbo display support"
	depends on (FB = y) && PCI
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES if PPC
	help
	  The IMS Twin Turbo is a PCI-based frame buffer card bundled with
	  many Macintosh and compatible computers.

config FB_VGA16
	tristate "VGA 16-color graphics support"
	depends on FB && (X86 || PPC)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select VGASTATE
	select FONT_8x16 if FRAMEBUFFER_CONSOLE
	help
	  This is the frame buffer device driver for VGA 16 color graphic
	  cards. Say Y if you have such a card.

	  To compile this driver as a module, choose M here: the
	  module will be called vga16fb.

config FB_STI
	tristate "HP STI frame buffer device support"
	depends on FB && PARISC
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	default y
	---help---
	  STI refers to the HP "Standard Text Interface" which is a set of
	  BIOS routines contained in a ROM chip in HP PA-RISC based machines.
	  Enabling this option will implement the linux framebuffer device
	  using calls to the STI BIOS routines for initialisation.
	
	  If you enable this option, you will get a planar framebuffer device
	  /dev/fb which will work on the most common HP graphic cards of the
	  NGLE family, including the artist chips (in the 7xx and Bxxx series),
	  HCRX, HCRX24, CRX, CRX24 and VisEG series.

	  It is safe to enable this option, so you should probably say "Y".

config FB_MAC
	bool "Generic Macintosh display support"
	depends on (FB = y) && MAC
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES

#      bool '  Apple DAFB display support' CONFIG_FB_DAFB
config FB_HP300
	bool
	depends on (FB = y) && HP300
	select FB_CFB_FILLRECT
	select FB_CFB_IMAGEBLIT
	default y

config FB_TGA
	tristate "TGA/SFB+ framebuffer support"
	depends on FB && (ALPHA || TC)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select BITREVERSE
	---help---
	  This is the frame buffer device driver for generic TGA and SFB+
	  graphic cards.  These include DEC ZLXp-E1, -E2 and -E3 PCI cards,
	  also known as PBXGA-A, -B and -C, and DEC ZLX-E1, -E2 and -E3
	  TURBOchannel cards, also known as PMAGD-A, -B and -C.

	  Due to hardware limitations ZLX-E2 and E3 cards are not supported
	  for DECstation 5000/200 systems.  Additionally due to firmware
	  limitations these cards may cause troubles with booting DECstation
	  5000/240 and /260 systems, but are fully supported under Linux if
	  you manage to get it going. ;-)

	  Say Y if you have one of those.

config FB_VESA
	bool "VESA VGA graphics support"
	depends on (FB = y) && X86
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select VIDEO_SELECT
	help
	  This is the frame buffer device driver for generic VESA 2.0
	  compliant graphic cards. The older VESA 1.2 cards are not supported.
	  You will get a boot time penguin logo at no additional cost. Please
	  read <file:Documentation/fb/vesafb.txt>. If unsure, say Y.

config FB_IMAC
	bool "Intel-based Macintosh Framebuffer Support"
	depends on (FB = y) && X86 && EFI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Intel-based Macintosh

config FB_HECUBA
       tristate "Hecuba board support"
       depends on FB && X86 && MMU
       select FB_SYS_FILLRECT
       select FB_SYS_COPYAREA
       select FB_SYS_IMAGEBLIT
       select FB_SYS_FOPS
       select FB_DEFERRED_IO
       help
         This enables support for the Hecuba board. This driver was tested
         with an E-Ink 800x600 display and x86 SBCs through a 16 bit GPIO
         interface (8 bit data, 4 bit control). If you anticpate using
         this driver, say Y or M; otherwise say N. You must specify the
         GPIO IO address to be used for setting control and data.

config FB_HGA
	tristate "Hercules mono graphics support"
	depends on FB && X86
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Say Y here if you have a Hercules mono graphics card.

	  To compile this driver as a module, choose M here: the
	  module will be called hgafb.

	  As this card technology is 15 years old, most people will answer N
	  here.

config FB_HGA_ACCEL
	bool "Hercules mono Acceleration functions (EXPERIMENTAL)"
	depends on FB_HGA && EXPERIMENTAL
	---help---
	This will compile the Hercules mono graphics with
	acceleration functions.

config FB_SGIVW
	tristate "SGI Visual Workstation framebuffer support"
	depends on FB && X86_VISWS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  SGI Visual Workstation support for framebuffer graphics.

config FB_GBE
	bool "SGI Graphics Backend frame buffer support"
	depends on (FB = y) && (SGI_IP32 || X86_VISWS)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
 	help
	  This is the frame buffer device driver for SGI Graphics Backend.
	  This chip is used in SGI O2 and Visual Workstation 320/540.

config FB_GBE_MEM
	int "Video memory size in MB"
	depends on FB_GBE
	default 4
	help
	  This is the amount of memory reserved for the framebuffer,
	  which can be any value between 1MB and 8MB.

config FB_SBUS
	bool "SBUS and UPA framebuffers"
	depends on (FB = y) && SPARC
	help
	  Say Y if you want support for SBUS or UPA based frame buffer device.

config FB_BW2
	bool "BWtwo support"
	depends on (FB = y) && (SPARC && FB_SBUS)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the BWtwo frame buffer.

config FB_CG3
	bool "CGthree support"
	depends on (FB = y) && (SPARC && FB_SBUS)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the CGthree frame buffer.

config FB_CG6
	bool "CGsix (GX,TurboGX) support"
	depends on (FB = y) && (SPARC && FB_SBUS)
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the CGsix (GX, TurboGX)
	  frame buffer.

config FB_FFB
	bool "Creator/Creator3D/Elite3D support"
	depends on FB_SBUS && SPARC64
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Creator, Creator3D,
	  and Elite3D graphics boards.

config FB_TCX
	bool "TCX (SS4/SS5 only) support"
	depends on FB_SBUS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the TCX 24/8bit frame
	  buffer.

config FB_CG14
	bool "CGfourteen (SX) support"
	depends on FB_SBUS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the CGfourteen frame
	  buffer on Desktop SPARCsystems with the SX graphics option.

config FB_P9100
	bool "P9100 (Sparcbook 3 only) support"
	depends on FB_SBUS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the P9100 card
	  supported on Sparcbook 3 machines.

config FB_LEO
	bool "Leo (ZX) support"
	depends on FB_SBUS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the SBUS-based Sun ZX
	  (leo) frame buffer cards.

config FB_IGA
	bool "IGA 168x display support"
	depends on (FB = y) && SPARC32
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the framebuffer device for the INTERGRAPHICS 1680 and
	  successor frame buffer cards.

config FB_XVR500
	bool "Sun XVR-500 3DLABS Wildcat support"
	depends on (FB = y) && PCI && SPARC64
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the framebuffer device for the Sun XVR-500 and similar
	  graphics cards based upon the 3DLABS Wildcat chipset.  The driver
	  only works on sparc64 systems where the system firwmare has
	  mostly initialized the card already.  It is treated as a
	  completely dumb framebuffer device.

config FB_XVR2500
	bool "Sun XVR-2500 3DLABS Wildcat support"
	depends on (FB = y) && PCI && SPARC64
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the framebuffer device for the Sun XVR-2500 and similar
	  graphics cards based upon the 3DLABS Wildcat chipset.  The driver
	  only works on sparc64 systems where the system firwmare has
	  mostly initialized the card already.  It is treated as a
	  completely dumb framebuffer device.

config FB_PVR2
	tristate "NEC PowerVR 2 display support"
	depends on FB && SH_DREAMCAST
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Say Y here if you have a PowerVR 2 card in your box.  If you plan to
	  run linux on your Dreamcast, you will have to say Y here.
	  This driver may or may not work on other PowerVR 2 cards, but is
	  totally untested.  Use at your own risk.  If unsure, say N.

	  To compile this driver as a module, choose M here: the
	  module will be called pvr2fb.

	  You can pass several parameters to the driver at boot time or at
	  module load time.  The parameters look like "video=pvr2:XXX", where
	  the meaning of XXX can be found at the end of the main source file
	  (<file:drivers/video/pvr2fb.c>). Please see the file
	  <file:Documentation/fb/pvr2fb.txt>.

config FB_EPSON1355
	bool "Epson 1355 framebuffer support"
	depends on (FB = y) && (SUPERH || ARCH_CEIVA)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Build in support for the SED1355 Epson Research Embedded RAMDAC
	  LCD/CRT Controller (since redesignated as the S1D13505) as a
	  framebuffer.  Product specs at
	  <http://www.erd.epson.com/vdc/html/products.htm>.

config FB_S1D15605
	tristate "Epson S1D15605 framebuffer support"
	depends on FB
	default m if MACH_KB9200
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Build in support for the S1D15605 Epson Research 128x64
	  LCD controller as a framebuffer.

config FB_S1D13XXX
	tristate "Epson S1D13XXX framebuffer support"
	depends on FB
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Support for S1D13XXX framebuffer device family (currently only
	  working with S1D13806). Product specs at
	  <http://www.erd.epson.com/vdc/html/legacy_13xxx.htm>

config FB_ATMEL
	tristate "AT91/AT32 LCD Controller support"
	depends on FB && (ARCH_AT91SAM9261 || ARCH_AT91SAM9263 || ARCH_AT91SAM9RL || AVR32)
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This enables support for the AT91/AT32 LCD Controller.

config FB_INTSRAM
	bool "Frame Buffer in internal SRAM"
	depends on FB_ATMEL && ARCH_AT91SAM9261
	help
	  Say Y if you want to map Frame Buffer in internal SRAM. Say N if you want
	  to let frame buffer in external SDRAM.

config FB_ATMEL_STN
	bool "Use a STN display with AT91/AT32 LCD Controller"
	depends on FB_ATMEL && MACH_AT91SAM9261EK
	default n
	help
	  Say Y if you want to connect a STN LCD display to the AT91/AT32 LCD
	  Controller. Say N if you want to connect a TFT.

	  If unsure, say N.

config FB_NVIDIA
	tristate "nVidia Framebuffer Support"
	depends on FB && PCI
	select FB_BACKLIGHT if FB_NVIDIA_BACKLIGHT
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select BITREVERSE
	select VGASTATE
	help
	  This driver supports graphics boards with the nVidia chips, TNT
	  and newer. For very old chipsets, such as the RIVA128, then use
	  the rivafb.
	  Say Y if you have such a graphics board.

	  To compile this driver as a module, choose M here: the
	  module will be called nvidiafb.

config FB_NVIDIA_I2C
       bool "Enable DDC Support"
       depends on FB_NVIDIA
       select FB_DDC
       help
	  This enables I2C support for nVidia Chipsets.  This is used
	  only for getting EDID information from the attached display
	  allowing for robust video mode handling and switching.

	  Because fbdev-2.6 requires that drivers must be able to
	  independently validate video mode parameters, you should say Y
	  here.

config FB_NVIDIA_DEBUG
	bool "Lots of debug output"
	depends on FB_NVIDIA
	default n
	help
	  Say Y here if you want the nVidia driver to output all sorts
	  of debugging information to provide to the maintainer when
	  something goes wrong.

config FB_NVIDIA_BACKLIGHT
	bool "Support for backlight control"
	depends on FB_NVIDIA
	default y
	help
	  Say Y here if you want to control the backlight of your display.

config FB_RIVA
	tristate "nVidia Riva support"
	depends on FB && PCI
	select FB_BACKLIGHT if FB_RIVA_BACKLIGHT
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select BITREVERSE
	select VGASTATE
	help
	  This driver supports graphics boards with the nVidia Riva/Geforce
	  chips.
	  Say Y if you have such a graphics board.

	  To compile this driver as a module, choose M here: the
	  module will be called rivafb.

config FB_RIVA_I2C
       bool "Enable DDC Support"
       depends on FB_RIVA
       select FB_DDC
       help
	  This enables I2C support for nVidia Chipsets.  This is used
	  only for getting EDID information from the attached display
	  allowing for robust video mode handling and switching.

	  Because fbdev-2.6 requires that drivers must be able to
	  independently validate video mode parameters, you should say Y
	  here.

config FB_RIVA_DEBUG
	bool "Lots of debug output"
	depends on FB_RIVA
	default n
	help
	  Say Y here if you want the Riva driver to output all sorts
	  of debugging information to provide to the maintainer when
	  something goes wrong.

config FB_RIVA_BACKLIGHT
	bool "Support for backlight control"
	depends on FB_RIVA
	default y
	help
	  Say Y here if you want to control the backlight of your display.

config FB_I810
	tristate "Intel 810/815 support (EXPERIMENTAL)"
	depends on FB && EXPERIMENTAL && PCI && X86_32
	select AGP
	select AGP_INTEL
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select VGASTATE
	help
	  This driver supports the on-board graphics built in to the Intel 810 
          and 815 chipsets.  Say Y if you have and plan to use such a board.

          To compile this driver as a module, choose M here: the
	  module will be called i810fb.

          For more information, please read 
	  <file:Documentation/fb/intel810.txt>

config FB_I810_GTF
	bool "use VESA Generalized Timing Formula"
	depends on FB_I810
	help
	  If you say Y, then the VESA standard, Generalized Timing Formula 
          or GTF, will be used to calculate the required video timing values
	  per video mode.  Since the GTF allows nondiscrete timings 
          (nondiscrete being a range of values as opposed to discrete being a
          set of values), you'll be able to use any combination of horizontal 
	  and vertical resolutions, and vertical refresh rates without having
	  to specify your own timing parameters.  This is especially useful
	  to maximize the performance of an aging display, or if you just 
          have a display with nonstandard dimensions. A VESA compliant 
	  monitor is recommended, but can still work with non-compliant ones.
	  If you need or want this, then select this option. The timings may 
	  not be compliant with Intel's recommended values. Use at your own 
	  risk.

          If you say N, the driver will revert to discrete video timings 
	  using a set recommended by Intel in their documentation.
  
          If unsure, say N.

config FB_I810_I2C
	bool "Enable DDC Support"
	depends on FB_I810 && FB_I810_GTF
	select FB_DDC
	help

config FB_LE80578
	tristate "Intel LE80578 (Vermilion) support"
	depends on FB && PCI && X86
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This driver supports the LE80578 (Vermilion Range) chipset

config FB_CARILLO_RANCH
	tristate "Intel Carillo Ranch support"
	depends on FB_LE80578 && FB && PCI && X86
	help
	  This driver supports the LE80578 (Carillo Ranch) board

config FB_INTEL
	tristate "Intel 830M/845G/852GM/855GM/865G/915G/945G support (EXPERIMENTAL)"
	depends on FB && EXPERIMENTAL && PCI && X86
	select AGP
	select AGP_INTEL
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This driver supports the on-board graphics built in to the Intel
          830M/845G/852GM/855GM/865G/915G/915GM/945G/945GM chipsets.
          Say Y if you have and plan to use such a board.

	  If you say Y here and want DDC/I2C support you must first say Y to
	  "I2C support" and "I2C bit-banging support" in the character devices
	  section.

	  If you say M here then "I2C support" and "I2C bit-banging support"
	  can be build either as modules or built-in.

	  To compile this driver as a module, choose M here: the
	  module will be called intelfb.

	  For more information, please read <file:Documentation/fb/intelfb.txt>

config FB_INTEL_DEBUG
	bool "Intel driver Debug Messages"
	depends on FB_INTEL
	---help---
	  Say Y here if you want the Intel driver to output all sorts
	  of debugging information to provide to the maintainer when
	  something goes wrong.

config FB_INTEL_I2C
	bool "DDC/I2C for Intel framebuffer support"
	depends on FB_INTEL
	select FB_DDC
	default y
	help
	  Say Y here if you want DDC/I2C support for your on-board Intel graphics.

config FB_MATROX
	tristate "Matrox acceleration"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_TILEBLITTING
	select FB_MACMODES if PPC_PMAC
	---help---
	  Say Y here if you have a Matrox Millennium, Matrox Millennium II,
	  Matrox Mystique, Matrox Mystique 220, Matrox Productiva G100, Matrox
	  Mystique G200, Matrox Millennium G200, Matrox Marvel G200 video,
	  Matrox G400, G450 or G550 card in your box.

	  To compile this driver as a module, choose M here: the
	  module will be called matroxfb.

	  You can pass several parameters to the driver at boot time or at
	  module load time. The parameters look like "video=matrox:XXX", and
	  are described in <file:Documentation/fb/matroxfb.txt>.

config FB_MATROX_MILLENIUM
	bool "Millennium I/II support"
	depends on FB_MATROX
	help
	  Say Y here if you have a Matrox Millennium or Matrox Millennium II
	  video card. If you select "Advanced lowlevel driver options" below,
	  you should check 4 bpp packed pixel, 8 bpp packed pixel, 16 bpp
	  packed pixel, 24 bpp packed pixel and 32 bpp packed pixel. You can
	  also use font widths different from 8.

config FB_MATROX_MYSTIQUE
	bool "Mystique support"
	depends on FB_MATROX
	help
	  Say Y here if you have a Matrox Mystique or Matrox Mystique 220
	  video card. If you select "Advanced lowlevel driver options" below,
	  you should check 8 bpp packed pixel, 16 bpp packed pixel, 24 bpp
	  packed pixel and 32 bpp packed pixel. You can also use font widths
	  different from 8.

config FB_MATROX_G
	bool "G100/G200/G400/G450/G550 support"
	depends on FB_MATROX
	---help---
	  Say Y here if you have a Matrox G100, G200, G400, G450 or G550 based
	  video card. If you select "Advanced lowlevel driver options", you
	  should check 8 bpp packed pixel, 16 bpp packed pixel, 24 bpp packed
	  pixel and 32 bpp packed pixel. You can also use font widths
	  different from 8.

	  If you need support for G400 secondary head, you must first say Y to
	  "I2C support" in the character devices section, and then to
	  "Matrox I2C support" and "G400 second head support" here in the
	  framebuffer section. G450/G550 secondary head and digital output
	  are supported without additional modules.

	  The driver starts in monitor mode. You must use the matroxset tool 
	  (available at <ftp://platan.vc.cvut.cz/pub/linux/matrox-latest/>) to 
	  swap primary and secondary head outputs, or to change output mode.  
	  Secondary head driver always start in 640x480 resolution and you 
	  must use fbset to change it.

	  Do not forget that second head supports only 16 and 32 bpp
	  packed pixels, so it is a good idea to compile them into the kernel
	  too. You can use only some font widths, as the driver uses generic
	  painting procedures (the secondary head does not use acceleration
	  engine).

	  G450/G550 hardware can display TV picture only from secondary CRTC,
	  and it performs no scaling, so picture must have 525 or 625 lines.

config FB_MATROX_I2C
	tristate "Matrox I2C support"
	depends on FB_MATROX
	select FB_DDC
	---help---
	  This drivers creates I2C buses which are needed for accessing the
	  DDC (I2C) bus present on all Matroxes, an I2C bus which
	  interconnects Matrox optional devices, like MGA-TVO on G200 and
	  G400, and the secondary head DDC bus, present on G400 only.

	  You can say Y or M here if you want to experiment with monitor
	  detection code. You must say Y or M here if you want to use either
	  second head of G400 or MGA-TVO on G200 or G400.

	  If you compile it as module, it will create a module named
	  i2c-matroxfb.

config FB_MATROX_MAVEN
	tristate "G400 second head support"
	depends on FB_MATROX_G && FB_MATROX_I2C
	---help---
	  WARNING !!! This support does not work with G450 !!!

	  Say Y or M here if you want to use a secondary head (meaning two
	  monitors in parallel) on G400 or MGA-TVO add-on on G200. Secondary
	  head is not compatible with accelerated XFree 3.3.x SVGA servers -
	  secondary head output is blanked while you are in X. With XFree
	  3.9.17 preview you can use both heads if you use SVGA over fbdev or
	  the fbdev driver on first head and the fbdev driver on second head.

	  If you compile it as module, two modules are created,
	  matroxfb_crtc2 and matroxfb_maven. Matroxfb_maven is needed for
	  both G200 and G400, matroxfb_crtc2 is needed only by G400. You must
	  also load i2c-matroxfb to get it to run.

	  The driver starts in monitor mode and you must use the matroxset
	  tool (available at
	  <ftp://platan.vc.cvut.cz/pub/linux/matrox-latest/>) to switch it to
	  PAL or NTSC or to swap primary and secondary head outputs.
	  Secondary head driver also always start in 640x480 resolution, you
	  must use fbset to change it.

	  Also do not forget that second head supports only 16 and 32 bpp
	  packed pixels, so it is a good idea to compile them into the kernel
	  too.  You can use only some font widths, as the driver uses generic
	  painting procedures (the secondary head does not use acceleration
	  engine).

config FB_MATROX_MULTIHEAD
	bool "Multihead support"
	depends on FB_MATROX
	---help---
	  Say Y here if you have more than one (supported) Matrox device in
	  your computer and you want to use all of them for different monitors
	  ("multihead"). If you have only one device, you should say N because
	  the driver compiled with Y is larger and a bit slower, especially on
	  ia32 (ix86).

	  If you said M to "Matrox unified accelerated driver" and N here, you
	  will still be able to use several Matrox devices simultaneously:
	  insert several instances of the module matroxfb into the kernel
	  with insmod, supplying the parameter "dev=N" where N is 0, 1, etc.
	  for the different Matrox devices. This method is slightly faster but
	  uses 40 KB of kernel memory per Matrox card.

	  There is no need for enabling 'Matrox multihead support' if you have
	  only one Matrox card in the box.

config FB_RADEON
	tristate "ATI Radeon display support"
	depends on FB && PCI
	select FB_BACKLIGHT if FB_RADEON_BACKLIGHT
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_MACMODES if PPC_OF
	help
	  Choose this option if you want to use an ATI Radeon graphics card as
	  a framebuffer device.  There are both PCI and AGP versions.  You
	  don't need to choose this to run the Radeon in plain VGA mode.

	  If you say Y here and want DDC/I2C support you must first say Y to
	  "I2C support" and "I2C bit-banging support" in the character devices
	  section.

	  If you say M here then "I2C support" and "I2C bit-banging support" 
	  can be build either as modules or built-in.

	  There is a product page at
	  http://apps.ati.com/ATIcompare/

config FB_RADEON_I2C
	bool "DDC/I2C for ATI Radeon support"
	depends on FB_RADEON
	select FB_DDC
	default y
	help
	  Say Y here if you want DDC/I2C support for your Radeon board. 

config FB_RADEON_BACKLIGHT
	bool "Support for backlight control"
	depends on FB_RADEON
	default y
	help
	  Say Y here if you want to control the backlight of your display.

config FB_RADEON_DEBUG
	bool "Lots of debug output from Radeon driver"
	depends on FB_RADEON
	default n
	help
	  Say Y here if you want the Radeon driver to output all sorts
	  of debugging information to provide to the maintainer when
	  something goes wrong.

config FB_ATY128
	tristate "ATI Rage128 display support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_BACKLIGHT if FB_ATY128_BACKLIGHT
	select FB_MACMODES if PPC_PMAC
	help
	  This driver supports graphics boards with the ATI Rage128 chips.
	  Say Y if you have such a graphics board and read
	  <file:Documentation/fb/aty128fb.txt>.

	  To compile this driver as a module, choose M here: the
	  module will be called aty128fb.

config FB_ATY128_BACKLIGHT
	bool "Support for backlight control"
	depends on FB_ATY128
	default y
	help
	  Say Y here if you want to control the backlight of your display.

config FB_ATY
	tristate "ATI Mach64 display support" if PCI || ATARI
	depends on FB && !SPARC32
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_BACKLIGHT if FB_ATY_BACKLIGHT
	select FB_MACMODES if PPC
	help
	  This driver supports graphics boards with the ATI Mach64 chips.
	  Say Y if you have such a graphics board.

	  To compile this driver as a module, choose M here: the
	  module will be called atyfb.

config FB_ATY_CT
	bool "Mach64 CT/VT/GT/LT (incl. 3D RAGE) support"
	depends on PCI && FB_ATY
	default y if SPARC64 && PCI
	help
	  Say Y here to support use of ATI's 64-bit Rage boards (or other
	  boards based on the Mach64 CT, VT, GT, and LT chipsets) as a
	  framebuffer device.  The ATI product support page for these boards
	  is at <http://support.ati.com/products/pc/mach64/>.

config FB_ATY_GENERIC_LCD
	bool "Mach64 generic LCD support (EXPERIMENTAL)"
	depends on FB_ATY_CT
	help
	  Say Y if you have a laptop with an ATI Rage LT PRO, Rage Mobility,
	  Rage XC, or Rage XL chipset.

config FB_ATY_GX
	bool "Mach64 GX support" if PCI
	depends on FB_ATY
	default y if ATARI
	help
	  Say Y here to support use of the ATI Mach64 Graphics Expression
	  board (or other boards based on the Mach64 GX chipset) as a
	  framebuffer device.  The ATI product support page for these boards
	  is at
	  <http://support.ati.com/products/pc/mach64/graphics_xpression.html>.

config FB_ATY_BACKLIGHT
	bool "Support for backlight control"
	depends on FB_ATY
	default y
	help
	  Say Y here if you want to control the backlight of your display.

config FB_S3
	tristate "S3 Trio/Virge support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_TILEBLITTING
	select FB_SVGALIB
	select VGASTATE
	select FONT_8x16 if FRAMEBUFFER_CONSOLE
	---help---
	  Driver for graphics boards with S3 Trio / S3 Virge chip.

config FB_SAVAGE
	tristate "S3 Savage support"
	depends on FB && PCI && EXPERIMENTAL
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select VGASTATE
	help
	  This driver supports notebooks and computers with S3 Savage PCI/AGP
	  chips.

	  Say Y if you have such a graphics card.

	  To compile this driver as a module, choose M here; the module
	  will be called savagefb.

config FB_SAVAGE_I2C
       bool "Enable DDC2 Support"
       depends on FB_SAVAGE
       select FB_DDC
       help
	  This enables I2C support for S3 Savage Chipsets.  This is used
	  only for getting EDID information from the attached display
	  allowing for robust video mode handling and switching.

	  Because fbdev-2.6 requires that drivers must be able to
	  independently validate video mode parameters, you should say Y
	  here.

config FB_SAVAGE_ACCEL
       bool "Enable Console Acceleration"
       depends on FB_SAVAGE
       default n
       help
          This option will compile in console acceleration support. If
          the resulting framebuffer console has bothersome glitches, then
          choose N here.

config FB_SIS
	tristate "SiS/XGI display support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the SiS 300, 315, 330
	  and 340 series as well as XGI V3XT, V5, V8, Z7 graphics chipsets.
	  Specs available at <http://www.sis.com> and <http://www.xgitech.com>.

	  To compile this driver as a module, choose M here; the module
	  will be called sisfb.

config FB_SIS_300
	bool "SiS 300 series support"
	depends on FB_SIS
	help
	  Say Y here to support use of the SiS 300/305, 540, 630 and 730.

config FB_SIS_315
	bool "SiS 315/330/340 series and XGI support"
	depends on FB_SIS
	help
	  Say Y here to support use of the SiS 315, 330 and 340 series
	  (315/H/PRO, 55x, 650, 651, 740, 330, 661, 741, 760, 761) as well
	  as XGI V3XT, V5, V8 and Z7.

config FB_NEOMAGIC
	tristate "NeoMagic display support"
	depends on FB && PCI
	select FB_MODE_HELPERS
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select VGASTATE
	help
	  This driver supports notebooks with NeoMagic PCI chips.
	  Say Y if you have such a graphics card. 

	  To compile this driver as a module, choose M here: the
	  module will be called neofb.

config FB_KYRO
	tristate "IMG Kyro support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  Say Y here if you have a STG4000 / Kyro / PowerVR 3 based
	  graphics board.

	  To compile this driver as a module, choose M here: the
	  module will be called kyrofb.

config FB_3DFX
	tristate "3Dfx Banshee/Voodoo3 display support"
	depends on FB && PCI
	select FB_CFB_IMAGEBLIT
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	help
	  This driver supports graphics boards with the 3Dfx Banshee/Voodoo3
	  chips. Say Y if you have such a graphics board.

	  To compile this driver as a module, choose M here: the
	  module will be called tdfxfb.

config FB_3DFX_ACCEL
	bool "3Dfx Banshee/Voodoo3 Acceleration functions (EXPERIMENTAL)"
	depends on FB_3DFX && EXPERIMENTAL
	---help---
	This will compile the 3Dfx Banshee/Voodoo3 frame buffer device
	with acceleration functions.


config FB_VOODOO1
	tristate "3Dfx Voodoo Graphics (sst1) support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Say Y here if you have a 3Dfx Voodoo Graphics (Voodoo1/sst1) or 
	  Voodoo2 (cvg) based graphics card.

	  To compile this driver as a module, choose M here: the
	  module will be called sstfb.

	  WARNING: Do not use any application that uses the 3D engine
	  (namely glide) while using this driver.
	  Please read the <file:Documentation/fb/README-sstfb.txt> for supported
	  options and other important info  support.

config FB_VT8623
	tristate "VIA VT8623 support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_TILEBLITTING
	select FB_SVGALIB
	select VGASTATE
	select FONT_8x16 if FRAMEBUFFER_CONSOLE
	---help---
	  Driver for CastleRock integrated graphics core in the
	  VIA VT8623 [Apollo CLE266] chipset.

config FB_CYBLA
	tristate "Cyberblade/i1 support"
	depends on FB && PCI && X86_32 && !64BIT
	select FB_CFB_IMAGEBLIT
	select VIDEO_SELECT
	---help---
	  This driver is supposed to support the Trident Cyberblade/i1
	  graphics core integrated in the VIA VT8601A North Bridge,
	  also known as VIA Apollo PLE133.

	  Status:
	   - Developed, tested and working on EPIA 5000 and EPIA 800.
	   - Does work reliable on all systems with CRT/LCD connected to
	     normal VGA ports.
	   - Should work on systems that do use the internal LCD port, but
	     this is absolutely not tested.

	  Character imageblit, copyarea and rectangle fill are hw accelerated,
	  ypan scrolling is used by default.

	  Please do read <file:Documentation/fb/cyblafb/*>.

	  To compile this driver as a module, choose M here: the
	  module will be called cyblafb.

config FB_TRIDENT
	tristate "Trident support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  This driver is supposed to support graphics boards with the
	  Trident CyberXXXX/Image/CyberBlade chips mostly found in laptops
	  but also on some motherboards. For more information, read
	  <file:Documentation/fb/tridentfb.txt>

	  Cyberblade/i1 support will be removed soon, use the cyblafb driver
	  instead.

	  Say Y if you have such a graphics board.


	  To compile this driver as a module, choose M here: the
	  module will be called tridentfb.

config FB_TRIDENT_ACCEL
	bool "Trident Acceleration functions (EXPERIMENTAL)"
	depends on FB_TRIDENT && EXPERIMENTAL
	---help---
	This will compile the Trident frame buffer device with
	acceleration functions.

config FB_ARK
	tristate "ARK 2000PV support"
	depends on FB && PCI
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	select FB_TILEBLITTING
	select FB_SVGALIB
	select VGASTATE
	select FONT_8x16 if FRAMEBUFFER_CONSOLE
	---help---
	  Driver for PCI graphics boards with ARK 2000PV chip
	  and ICS 5342 RAMDAC.

config FB_PM3
	tristate "Permedia3 support (EXPERIMENTAL)"
	depends on FB && PCI && EXPERIMENTAL
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the 3DLabs Permedia3
	  chipset, used in Formac ProFormance III, 3DLabs Oxygen VX1 &
	  similar boards, 3DLabs Permedia3 Create!, Appian Jeronimo 2000
	  and maybe other boards.

config FB_AU1100
	bool "Au1100 LCD Driver"
	depends on (FB = y) && EXPERIMENTAL && PCI && MIPS && MIPS_PB1100=y

config FB_AU1200
	bool "Au1200 LCD Driver"
	depends on (FB = y) && MIPS && SOC_AU1200
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the framebuffer driver for the AMD Au1200 SOC.  It can drive
	  various panels and CRTs by passing in kernel cmd line option
	  au1200fb:panel=<name>.

source "drivers/video/geode/Kconfig"

config FB_HIT
	tristate "HD64461 Frame Buffer support"
	depends on FB && HD64461
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  This is the frame buffer device driver for the Hitachi HD64461 LCD
	  frame buffer card.

config FB_PMAG_AA
	bool "PMAG-AA TURBOchannel framebuffer support"
	depends on (FB = y) && TC
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  Support for the PMAG-AA TURBOchannel framebuffer card (1280x1024x1)
	  used mainly in the MIPS-based DECstation series.

config FB_PMAG_BA
	tristate "PMAG-BA TURBOchannel framebuffer support"
	depends on FB && TC
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  Support for the PMAG-BA TURBOchannel framebuffer card (1024x864x8)
	  used mainly in the MIPS-based DECstation series.

config FB_PMAGB_B
	tristate "PMAGB-B TURBOchannel framebuffer support"
	depends on TC
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  Support for the PMAGB-B TURBOchannel framebuffer card used mainly
	  in the MIPS-based DECstation series. The card is currently only
	  supported in 1280x1024x8 mode.

config FB_MAXINE
	bool "Maxine (Personal DECstation) onboard framebuffer support"
	depends on (FB = y) && MACH_DECSTATION
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  Support for the onboard framebuffer (1024x768x8) in the Personal
	  DECstation series (Personal DECstation 5000/20, /25, /33, /50,
	  Codename "Maxine").

config FB_TX3912
	bool "TMPTX3912/PR31700 frame buffer support"
	depends on (FB = y) && NINO
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	help
	  The TX3912 is a Toshiba RISC processor based on the MIPS 3900 core
	  see <http://www.toshiba.com/taec/components/Generic/risc/tx3912.htm>.

	  Say Y here to enable kernel support for the on-board framebuffer.

config FB_G364
	bool "G364 frame buffer support"
	depends on (FB = y) && (MIPS_MAGNUM_4000 || OLIVETTI_M700)
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  The G364 driver is the framebuffer used in MIPS Magnum 4000 and
	  Olivetti M700-10 systems.

config FB_68328
	bool "Motorola 68328 native frame buffer support"
	depends on (FB = y) && (M68328 || M68EZ328 || M68VZ328)
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	help
	  Say Y here if you want to support the built-in frame buffer of
	  the Motorola 68328 CPU family.

config FB_PXA
	tristate "PXA LCD framebuffer support"
	depends on FB && ARCH_PXA
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Frame buffer driver for the built-in LCD controller in the Intel
	  PXA2x0 processor.

	  This driver is also available as a module ( = code which can be
	  inserted and removed from the running kernel whenever you want). The
	  module will be called pxafb. If you want to compile it as a module,
	  say M here and read <file:Documentation/kbuild/modules.txt>.

	  If unsure, say N.

config FB_PXA_PARAMETERS
	bool "PXA LCD command line parameters"
	default n
	depends on FB_PXA
	---help---
	  Enable the use of kernel command line or module parameters
	  to configure the physical properties of the LCD panel when
	  using the PXA LCD driver.

	  This option allows you to override the panel parameters
	  supplied by the platform in order to support multiple
	  different models of flatpanel. If you will only be using a
	  single model of flatpanel then you can safely leave this
	  option disabled.

	  <file:Documentation/fb/pxafb.txt> describes the available parameters.

config FB_MBX
	tristate "2700G LCD framebuffer support"
	depends on FB && ARCH_PXA
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Framebuffer driver for the Intel 2700G (Marathon) Graphics
	  Accelerator

config FB_MBX_DEBUG
       bool "Enable debugging info via debugfs"
       depends on FB_MBX && DEBUG_FS
       default n
       ---help---
         Enable this if you want debugging information using the debug
         filesystem (debugfs)

         If unsure, say N.

config FB_W100
	tristate "W100 frame buffer support"
	depends on FB && PXA_SHARPSL
 	select FB_CFB_FILLRECT
 	select FB_CFB_COPYAREA
 	select FB_CFB_IMAGEBLIT
	---help---
	  Frame buffer driver for the w100 as found on the Sharp SL-Cxx series.

	  This driver is also available as a module ( = code which can be
	  inserted and removed from the running kernel whenever you want). The
	  module will be called w100fb. If you want to compile it as a module,
	  say M here and read <file:Documentation/kbuild/modules.txt>.

	  If unsure, say N.

config FB_S3C2410
	tristate "S3C2410 LCD framebuffer support"
	depends on FB && ARCH_S3C2410
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Frame buffer driver for the built-in LCD controller in the Samsung
	  S3C2410 processor.

	  This driver is also available as a module ( = code which can be
	  inserted and removed from the running kernel whenever you want). The
	  module will be called s3c2410fb. If you want to compile it as a module,
	  say M here and read <file:Documentation/kbuild/modules.txt>.

	  If unsure, say N.
config FB_S3C2410_DEBUG
	bool "S3C2410 lcd debug messages"
	depends on FB_S3C2410
	help
	  Turn on debugging messages. Note that you can set/unset at run time
	  through sysfs

config FB_SM501
	tristate "Silicon Motion SM501 framebuffer support"
	depends on FB && MFD_SM501
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Frame buffer driver for the CRT and LCD controllers in the Silicon
	  Motion SM501.

	  This driver is also available as a module ( = code which can be
	  inserted and removed from the running kernel whenever you want). The
	  module will be called sm501fb. If you want to compile it as a module,
	  say M here and read <file:Documentation/modules.txt>.

	  If unsure, say N.


config FB_PNX4008_DUM
	tristate "Display Update Module support on Philips PNX4008 board"
	depends on FB && ARCH_PNX4008
	---help---
	  Say Y here to enable support for PNX4008 Display Update Module (DUM)

config FB_PNX4008_DUM_RGB
	tristate "RGB Framebuffer support on Philips PNX4008 board"
	depends on FB_PNX4008_DUM
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Say Y here to enable support for PNX4008 RGB Framebuffer

config FB_IBM_GXT4500
	tristate "Framebuffer support for IBM GXT4500P adaptor"
	depends on PPC
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Say Y here to enable support for the IBM GXT4500P display
	  adaptor, found on some IBM System P (pSeries) machines.

config FB_PS3
	bool "PS3 GPU framebuffer driver"
	depends on (FB = y) && PS3_PS3AV
	select FB_SYS_FILLRECT
	select FB_SYS_COPYAREA
	select FB_SYS_IMAGEBLIT
	select FB_SYS_FOPS
	---help---
	  Include support for the virtual frame buffer in the PS3 platform.

config FB_PS3_DEFAULT_SIZE_M
	int "PS3 default frame buffer size (in MiB)"
	depends on FB_PS3
	default 18
	---help---
	  This is the default size (in MiB) of the virtual frame buffer in
	  the PS3.
	  The default value can be overridden on the kernel command line
	  using the "ps3fb" option (e.g. "ps3fb=9M");

config FB_XILINX
	tristate "Xilinx frame buffer support"
	depends on FB && XILINX_VIRTEX
	select FB_CFB_FILLRECT
	select FB_CFB_COPYAREA
	select FB_CFB_IMAGEBLIT
	---help---
	  Include support for the Xilinx ML300/ML403 reference design
	  framebuffer. ML300 carries a 640*480 LCD display on the board,
	  ML403 uses a standard DB15 VGA connector.

config FB_VIRTUAL
	tristate "Virtual Frame Buffer support (ONLY FOR TESTING!)"
	depends on FB
	select FB_SYS_FILLRECT
	select FB_SYS_COPYAREA
	select FB_SYS_IMAGEBLIT
	select FB_SYS_FOPS
	---help---
	  This is a `virtual' frame buffer device. It operates on a chunk of
	  unswappable kernel memory instead of on the memory of a graphics
	  board. This means you cannot see any output sent to this frame
	  buffer device, while it does consume precious memory. The main use
	  of this frame buffer device is testing and debugging the frame
	  buffer subsystem. Do NOT enable it for normal systems! To protect
	  the innocent, it has to be enabled explicitly at boot time using the
	  kernel option `video=vfb:'.

	  To compile this driver as a module, choose M here: the
	  module will be called vfb. In order to load it, you must use
	  the vfb_enable=1 option.

	  If unsure, say N.

if VT
	source "drivers/video/console/Kconfig"
endif

if FB || SGI_NEWPORT_CONSOLE
	source "drivers/video/logo/Kconfig"
endif

endmenu