# ALSA ARM drivers

menu "ALSA ARM devices"
	depends on SND!=n && ARM

config SND_SA11XX_UDA1341
	tristate "SA11xx UDA1341TS driver (iPaq H3600)"
	depends on ARCH_SA1100 && SND && L3
	select SND_PCM
	help
	  Say Y here if you have a Compaq iPaq H3x00 handheld computer
	  and want to use its Philips UDA 1341 audio chip.

	  To compile this driver as a module, choose M here: the module
	  will be called snd-sa11xx-uda1341.

config SND_ARMAACI
	tristate "ARM PrimeCell PL041 AC Link support"
	depends on SND && ARM_AMBA
	select SND_PCM
	select SND_AC97_CODEC

config SND_PXA2XX_PCM
	tristate
	select SND_PCM

config SND_PXA2XX_AC97
	tristate "AC97 driver for the Intel PXA2xx chip"
	depends on ARCH_PXA && SND
	select SND_PXA2XX_PCM
	select SND_AC97_CODEC
	help
	  Say Y or M if you want to support any AC97 codec attached to
	  the PXA2xx AC97 interface.

config SND_AT73C213
	tristate "Atmel AT73C213 DAC driver"
	depends on SND && SPI_ATMEL && ARCH_AT91 && AT91_PROGRAMMABLE_CLOCKS
	select SND_PCM
	help
	  Say Y here if you want to use the Atmel AT73C213 external DAC.

config SND_AT91_AC97
	tristate "AC97 Controller driver for SAM926X familly from ATMEL"
	depends on SND && ARCH_AT91
	select SND_PCM
	select SND_AC97_CODEC
	help
	  Say Y or M if you want to support any AC97 codec attached to
	  the SAM926X AC97 Controller.

endmenu