// -*- mode:doc; -*-
// vim: set syntax=asciidoc:

== Coding style

Overall, these coding style rules are here to help you to add new files in
Buildroot or refactor existing ones.

If you slightly modify some existing file, the important thing is
to keep the consistency of the whole file, so you can:

* either follow the potentially deprecated coding style used in this
file,

* or entirely rework it in order to make it comply with these rules.

[[writing-rules-config-in]]

=== +Config.in+ file

+Config.in+ files contain entries for almost anything configurable in
Buildroot.

An entry has the following pattern:

---------------------
config BR2_PACKAGE_LIBFOO
	bool "libfoo"
	depends on BR2_PACKAGE_LIBBAZ
	select BR2_PACKAGE_LIBBAR
	help
	  This is a comment that explains what libfoo is. The help text
	  should be wrapped.

	  http://foosoftware.org/libfoo/
---------------------

* The +bool+, +depends on+, +select+ and +help+ lines are indented
  with one tab.

* The help text itself should be indented with one tab and two
  spaces.

* The help text should be wrapped to fit 72 columns, where tab counts
  for 8, so 62 characters in the text itself.

The +Config.in+ files are the input for the configuration tool
used in Buildroot, which is the regular _Kconfig_. For further
details about the _Kconfig_ language, refer to
http://kernel.org/doc/Documentation/kbuild/kconfig-language.txt[].

[[writing-rules-mk]]

=== The +.mk+ file

* Header: The file starts with a header. It contains the module name,
preferably in lowercase, enclosed between separators made of 80 hashes. A
blank line is mandatory after the header:
+
---------------------
################################################################################
#
# libfoo
#
################################################################################
---------------------
+
* Assignment: use +=+ preceded and followed by one space:
+
---------------------
LIBFOO_VERSION = 1.0
LIBFOO_CONF_OPTS += --without-python-support
---------------------
+
Do not align the +=+ signs.

* Indentation: use tab only:
+
---------------------
define LIBFOO_REMOVE_DOC
	$(RM) -fr $(TARGET_DIR)/usr/share/libfoo/doc \
		$(TARGET_DIR)/usr/share/man/man3/libfoo*
endef
---------------------
+
Note that commands inside a +define+ block should always start with a tab,
so _make_ recognizes them as commands.

* Optional dependency:

** Prefer multi-line syntax.
+
YES:
+
---------------------
ifeq ($(BR2_PACKAGE_PYTHON),y)
LIBFOO_CONF_OPTS += --with-python-support
LIBFOO_DEPENDENCIES += python
else
LIBFOO_CONF_OPTS += --without-python-support
endif
---------------------
+
NO:
+
---------------------
LIBFOO_CONF_OPTS += --with$(if $(BR2_PACKAGE_PYTHON),,out)-python-support
LIBFOO_DEPENDENCIES += $(if $(BR2_PACKAGE_PYTHON),python,)
---------------------

** Keep configure options and dependencies close together.

* Optional hooks: keep hook definition and assignment together in one
  if block.
+
YES:
+
---------------------
ifneq ($(BR2_LIBFOO_INSTALL_DATA),y)
define LIBFOO_REMOVE_DATA
	$(RM) -fr $(TARGET_DIR)/usr/share/libfoo/data
endef
LIBFOO_POST_INSTALL_TARGET_HOOKS += LIBFOO_REMOVE_DATA
endif
---------------------
+
NO:
+
---------------------
define LIBFOO_REMOVE_DATA
	$(RM) -fr $(TARGET_DIR)/usr/share/libfoo/data
endef

ifneq ($(BR2_LIBFOO_INSTALL_DATA),y)
LIBFOO_POST_INSTALL_TARGET_HOOKS += LIBFOO_REMOVE_DATA
endif
---------------------

=== The documentation

The documentation uses the
http://www.methods.co.nz/asciidoc/[asciidoc] format.

For further details about the asciidoc syntax, refer to
http://www.methods.co.nz/asciidoc/userguide.html[].

=== Support scripts

Some scripts in the +support/+ and +utils/+ directories are written in
Python and should follow the
https://www.python.org/dev/peps/pep-0008/[PEP8 Style Guide for Python Code].