2009-10-16  John Dallaway  <john@dallaway.org.uk>

	* cdl/hal_arm_xscale_verde.cdl: Parent under
	CYGPKG_HAL_ARM_XSCALE_CORE.

2004-09-24  Drew Moseley  <drew.moseley@intel.com>

       * src/verde_misc.c: Fix typo in drain-write-buffer command.

2003-07-18  Nick Garnett  <nickg@balti.calivar.com>

	* cdl/hal_arm_xscale_verde.cdl:
        Changed values for CYGNUM_HAL_RTC_NUMERATOR,
        CYGNUM_HAL_RTC_DENOMINATOR and CYGNUM_HAL_RTC_PERIOD to
        "default_value" from "calculated". This makes it easier
        to change these values globally.
        
2003-06-21  Mark Salter  <msalter@redhat.com>

	* src/verde_pci.c (pci_config_setup): Add dev field to PCI-X Type 0
	config cycles. 
	* include/hal_verde.h: Define I2C registers as base+offset.

2003-01-24  Mark Salter  <msalter@redhat.com>

	* include/hal_verde.h: Add some arbitatration unit defines.
	* src/verde_misc.c (_scrub_ecc): Make scrub an atomic operation on
	the bus. Thanks to rickr@mn.rr.com for pointing out the need for
	this.

2002-11-12  Mark Salter  <msalter@redhat.com>

	* include/hal_var_ints.h (CYGNUM_HAL_INTERRUPT_MSG_IBPQ): IRQ 26
	belongs to messaging unit.

2002-09-19  Mark Salter  <msalter@redhat.com>

	* include/hal_verde.h: Remove stuff provided by XScale core package.
	* src/verde_misc.c: Ditto.
	* cdl/hal_arm_xscale_verde.cdl (CYGBLD_HAL_VAR_H): Define.

2002-08-29  Mark Salter  <msalter@redhat.com>

	* include/plf_stub.h: Add HAL_STUB_HW_BREAKPOINT_LIST_SIZE and
	HAL_STUB_HW_WATCHPOINT_LIST_SIZE.

2002-08-12  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl: Remove CYGSEM_REDBOOT_ARM_LINUX_BOOT
	requirement.

2002-05-28  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl: Fix linux exec address test.

	* include/hal_verde.h (CYGARC_HAL_MMU_OFF): XScale has
	special requirements for turning off MMU.

2002-05-24  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl: Remove implement of
	CYGINT_HAL_VIRTUAL_VECTOR_COMM_BAUD_SUPPORT since platforms should
	define whether baud rate changes are possible.

2002-04-01  Rory Bolt  <rorybolt@pacbell.net>

	* include/hal_var_ints.h: Fix definition for DMA1_ERR.

2002-02-25  Mark Salter  <msalter@redhat.com>

	* src/verde_misc.c: Timer source clock is always exactly 200MHz.

2002-02-22  Mark Salter  <msalter@redhat.com>

	* src/verde_misc.c: Fix hw watch/break support.

2002-02-20  Mark Salter  <msalter@redhat.com>

	* include/plf_stub.h: Add HW watchpoint/breakpoint support.
	* src/verde_misc.c: Ditto.

2002-02-19  Mark Salter  <msalter@redhat.com>

	* src/verde_misc.c (hal_hardware_init): Initialize debug unit to
	sane state.

2002-01-31  Mark Salter  <msalter@redhat.com>

	* src/verde_pci.c: New file. PCI support common to verde.
	* cdl/hal_arm_xscale_verde.cdl: Add verde_pci.c to compile list.
	* include/var_io.h: Move HAL_PCI_CFG_* macros from plf_io.h
	(CYGARC_PHYSICAL_ADDRESS): Fix conversion.

2002-01-30  Mark Salter  <msalter@redhat.com>

	* src/verde_misc.c (hal_delay_us): Fix delay calculation.

2002-01-29  Jesper Skov  <jskov@redhat.com>

	* include/var_io.h (CYGARC_PHYSICAL_ADDRESS): Added.

	* cdl/hal_arm_xscale_verde.cdl: Use common ARM linux exec
	command.
	* src/redboot_linux_exec.c: Removed.

2002-01-28  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl: Declare var_io.h

	* include/var_io.h: Added.

	* src/verde_misc.c: Don't include CYGBLD_HAL_PLATFORM_IO_H.

	* include/hal_cache.h: Include hal_io.h

2002-01-24  Nick Garnett  <nickg@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl: Removed CYGHWR_HAL_ARM_VERDE_P_CLK
	and CYGHWR_HAL_ARM_VERDE_BUS_CLK options in favour of a more
	dynamic determination of the P_CLK value. CYGNUM_HAL_RTC_PERIOD is
	now a simple number of microseconds which is converted to the
	actual clock value in the HAL.

	* src/verde_misc.c: Rearranged clock code to make use of
	dynamically determined P_CLK value to set timer value.

2002-01-23  Mark Salter  <msalter@redhat.com>

	* include/hal_verde.h: Add PCSR bit defines.

	* include/hal_var_ints.h (HAL_PLATFORM_RESET): Use HW feature to
	perform reset.

2002-01-23  Nick Garnett  <nickg@redhat.com>

	* cdl/hal_arm_xscale_verde.cdl:
	Added CYGHWR_HAL_ARM_VERDE_P_CLK, which defines the external clock
	frequency applied to the Verde chip. All other CPU frequencies are
	derived from this.
	Added CYGHWR_HAL_ARM_VERDE_BUS_CLK which calculates the internal
	bus clock from the P_CLK value.
	Rewrote calculation for CYGNUM_HAL_RTC_PERIOD to derive the period
	from the bus clock and CYGNUM_HAL_RTC_DENOMINATOR.

	* src/verde_misc.c:
	Reorganized hal_IRQ_handler() to do the right thing.
	Added test to hal_interrupt_acknowledge() to acknowledge timer
	interrupts. Also removed misleading comment from hal_clock_reset().

	* include/hal_verde.h: Added TISR_WRITE().

2002-01-21  Mark Salter  <msalter@redhat.com>

	* include/hal_verde.h: Add definitions for ATU, I2C, etc.

	* include/hal_cache.h: Turn write buffer coalescing on and off
	along with Dcache.

2002-01-18  Hugo Tyson  <hmt@redhat.com>

	* include/hal_var_ints.h (HAL_CLOCK_REINITIALIZE): New macro
        which calls the below, also a prototype for it.

	* src/verde_misc.c (hal_clock_reinitialize): New routine to
        reset the clock to a different frequency.  This is for GPROF type
        profiling use only; not general purpose eCos usage.
	
2002-01-09  Mark Salter  <msalter@redhat.com>

	* src/verde_misc.c: Add MCU ISR handler for ECC scrubbing.

	* include/hal_verde.h (MCU_MCISR): Define.

	* include/hal_cache.h (HAL_DCACHE_SYNC): Use platform defined
	constant instead of hardcoded flush area base.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================