2011-02-03  Alan Bowman  <alan.bowman@datong.co.uk>

	* include/var_io.h: Fix CYGHWR_HAL_STM32_RCC_CFGR_PPRE2_*
	definitions. [ Bugzilla 1001137 ]

2011-01-21  Ilija Kocho  <ilijak@siva.com.mk>

	* src/stm32_misc.c (hal_start_clocks): Added optional calculation of
	hal_cortexm_systick_clock when 'internal' clock source is selected.

2011-01-13  John Dallaway  <john@dallaway.org.uk>

	* src/stm32_misc.c: Implement a profiling timer on TIM2.
	* cdl/hal_cortexm_stm32.cdl: Add CDL option to enable the profiling
	timer.

2011-01-13  Nick Garnett  <nickg@ecoscentric.com>

	* src/stm32_misc.c (hal_start_clocks): Correct bit clear operation
	when disabling external clock.

2009-10-26  Ross Younger  <wry@ecoscentric.com>

	* include/var_io.h: Minor corrections to the FSMC register defs.

2009-08-10  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/var_io.h: Added more register definitions for FSMC

2009-04-17  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/hal_diag.c (hal_stm32_serial_getc_timeout): Fix for higher
	baudrates. The original version lost bytes due to the long
	timeout.

2009-02-27  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/var_io.h:
	Add mask for CYGHWR_HAL_STM32_RCC_CFGR_ADCPRE.
	Fixed CYGHWR_HAL_STM32_RTC_CRL_ALRF.
	Add register definitions for ADC.
	Add additional timer registers.
	* src/stm32_mis.c:
	Moved system clock initialization into it's own function, so it can
	be called after wakeup from sleep modes.
	Added hal_stm32_timer_clock() to get current clock of timers.

2009-02-10  Chris Holgate  <chris@zynaptic.com>

	* include/var_io.h: Add mask for CYGHWR_HAL_STM32_AFIO_MAPR_SWJ.

2009-02-04  Nick Garnett  <nickg@ecoscentric.com>

	* include/var_intr.h: Various fixes to allow external interrupts
	to work.

	* include/var_io.h: Add AFIO, DMA, SPI and USB definitions.

	* src/stm32_misc.c (hal_stm32_gpio_set): Refetch bit number for
	setting pullup/down.

2008-11-24  Nick Garnett  <nickg@ecoscentric.com>

	* include/var_intr.h (CYGNUM_HAL_INTERRUPT_DMA1_CHX): Rename DMA0
	to DMA1 to match ST's numbering elsewhere.

	* include/var_io.h (CYGHWR_HAL_STM32_GPIO_CFG): Remove PULLUP bit
	from mask. Previous addition was incorrect.

2008-11-24  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/var_io.h: Corrected capitalisation.
	
2008-11-12  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/var_io.h: Changed CYGHWR_HAL_STM32_BD_UNPROTECT to
	CYGHWR_HAL_STM32_BD_PROTECT, inverting the argument.
	* src/stm32_misc.c: Changed hal_stm32_bd_unprotect() to
	hal_stm32_bd_protect(), inverting the argument.

2008-11-11  Nick Garnett  <nickg@ecoscentric.com>

	* include/var_io.h: Add power control definitions.

	* src/stm32_misc.c (hal_stm32_bd_unprotect): Add this function to
	control backup domain write protection.

2008-10-14  Nick Garnett  <nickg@ecoscentric.com>

	* tests/timers.c: Add ifdefs to avoid compiling tests when not all
	packages or components are present.

2008-10-10  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_cortexm_stm32.cdl: Only build tests if the kernel is present.

	* include/var_io.h (CYGHWR_HAL_STM32_GPIO_CFG): Add PULLUP bit to mask.

	* tests/timers.c (timers_test): Terminate with PASS_FINISH rather
	than just FINISH.

2008-10-08  Nick Garnett  <nickg@ecoscentric.com>

	* include/var_intr.h (CYGNUM_HAL_ISR_MAX, CYGNUM_HAL_VSR_MAX): Fix
	definition of these values.

	* tests/timers.c: Fix to run for maximum duration of 2 minutes.

2008-10-06  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_cortexm_stm32.cdl:
	* include/variant.inc:
	* include/var_arch.h:
	* include/var_intr.h:
	* include/var_io.h:
	* include/hal_cache.h:
	* include/hal_diag.h:
	* include/plf_stub.h:
	* src/hal_diag.c:
	* src/stm32_misc.c:
	New package -- ST STM32 variant HAL.	
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2008, 2009, 2011 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================