2011-01-02  Sergei Gavrikov  <sergei.gavrikov@gmail.com>

	* cdl/hal_sh_sh2.cdl: Eliminate some warnings. [ Bugzilla
	1001083 ]

2004-04-22  Jani Monoses <jani@iv.ro>

	 * cdl/hal_sh_sh2.cdl :
	 Invoke tail with stricter syntax that works in latest coreutils. 

2002-08-06  Gary Thomas  <gary@chez-thomas.org>
2002-08-06  Motoya Kurotsu <kurotsu@allied-telesis.co.jp>	

	* src/sh2_scif.c: 
	* src/sh2_sci.c: I/O channel data can't be constant - contains
	timeout information which can be changed.

2002-05-22  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Select variant 7044 by default.

2002-05-08  Jesper Skov  <jskov@redhat.com>

	* src/sh2_sci.c: Register renaming.
	* src/sh2_scif.c: Register renaming.

	* include/sh2_scif.h (_REG_SCSSR): Define.

	* include/mod_regs_ser.h: Register renaming. SCI registers now
	contain _SCI_, SCIF registers contain _SCIF_.

2002-04-30  Jesper Skov  <jskov@redhat.com>

	* include/var_intr.h: Renumber the 7044 vectors to get rid of the
	gaps. CYGHWR_HAL_SH_SH2_CUSTOM_INTERRUPT_LAYOUT now takes care of
	the translation from HW interrupt vectors to the eCos vector
	numbers.

2002-04-24  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_adc.h: Added.

	* include/var_regs.h: Include adc header.

	* include/mod_7044.h (CYGARC_SH_MOD_ADC): Added.

2002-04-22  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_wdt.h (CYGARC_REG_RSTCSR_W_RSTx_MAGIC,
	CYGARC_REG_RSTCSR_W_WOVF_MAGIC): set 5 lsb.
	* include/mod_regs_wdt_2.h (CYGARC_REG_RSTCSR_W_RSTx_MAGIC,
	CYGARC_REG_RSTCSR_W_WOVF_MAGIC): set 5 lsb.
	Also define CYGARC_REG_WTCNT_W.

	* include/var_intr.h (HAL_PLATFORM_RESET): Fixed. Set WTIT flag.

	* src/var_misc.c (hal_interrupt_mask, hal_interrupt_unmask): Add
	range for INTC=2 and error for undefined to catch such a bobo
	easier next time.

	* include/var_intr.h: Fix access size typos.

	* include/sh2_sci.h: Fix offsets.

	* include/mod_regs_pfc_2.h (CYGARC_REG_PEDR): Added.

2002-04-18  Jesper Skov  <jskov@redhat.com>

	* include/var_regs.h: Include BSC header according to type.
	* include/mod_regs_pfc_2.h (CYGARC_REG_PADRH, CYGARC_REG_PADRL): Added.
	* include/mod_regs_bsc_2.h: Added.
	* include/mod_7044.h: BSC Type 2.
	* include/mod_7615.h: BSC Type 1.

	* include/variant.inc: Only disable UBC if type defined. Fix INTC
	type 1/2 mixup.
	* include/var_regs.h: Include watchdog header according to type.
	* include/mod_regs_wdt_2.h: Added.
	* include/mod_7615.h: WDT type 1.
	* include/mod_7044.h: WDT type 2.

	* src/var_misc.c (cyg_var_enable_caches): Only set mode if the
	feature is present.
	* include/variant.inc: CYGARC_REG_CCR is 16bit in type 2 CAC
	module.
	* src/variant.S: Support for type 2 cache.
	* include/var_regs.h: Include cache header according to type.
	* include/mod_7615.h (CYGARC_SH_MOD_CAC): Type 1.
	* include/var_cache.h: Support for type 2.
	* include/mod_regs_cac_2.h: Added.
	* include/mod_7044.h (CYGARC_SH_MOD_CAC): Type 2.
	Also define cache array addresses.

	* src/var_misc.c (hal_interrupt_update_level): 7044 support.

	* include/var_intr.h: Fall-back
	CYGPRI_HAL_INTERRUPT_UPDATE_LEVEL_PLF is variant specific.

2002-04-17  Jesper Skov  <jskov@redhat.com>

	* src/var_mk_defs.c: Adjustment for 7044.
	* src/variant.S: Same.

	* src/var_misc.c: Most of the functions update to handle INTC type
	2. Some still to do. Added hal_delay_us for CMT.

	* include/variant.inc: Clear CMT on init, and clear INTC type 2
	registers.

	* include/var_regs.h: Allow different headers for INT and
	PFC. Also include CMT header.

	* include/var_intr.h: Some adjustments for 7044, and vectors for
	it. Also define CMT style RTC support.

	* include/sh2_sci.h: Removed error.
	* src/sh2_sci.c: Same.

	* include/mod_regs_intc_2.h: Added.
	* include/mod_regs_pfc_2.h: Added.
	* include/mod_regs_cmt.h: Added.

	* include/mod_regs_cpg.h: Handle type 2.

	* include/mod_7044.h: Enable more modules. No cache windows in
	memory map.

	* cdl/hal_sh_sh2.cdl: Added 7044 clock options.
	Added 7044 variant option.	

	* include/mod_regs_ser.h: Fixed SCI definitions.

	* include/mod_7044.h: Added.

2002-03-07  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_eth.h (CYGARC_REG_CNDCR): Added more
	definitions.

2002-03-06  Jesper Skov  <jskov@redhat.com>

	* src/sh2_scif.c: Added cyg_hal_plf_scif_sync_rxtx that allows
	switching mode at runtime. Changed code to respect setting.
	* include/sh2_scif.h: Same.

	* cdl/hal_sh_sh2.cdl: Added CYGHWR_HAL_SH_SH2_SCIF_ASYNC_RXTX to
	control RX/TX enabling. In async mode (when set), only one of TX
	or RX will be set at the same time.

2002-03-01  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Added 
	CYGHWR_HAL_SH_SH2_SCIF_IRDA_TXRX_COMPENSATION option to control
	IrDA TX/RX kludge.
	* src/sh2_scif.c: Use above option. Don't force 9600 baud in IrDA
	mode.

2002-02-22  Jesper Skov  <jskov@redhat.com>

	* src/sh2_scif.c (cyg_hal_plf_scif_putc): In IrDA mode, eat the
	spurious received character after TX has completed.

2002-02-21  Jesper Skov  <jskov@redhat.com>

	* src/sh2_scif.c: Force 9600 baud for IrDA mode
	initialization. Disable transmitter when not used in IrDA
	mode. Check transmitter state instead of FIFO count for
	determining when to cease transmission.

2002-02-20  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_eth.h: More definitions.

2002-02-19  Jesper Skov  <jskov@redhat.com>

	* include/var_regs.h: Include ethernet definitions.

	* include/mod_7615.h: Has ethernet module.

	* include/mod_regs_eth.h: Added more definitions.

	* include/mod_regs_wdt.h: Added some more definitions.

	* include/var_intr.h (HAL_PLATFORM_RESET): Defined (doesn't work
	though).

	* include/mod_7615.h: Disable UBC for now since software emulation
	works just fine.

2002-02-12  Jesper Skov  <jskov@redhat.com>

	* include/var_intr.h: Added HAL_CLOCK_VAR_INITIALIZE which does
	partial FRT initialization so it can be used from
	hal_delay_us. Updated other timer macros.
	(HAL_CLOCK_READ): Fix typo.

	* include/mod_regs_frt.h: Renamed 16bit access registers.

	* src/var_misc.c (hal_delay_us): Fixed.
	Call HAL_CLOCK_VAR_INITIALIZE from hal_variant_init.

	* include/mod_regs_bsc.h: Changed register locations and made
	flags be 32bit constants.

2002-02-07  Jesper Skov  <jskov@redhat.com>

	* src/var_misc.c (hal_delay_us): Fixed typo. Increasy dummy loop
	since the typo didn't fix the problem.

	* include/mod_regs_pcm.h: Added.

	* include/var_regs.h: Include PCM.

	* include/mod_7615.h: Added DMA and PCM defs.

2002-02-06  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_frt.h: Fix comment.

2002-02-05  Jesper Skov  <jskov@redhat.com>

	* src/sh2_scif.c: Set SC2SSR in initialization. Clear errors in
	getc function.

	* include/mod_regs_cpg.h (CYGARC_REG_FMR_INIT): Define as value
	provided by platform.

	* cdl/hal_sh_sh2.cdl: Variant is big-endian only.

2002-01-30  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_eth.h: Added.

	* include/mod_regs_pfc.h: Updated for SH7615.

2002-01-22  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Set as type1 clock module.

	* src/sh2_scif.c: Added IrDA mode support.
	* include/sh2_scif.h: Same.

	* include/mod_regs_dma.h: Updated for SH7615.

	* include/mod_regs_ser.h: Fixed a typo.

2002-01-18  Jesper Skov  <jskov@redhat.com>

	* src/sh2_sci.c: Added #error about not being updated.
	* src/sh2_sci.h: Updated for SH2 naming.
	* src/sh2_scif.h: Updated for SH2 naming, and registers.
	* src/sh2_scif.c: Updated for changed register names.
	* include/mod_regs_ser.h: Updated SCIF register names/values.

	* src/var_misc.c (hal_delay_us): Added.

	* include/variant.inc: Fixed some bade conditional code.

	* include/var_intr.h (HAL_CLOCK_INITIALIZE): Fix typos. Guard
	against too large period.

	* include/mod_regs_ubc.h: Updated to match SH7615 (type 2).

	* include/mod_7615.h (CYGARC_SH_MOD_UBC): Is type 2.

2002-01-17  Jesper Skov  <jskov@redhat.com>

	* include/mod_regs_ubc.h: Partially updated.

	* include/mod_regs_wdt.h: Added.
	* include/var_regs.h: Include WDT header.

	* src/var_misc.c (hal_interrupt_set_vectors): Updated vector
	names.

	* src/variant.S (cyg_hal_ILVL_table): Changed for SH2.

	* src/var_mk_defs.c: Added more interrupt defs.

	* include/var_intr.h (CYGPRI_HAL_INTERRUPT_UPDATE_LEVEL_PLF):
	Ignore LVLs 0-3 since they overlap with IRQs
	0-3. hal_interrupt_update_level contains code to handle according
	to configuration.

	* include/mod_regs_intc.h: Added def.

	* src/var_misc.c: Interrupt configury updated for 7615.

	* include/var_intr.h: Add module identifier to vector names. Set
	RTC vector.

2002-01-16  Jesper Skov  <jskov@redhat.com>

	* src/var_mk_defs.c: Removed some defs.

	* src/var_misc.c: Cache init fixed and compiler warnings + typos
	fixed.

	* src/sh2_scif.c: Renamed for SH2.
	* src/sh2_sci.c: Same.

	* include/var_regs.h: TMU header inclusion removed.

	* include/var_intr.h: Shift vectors down one (to make room for NMI
	as vector 0).

	* include/mod_regs_ser.h: Protect SCI defs by CYGARC_SH_MOD_SCI.

	* include/mod_regs_cpg.h: No magic here - CDL provides a hardwired
	constant to use.

	* include/mod_regs_bsc.h: Updated to match SH7615.

	* include/mod_7615.h (CYGARC_SH_MOD_BCN): Is type 2.

	* cdl/hal_sh_sh2.cdl: Added CYGHWR_HAL_SH_RTC_PRESCALE.

	* include/mod_regs_frt.h: Added.

	* include/var_intr.h: Added support for eCos RTC driven by FRT module.

	* include/mod_7615.h (CYGARC_SH_MOD_FRT): Added.
	* include/var_regs.h: Include FRT header. Removed RTC header inclusion.

	* src/var_misc.c (hal_interrupt_set_vectors): Set VCRx registers
	to map the module interrupt sources to specific HWR_EXC vectors.

	* include/var_intr.h: Added SH7615 vectors.

	* cdl/hal_sh_sh2.cdl: Select INTR model header.

	* include/mod_regs_intc.h: Added stuff for 7615 INTC.

	* include/mod_7615.h: Does update the IP on exception. All modules
	are type 1.

2002-01-14  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Added exception model header definitions.

	* include/variant.inc: Fixed assembler warning. Change CYG_SR.

2002-01-11  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Changed the clock setup some.

2002-01-09  Jesper Skov  <jskov@redhat.com>

	* cdl/hal_sh_sh2.cdl: Changed to match SH2 caching details.
	* src/var_misc.c: Same.
	* include/var_cache.h: Same.
	* src/variant.S: Same.

	* include/mod_7615.h: Added some 7615 details.

	Cloned from SH3 HAL.
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================