2010-11-11  Sergei Gavrikov  <sergei.gavrikov@gmail.com>

	* cdl/libm.cdl (CYGPKG_LIBM_CFLAGS_ADD): Add a set of parentheses
	around 'if-then-else' expression, simplified evaluated expression.

2010-05-15  Jonathan Larmour  <jifl@jifvik.org>

	* cdl/libm.cdl (CYGPKG_LIBM_CFLAGS_ADD): Compile with
	-fno-strict-aliasing to avoid miscompilation. Workaround for a more
	fundamental problem with CYG_LIBM_HI/LO.

2008-11-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/libm.cdl: Rename X_TLOSS CDL option to match normal convention.

2007-09-04  Stephen Finney  <shf@pfinc.com>
2007-09-04  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/misc/infconst.c: Declare infinity byte order as dependent on
	double byte order, not integer.
	Fixes bug #1000448.

2004-04-14  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/double/ieee754-core/e_cosh.c (__ieee754_cosh): 
	* src/double/ieee754-core/e_sinh.c (__ieee754_sinh): Make use of
	the CYG_LIBM_LO() macro which does not generate a compiler warning.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/libm.cdl: Fix doc link.

2001-09-28  Jesper Skov  <jskov@redhat.com>

	* src/double/portable-api/s_expm1.c (expm1): Init c before it's used.

2001-07-20  Jonathan Larmour  <jlarmour@redhat.com>

	* src/double/portable-api/s_expm1.c: Reimport from newlib
	* src/double/ieee754-core/e_pow.c: Ditto.
	* src/mathincl/fdlibm.h: Define macros and types required for
	newlib versions	of libm files.

2001-04-25  Bart Veer  <bartv@redhat.com>

	* cdl/libm.cdl:
	Ensure -ffloat-store is also used for the updated synthetic target
	when running on x86 hardware.

2000-09-11  Jonathan Larmour  <jlarmour@redhat.com>

	* src/misc/infconst.c: Revert below two changes - the gcc problem
	that provoked it is now fixed.

2000-09-01  Jonathan Larmour  <jlarmour@redhat.com>

	* src/misc/infconst.c: Silence warning about number of brackets

2000-08-31  Jonathan Larmour  <jlarmour@redhat.com>

	* include/math.h: Declare cyg_libm_infinity as an array type for correct
	relocations
	* src/misc/infconst.c: Define it likewise

2000-05-30  Jesper Skov  <jskov@redhat.com>

	* include/sys/ieeefp.h: Undo below change.

2000-05-26  Jesper Skov  <jskov@redhat.com>

	* include/sys/ieeefp.h: Support FPU double-LE layout in BE mode.
	Fix paste bug.

2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/vectors/vector_support.h:
	Update startup configury to reflect changes in libc startup. 
	Use default stacksize of CYGNUM_HAL_STACK_SIZE_TYPICAL rather than 32K

2000-03-28  John Dallaway  <jld@cygnus.co.uk>

	* cdl/libm.cdl:

	Adjust documentation URLs.

2000-03-16  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/libm.cdl (CYGPKG_LIBM_CFLAGS_ADD): Add -ffloat-store for i386
	targets. The math library implementation relies on accurate IEEE FP.

2000-01-31 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/*.cdl:

  Adjust help URLs in line with new doc layout.
  
2000-01-28 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/*.cdl:

  Adjust help URLs in line with new doc layout.
  
2000-01-28  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/libm.cdl: Don't need to compile with -O1 any more

2000-01-19  Hugo Tyson  <hmt@cygnus.co.uk>

	* cdl/*.cdl: Add descriptions to a number of options &c which were
	lacking same, also tidied up other typos as noticed en passant.

1999-11-23  Hugo Tyson  <hmt@cygnus.co.uk>

	* include/pkgconf/libm.h: Cooperate with permtest combo10 setting
	an intermediate variable CYGNUM_LIBM_COMPAT_DEFAULT directly.

1999-11-03  John Dallaway  <jld@cygnus.co.uk>

	* cdl/libm.cdl: Define tests.

1999-10-18  John Dallaway  <jld@cygnus.co.uk>

	* cdl/libm.cdl:
	Parent CYGPKG_LIBM_CFLAGS_ADD and CYGPKG_LIBM_CFLAGS_REMOVE
        under a CDL component.

1999-10-15  John Dallaway  <jld@cygnus.co.uk>

	* cdl/libm.cdl:
	Define CYGPKG_LIBM_CFLAGS_ADD and CYGPKG_LIBM_CFLAGS_REMOVE.

1999-10-07  John Dallaway  <jld@cygnus.co.uk>

	* cdl/compat.cdl: Specify radio buttons using CDL interfaces.

1999-08-24  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: Optimize by default everywhere, except when compiling
	e_pow.c, in which case use -fno-schedule-insns

1999-08-17  John Dallaway  <jld@cygnus.co.uk>

	* cdl/compat.cdl:

	Implement radio buttons using "FIXME radio" hack in
	description field for now.

1999-08-14  John Dallaway  <jld@cygnus.co.uk>

	* cdl/compat.cdl:
	Change CYGNUM_LIBM_COMPATIBILITY flavor to 'booldata'.

1999-08-12  John Dallaway  <jld@cygnus.co.uk>

	* cdl/libm.cdl, cdl/compat.cdl:
	Take advantage of MACRONAME_ENUMVAL macros output by CDL.

1999-06-17  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: Disable optimization completely until CR 100802 is
	fixed

1999-06-07  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mathincl/fdlibm.h: Fix for alias problem
	Fix for PR 19698
	* src/PKGconf.mak: workaround no longer needed

1999-06-04  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: 
	Only use -fno-strict-aliasing if we have enough a recent toolchain
	Default is that we have
	
1999-06-03  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: 
	Finally found the option to do the right workaround:
	-fno-strict-aliasing

1999-06-02  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak (SPECIAL_FLAGS): Don't use -fschedule-insns[2] on
	mn10300

1999-05-27  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak (SPECIAL_FLAGS): Add workaround flags for new
	toolchains for all targets

1999-05-24  Jesper Skov  <jskov@cygnus.co.uk>

	* src/PKGconf.mak: Same workaround for sh.

1999-05-19  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: Make below workaround be the other way around by
	using -O1 and adding more explicit -O2 optimizations, just so we
	don't lose very many optimizations. This is for sparclite

1999-05-19  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: Make below workaround be the other way around by
	using -O1 and adding more explicit -O2 optimizations, just so we
	don't lose very many optimizations. This is for ARM

1999-05-18  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: For the sparclite, prevent insn scheduling -
	workaround for PR 19698

1999-05-18  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: For the ARM, change from -O1 to just prevent insn
	scheduling - workaround for PR 19698

1999-04-15  John Dallaway  <jld@cygnus.co.uk>

	* include/pkgconf/libm.h: Tidy display string capitalization.

1999-04-07  Jesper Skov  <jskov@cygnus.co.uk>
        PR 19442
	* tests/vectors/vector_support.h: Make an occasional chirp to keep
	the testing infra interested.

1999-04-06  Gary Thomas  <gthomas@cygnus.co.uk>

	* src/PKGconf.mak: More brute-force fix for ARM compiler
	problems - PR 19772

1999-03-31  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: Remove unnecessary define
	Fix for PR 19423

1999-03-29  Gary Thomas  <gthomas@cygnus.co.uk>

	* src/PKGconf.mak: Add special compile options to work around ARM
	compiler bugs.

1999-02-09  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mathincl/fdlibm.h: 
	Change definition of CYG_LIBM_HI/CYG_LIBM_LO to use inline
	function
	Fix for PR 18859

1999-01-28  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/signgam.cxx: 
	* src/misc/compatmode.cxx: 
	Include <pkgconf/kernel.h> if we use kernel header files

1999-01-21  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (doTestVec): Makes more
	sense to output vector number than array index

	* src/double/portable-api/s_ceil.c: Fix comment s/+inf/-inf/

1999-01-20  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (doTestVec): 
	Add output to let you know which vectors failed

1999-01-12  Gary Thomas  <gthomas@cygnus.co.uk>

	* src/mathincl/fdlibm.h: 
	* include/sys/ieeefp.h: Add different structure layouts for
	machines that have doubles that aren't pure big/little endian.

Fri Oct 23 19:27:04 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (START_TEST): 
	Ensure that dummy START_TEST (the one used when the test should
	*not* be run) does have a reference to the test function. And
	make sure that there is a default one if there's no C API

	* src/mathincl/fdlibm.h: 
	Add matherr() prototype if no namespace pollution

	Fixes for PR 17972

1998-10-22  Jesper Skov  <jskov@cygnus.co.uk>
        PR 17925

	* include/pkgconf/libm.h: 
	* src/misc/matherr.c:
	Removed the CYGFUN_LIBM_matherr config. The function is already
	weakly defined so shouldn't need to be configured out.

1998-10-19  Mark Galassi  <rosalia@cygnus.com>

	* include/pkgconf/libm.h: updated the doc URL

Thu Oct 15 21:36:12 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/compatmode.cxx, src/misc/signgam.cxx:
	Only include kernel headers if we want thread-safe operation
	Required for PR 17229

Wed Oct 14 17:24:46 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Make CYGPKG_LIBM_COMPATIBILITY_DEFAULT require CYGPKG_LIBC
	rather than all of libm, and put a check (with #error) that
	this is the case

	* src/double/ieee754-api/w_scalb.c:
	Only include errno.h if we aren't IEEE-only

	* src/double/portable-api/s_ldexp.c, src/misc/standard.c:
	Make the error checking in s_ldexp.c more like every other libm
	sources by putting the actual error handling into standard.c.
	The error handling is just like scalb

	* tests/vectors/acos.c, tests/vectors/asin.c,
	  tests/vectors/atan.c, tests/vectors/atan2.c,
 	  tests/vectors/ceil.c, tests/vectors/cos.c, tests/vectors/cosh.c,
 	  tests/vectors/exp.c, tests/vectors/fabs.c,
 	  tests/vectors/floor.c, tests/vectors/fmod.c,
 	  tests/vectors/frexp.c, tests/vectors/ldexp.c,
 	  tests/vectors/log.c, tests/vectors/log10.c,
 	  tests/vectors/modf.c, tests/vectors/pow.c, tests/vectors/sin.c,
 	  tests/vectors/sinh.c, tests/vectors/sqrt.c, tests/vectors/tan.c,
 	  tests/vectors/tanh.c:
	Remove unnecessary include of <errno.h>

	* tests/vectors/vector_support.h:
	Only include errno.h if we aren't IEEE-only.
	If we don't have Cyg_ErrNo, just use a cyg_int32 instead, to
	make sure that the fields are still correct for the input
	test vector.
	In doTestVec(), before checking errno, check if we're
	in IEEE mode (either compiled in or set at runtime) because if
	so, and errno is set in the errno field of the input test
	vector, then we have to skip this, since we can't validate the
	output.
	In all modes, if errno is set in the input test vector, don't
	bother checking the actual values

	All of the above changes are for PR 17503
	
	* tests/vectors/pow.c:
	Remove requirement of being in POSIX mode, as the change to
	vector_support.h should make this work better now.


Sun Sep 27 20:46:09 1998  David Moore  <dsm@keema.cygnus.co.uk>

	* include/pkgconf/libm.h:
	PR 17515: Corrected notcdl doc string.

1998-09-26  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/libm.h:
	PR 17503: there are uses of errno in a couple of places in libm,
	and errno will only be available if the C library is present.
	Therefore libm requires libc.
	

Fri Sep 25 19:00:35 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/compatmode.cxx: 
	Make sure CYGNUM_LIBM_COMPATMODE_TRACE_LEVEL is defined before
	we attempt tracing, otherwise set trace level to 0 i.e. never

	* src/misc/signgam.cxx: 
	Make sure CYGNUM_LIBM_SIGNGAM_TRACE_LEVEL is defined before
	we attempt tracing, otherwise set trace level to 0 i.e. never
	Fix for PR 17478

	* include/pkgconf/libm.h: 
	Define trace levels only if parent CYGPKG_LIBM_TRACE is defined
	for consistency with Configuration Tool

Fri Sep 25 18:25:02 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Only check valid compatibility setting if we aren't IEEE-only
	mode
	Fix for PR 17481

Fri Sep 25 18:13:24 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mathincl/fdlibm.h: 
	* src/double/ieee754-core/e_scalb.c: 
	* src/double/ieee754-api/w_scalb.c: 
	Use CYGFUN_LIBM_SVID3_scalb for whether 2nd arg of scalb is
	double or int, rather than _SCALB_INT.
	Fix for PR 17479

Wed Sep 23 08:07:48 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/pow.c (test): 
	Make pow test conditional on being in POSIX compatibility mode.
	This is the only mode that can set errno correctly, in
	relation to what the tests expect.
	Fix for PR 16933

1998-09-20  Mark Galassi  <rosalia@cygnus.com>

	* include/pkgconf/libm.h: updated CDL doc strings.

Thu Sep 17 17:10:47 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (checkErrorAcceptable): 
	Move check for signed-ness after all of the special cases
	Fix for PR 16933

Tue Sep 15 19:26:32 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Updated descriptions and a few other minor things after review

1998-09-11  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/libm.h:
	Sorting out dependencies for error package.

Fri Sep  4 14:20:04 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Fix thread-safe modes "requires" lines not to be associated
	with the dummy parent package, but with the options themselves.
	Also we don't need "requires CYGPKG_KERNEL" if we already require
	a particular kernel option anyway.

Thu Sep  3 09:50:20 1998  Tim Goodwin  <tgoodwin@cygnus.co.uk>

	* tests/vectors/vector_support.h
	Change to cyg_thread_create() interface.

Wed Sep  2 14:41:54 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Add default define for CYGPKG_LIBM_COMPATIBILITY_DEFAULT,
	and shorten some display texts

Wed Sep  2 13:15:43 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/double/ieee754-core/e_pow.c: 
	Fix bug for when x is negative and y isn't an integer. A CYGNUS
	LOCAL change got it wrong when casting a signed integer to
	unsigned before right shifting.
	
	Reformat for 76 columns

	* src/double/ieee754-api/w_pow.c: 
	Reformat for 76 columns
	

Wed Sep  2 12:30:11 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Default tracing to off
	Reformat for 76 columns

	* tests/vectors/vector_support.h: 
	Align '{'s and "verbs" on the same line. Tidy to 76 columns

Mon Aug 31 13:38:25 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Require infra tracing support to allow tracing

1998-08-28  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/libm.h:
	* src/misc/compatmode.cxx, src/misc/signgam.cxx:
	* tests/vectors/vector_support.h

	Updated for new kernel configuration option symbol names

Fri Aug 28 09:07:07 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h: 
	Change START_TEST macro, adjust config options and add
	cyg_package_start() to get tests working correctly with new entry
	point mechanism, including cyg_iso_c_start() if available

Wed Aug 26 20:25:36 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Remove #define CYGPKG_LIBM is that is meant to live in
	<pkgconf/system.h> after all


Wed Aug 26 19:38:54 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	More fixes to CDL stuff to make it work better, and look better on
	the screen

Tue Aug 25 20:23:25 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Make some fixes after running the ConfigTool

Tue Aug 25 16:59:11 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Turns out the nesting wasn't quite right. Correct it, and replace
	the "not" prefix on CFG_DATA, which slipped in to the previous change.

Tue Aug 25 16:53:03 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Ensure there is a default compatibility mode and fix the
	ifdef nesting for the compat modes

Tue Aug 25 15:24:51 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Tidy up CDL stuff prior to checking if it all actually works!

Tue Aug 25 05:17:55 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h: 
	Do a first pass of CDLification of configuration data

	* include/pkgconf/libm.h, src/misc/matherr.c: 
	Rename CYGFUN_LIBC_matherr to CYGFUN_LIBM_matherr

Wed Aug 19 19:35:16 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/acos.c, tests/vectors/cosh.c, tests/vectors/ldexp.c,
	  tests/vectors/sinh.c, tests/vectors/asin.c, tests/vectors/exp.c,
	  tests/vectors/log.c, tests/vectors/sqrt.c, tests/vectors/atan.c,
   	  tests/vectors/fabs.c, tests/vectors/log10.c, tests/vectors/tan.c,
	  tests/vectors/atan2.c, tests/vectors/floor.c, tests/vectors/modf.c,
   	  tests/vectors/tanh.c, tests/vectors/ceil.c, tests/vectors/fmod.c,
   	  tests/vectors/pow.c, tests/vectors/cos.c, tests/vectors/frexp.c,
  	  tests/vectors/sin.c

	* tests/vectors/vector_support.h (doTestVec): 
	Remove "register" on variable

Wed Aug 19 18:59:47 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/double/ieee754-core/e_gamma.c,
	  src/double/ieee754-core/e_lgamma.c,
	  src/double/ieee754-api/w_gamma.c,
	  src/double/ieee754-api/w_lgamma.c:
	Remove direct reference to extern int signgam and include <math.h>
	instead

Mon Jul 27 23:47:52 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/math.h, include/pkgconf/libm.h,
	  src/double/ieee754-api/w_acos.c, src/double/ieee754-api/w_acosh.c,
	  src/double/ieee754-api/w_asin.c, src/double/ieee754-api/w_atan2.c,
	  src/double/ieee754-api/w_atanh.c, src/double/ieee754-api/w_cosh.c,
	  src/double/ieee754-api/w_exp.c, src/double/ieee754-api/w_fmod.c,
	  src/double/ieee754-api/w_gamma.c,
	  src/double/ieee754-api/w_gamma_r.c,
	  src/double/ieee754-api/w_hypot.c, src/double/ieee754-api/w_j0.c,
	  src/double/ieee754-api/w_j1.c, src/double/ieee754-api/w_jn.c,
	  src/double/ieee754-api/w_lgamma.c,
	  src/double/ieee754-api/w_lgamma_r.c,
	  src/double/ieee754-api/w_log.c,
	  src/double/ieee754-api/w_log10.c, src/double/ieee754-api/w_pow.c,
	  src/double/ieee754-api/w_remainder.c,
	  src/double/ieee754-api/w_scalb.c, src/double/ieee754-api/w_sinh.c,
	  src/double/ieee754-api/w_sqrt.c, src/double/ieee754-core/e_acos.c,
	  src/double/ieee754-core/e_acosh.c,
	  src/double/ieee754-core/e_asin.c,
	  src/double/ieee754-core/e_atan2.c,
	  src/double/ieee754-core/e_atanh.c,
	  src/double/ieee754-core/e_cosh.c,
	  src/double/ieee754-core/e_exp.c, src/double/ieee754-core/e_fmod.c,
	  src/double/ieee754-core/e_gamma.c,
	  src/double/ieee754-core/e_gamma_r.c,
	  src/double/ieee754-core/e_hypot.c, src/double/ieee754-core/e_j0.c,
	  src/double/ieee754-core/e_j1.c, src/double/ieee754-core/e_jn.c,
	  src/double/ieee754-core/e_lgamma.c,
	  src/double/ieee754-core/e_lgamma_r.c,
	  src/double/ieee754-core/e_log.c, src/double/ieee754-core/e_log10.c,
	  src/double/ieee754-core/e_pow.c,
	  src/double/ieee754-core/e_rem_pio2.c,
	  src/double/ieee754-core/e_remainder.c,
	  src/double/ieee754-core/e_scalb.c,
	  src/double/ieee754-core/e_sinh.c,
	  src/double/ieee754-core/e_sqrt.c, src/double/internal/k_cos.c,
	  src/double/internal/k_rem_pio2.c, src/double/internal/k_sin.c,
	  src/double/internal/k_tan.c, src/double/portable-api/s_asinh.c,
	  src/double/portable-api/s_atan.c, src/double/portable-api/s_cbrt.c,
	  src/double/portable-api/s_ceil.c,
	  src/double/portable-api/s_copysign.c,
	  src/double/portable-api/s_cos.c, src/double/portable-api/s_erf.c,
	  src/double/portable-api/s_expm1.c,
	  src/double/portable-api/s_fabs.c,
	  src/double/portable-api/s_finite.c,
	  src/double/portable-api/s_floor.c,
	  src/double/portable-api/s_frexp.c,
	  src/double/portable-api/s_ilogb.c,
	  src/double/portable-api/s_isnan.c,
	  src/double/portable-api/s_ldexp.c,
	  src/double/portable-api/s_log1p.c,
	  src/double/portable-api/s_logb.c,
	  src/double/portable-api/s_modf.c,
	  src/double/portable-api/s_nextafter.c,
	  src/double/portable-api/s_rint.c,
	  src/double/portable-api/s_scalbn.c,
	  src/double/portable-api/s_significand.c,
	  src/double/portable-api/s_sin.c, src/double/portable-api/s_tan.c,
	  src/double/portable-api/s_tanh.c, src/mathincl/fdlibm.h,
	  src/misc/standard.c:

	Untabify

Mon Jul 27 22:52:24 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (doTestVec): 
	Remove "register" when declaring variable i

	* host/acosgen.c, host/cosgen.c, host/fmodgen.c, host/modfgen.c,
   	  host/tangen.c, host/asingen.c, host/coshgen.c, host/frexpgen.c,
  	  host/powgen.c, host/tanhgen.c, host/atan2gen.c, host/expgen.c,
    	  host/ldexpgen.c, host/singen.c, host/atangen.c, host/fabsgen.c,
   	  host/log10gen.c, host/sinhgen.c, host/ceilgen.c, host/floorgen.c,
  	  host/loggen.c, host/sqrtgen.c:
	Remove "register" when declaring variable "int x"

Mon Jul 27 22:45:01 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/vector_support.h (checkErrorAcceptable): 
	Add extra check for tolerance acceptance so it behaves correctly with
	underflow and overflow

	Also reverse sense of checkErrorAcceptable() so it now returns
	false on success and true on failure, as suggested by hmt. Change
	this in doTestVec() (which is where it is called) too.

	* tests/vectors/vector_support.h: 
	Remove #if 0'd shift_double() function

Mon Jul 27 21:55:04 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mathincl/fdlibm.h: 
	Rename CYGONCE_LIBM_FDLIBM_H to CYGONCE_LIBM_MATHINCL_FDLIBM_H as per
	code review comments

Fri Jul 24 22:20:42 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/math.h, include/pkgconf/libm.h,
	  src/double/ieee754-api/w_acos.c, src/double/ieee754-api/w_acosh.c,
	  src/double/ieee754-api/w_asin.c, src/double/ieee754-api/w_atan2.c,
	  src/double/ieee754-api/w_atanh.c, src/double/ieee754-api/w_cosh.c,
	  src/double/ieee754-api/w_exp.c, src/double/ieee754-api/w_fmod.c,
	  src/double/ieee754-api/w_gamma.c, src/double/ieee754-api/w_gamma_r.c,
	  src/double/ieee754-api/w_hypot.c, src/double/ieee754-api/w_j0.c,
	  src/double/ieee754-api/w_j1.c, src/double/ieee754-api/w_jn.c,
	  src/double/ieee754-api/w_lgamma.c,
	  src/double/ieee754-api/w_lgamma_r.c, src/double/ieee754-api/w_log.c,
	  src/double/ieee754-api/w_log10.c, src/double/ieee754-api/w_pow.c,
	  src/double/ieee754-api/w_remainder.c,
	  src/double/ieee754-api/w_scalb.c, src/double/ieee754-api/w_sinh.c,
	  src/double/ieee754-api/w_sqrt.c, src/mathincl/fdlibm.h,
	  src/misc/compatmode.cxx, src/misc/matherr.c, src/misc/signgam.cxx,
	  src/misc/standard.c:

	Rename libm config option names as per the libm coding standard
	review. Chiefly ensuring that CYGXXX_ prefixes are correct

	* src/misc/matherr.c, include/pkgconf/libm.h:
	Add new CYGFUN_LIBC_matherr config option to prevent inclusion of
	default matherr

Mon Jul 20 18:07:31 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/infconst.c: 
	Oops. Don't let cyg_libm_infinity be static!

Thu Jul 16 20:07:26 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/math.h, include/sys/ieeefp.h, src/misc/infconst.c:
	Remove union Cyg_libm_int_double from math.h, which was used to
	define infinity, and replace with use of
	Cyg_libm_ieee_double_shape_type from ieeefp.h

	That type (which is a union) is now reordered so that it can be
	initialised in terms of two int's

Mon Jul 13 21:55:06 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/double/ieee754-api/w_acos.c, src/double/ieee754-api/w_acosh.c,
	  src/double/ieee754-api/w_asin.c, src/double/ieee754-api/w_atan2.c,
	  src/double/ieee754-api/w_atanh.c, src/double/ieee754-api/w_cosh.c,
	  src/double/ieee754-api/w_exp.c, src/double/ieee754-api/w_fmod.c,
	  src/double/ieee754-api/w_gamma.c, src/double/ieee754-api/w_gamma_r.c,
 	  src/double/ieee754-api/w_hypot.c, src/double/ieee754-api/w_j0.c,
 	  src/double/ieee754-api/w_j1.c, src/double/ieee754-api/w_jn.c,
 	  src/double/ieee754-api/w_lgamma.c,
 	  src/double/ieee754-api/w_lgamma_r.c, src/double/ieee754-api/w_log.c,
 	  src/double/ieee754-api/w_log10.c, src/double/ieee754-api/w_pow.c,
 	  src/double/ieee754-api/w_remainder.c,
 	  src/double/ieee754-api/w_scalb.c, src/double/ieee754-api/w_sinh.c,
 	  src/double/ieee754-api/w_sqrt.c, src/double/ieee754-core/e_acos.c,
 	  src/double/ieee754-core/e_acosh.c, src/double/ieee754-core/e_asin.c,
 	  src/double/ieee754-core/e_atan2.c, src/double/ieee754-core/e_atanh.c,
 	  src/double/ieee754-core/e_cosh.c, src/double/ieee754-core/e_exp.c,
 	  src/double/ieee754-core/e_fmod.c, src/double/ieee754-core/e_gamma.c,
 	  src/double/ieee754-core/e_gamma_r.c,
 	  src/double/ieee754-core/e_hypot.c, src/double/ieee754-core/e_j0.c,
 	  src/double/ieee754-core/e_j1.c, src/double/ieee754-core/e_jn.c,
 	  src/double/ieee754-core/e_lgamma.c,
 	  src/double/ieee754-core/e_lgamma_r.c,
 	  src/double/ieee754-core/e_log.c, src/double/ieee754-core/e_log10.c,
 	  src/double/ieee754-core/e_pow.c,
 	  src/double/ieee754-core/e_rem_pio2.c,
 	  src/double/ieee754-core/e_remainder.c,
 	  src/double/ieee754-core/e_scalb.c, src/double/ieee754-core/e_sinh.c,
 	  src/double/ieee754-core/e_sqrt.c, src/double/internal/k_cos.c, 
	  src/double/internal/k_rem_pio2.c, src/double/internal/k_sin.c,
 	  src/double/internal/k_tan.c, src/double/portable-api/s_asinh.c,
 	  src/double/portable-api/s_atan.c, src/double/portable-api/s_cbrt.c,
 	  src/double/portable-api/s_ceil.c,
 	  src/double/portable-api/s_copysign.c,
 	  src/double/portable-api/s_cos.c, src/double/portable-api/s_erf.c,
 	  src/double/portable-api/s_expm1.c, src/double/portable-api/s_fabs.c,
 	  src/double/portable-api/s_finite.c,
 	  src/double/portable-api/s_floor.c, src/double/portable-api/s_frexp.c,
 	  src/double/portable-api/s_ilogb.c, src/double/portable-api/s_isnan.c,
 	  src/double/portable-api/s_ldexp.c, src/double/portable-api/s_log1p.c,
 	  src/double/portable-api/s_logb.c, src/double/portable-api/s_modf.c,
 	  src/double/portable-api/s_nextafter.c,
 	  src/double/portable-api/s_rint.c, src/double/portable-api/s_scalbn.c,
 	  src/double/portable-api/s_significand.c,
	  src/double/portable-api/s_sin.c, src/double/portable-api/s_tan.c,
 	  src/double/portable-api/s_tanh.c, src/misc/standard.c:

	Make #ifdef __STDC__ bits compulsory and remove the associated #else
	clause. We know that gcc is ISO C compatible!

Tue Jul  7 16:05:48 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/compatmode.cxx:
	Fix conditionalisation to prevent unused variable warning for tracing

Thu Jun 25 04:58:21 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/vectors/acos.c, tests/vectors/acos.h, tests/vectors/asin.c,
	  tests/vectors/asin.h, tests/vectors/atan.c, tests/vectors/atan.h,
	  tests/vectors/atan2.c, tests/vectors/atan2.h, tests/vectors/ceil.c,
	  tests/vectors/ceil.h, tests/vectors/cos.c, tests/vectors/cos.h,
	  tests/vectors/cosh.c, tests/vectors/cosh.h, tests/vectors/exp.c,
	  tests/vectors/exp.h, tests/vectors/fabs.c, tests/vectors/fabs.h,
	  tests/vectors/floor.c, tests/vectors/floor.h, tests/vectors/fmod.c,
	  tests/vectors/fmod.h, tests/vectors/frexp.c, tests/vectors/frexp.h,
	  tests/vectors/ldexp.c, tests/vectors/ldexp.h, tests/vectors/log.c,
	  tests/vectors/log.h, tests/vectors/log10.c, tests/vectors/log10.h,
	  tests/vectors/modf.c, tests/vectors/modf.h, tests/vectors/pow.c,
	  tests/vectors/pow.h, tests/vectors/sin.c, tests/vectors/sin.h,
	  tests/vectors/sinh.c, tests/vectors/sinh.h, tests/vectors/sqrt.c,
	  tests/vectors/sqrt.h, tests/vectors/tan.c, tests/vectors/tan.h,
	  tests/vectors/tanh.c, tests/vectors/tanh.h,
	  tests/vectors/vector_support.h:
	Add math library tests for functions specified in the ISO standard.
	These are based on precomputed test vectors

	* tests/PKGconf.mak:
	Create with above files being built

	* host/acosgen.c, host/asingen.c, host/atan2gen.c, host/atangen.c,
	  host/ceilgen.c, host/cosgen.c, host/coshgen.c, host/expgen.c,
	  host/fabsgen.c, host/floorgen.c, host/fmodgen.c, host/frexpgen.c,
	  host/ldexpgen.c, host/log10gen.c, host/loggen.c, host/modfgen.c,
	  host/powgen.c, host/singen.c, host/sinhgen.c, host/sqrtgen.c,
	  host/tangen.c, host/tanhgen.c:
	Host-side (and currently linux-specific) sources to automatically
	generate test vector data used by the above tests.

	* include/pkgconf/libm.h:
	Ensure the kernel C API is available if we want thread safety

Wed Jun 24 15:42:31 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/standard.c:
	Fix typo in ifdef

Wed Jun 24 13:04:30 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/standard.c:
	Fix #defines for IEEE mode, revealed by permutation testing

Mon Jun 22 14:42:50 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/infconst.c:
	Fix compiler warning

Sun Jun 21 04:42:18 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/sys/ieeefp.h:
	Add this to allow bitfield break down of IEEE floating point doubles

Wed Jun 17 08:55:21 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/libm.h:
	Make the use of stderr for messages _not_ the default
	Make thread safety the default

	* src/misc/standard.c:
	Change alternative for fprintf(stderr,...) _not_ being used from
	"CYG_EMPTY_STATEMENT" to just "0" to placate compiler.

Mon Jun 15 19:59:36 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/compatmode.cxx:
	Fix typo in compatibility mode name

Fri Jun  5 16:31:26 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/misc/signgam.cxx, src/misc/compatmode.cxx:
	Fix some minor typos when thread safety is turned on

	* src/misc/matherr.c
	Correct syntax of weak attribute

Fri Jun  5 07:07:03 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* Initial check-in of all math library sources. Based on fdlibm-5.2.


//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004, 2007, 2008, 2010 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================