2009-07-14  Bart Veer  <bartv@ecoscentric.com>

	* host/configure.in: allow builds on x86_64 machines.

	* host/configure, host/Makefile.in, host/aclocal.m4: regenerate

2008-08-18  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am, host/configure.in: update host-configury.
	* host/Makefile.in, host/configure, host/aclocal.m4: regenerate

2008-08-13  Bart Veer  <bartv@ecoscentric.com>

	* host/rawether.c: eliminate compiler warning.
	* src/syntheth.c (synth_eth_start): ignore the enaddr argument.

2005-07-22  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/syntheth.c (synth_eth_init): Cast to keep the compiler
	happy.

2003-07-16  Gary Thomas  <gary@mlbassoc.com>

	* host/rawether.c: Change error reporting to use standard 'strerror()' 
	function since the use of sys_errlist[] is depricated.

2003-07-09  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am: add a dummy install-data-hook if not
	supported.

	* host/Makefile.in, host/aclocal.m4, host/configure: regenerate

2003-05-06  Bart Veer  <bartv@ecoscentric.com>

	* host/ethernet.tcl (filters_initialize):
	Fix typo reported by Scott Wilkinson

2003-02-25  Iztok Zupet  <iz@vsr.si>

	* doc/syntheth.sgml: Replaced .gif with .png to get PDF
	output.
	* doc/overview.gif: delete.
	* doc/overview.png: add.

2003-04-08  Andrew Lunn  <lunn@londo>

	* host/rawether.c (tap_init): Set the persistent flag on the tap
	device if requested by the user. This allows dhcpd and radvd to
	keep running on the tap device between invocations of the synth
	target.	
	* doc/syntheth.sgml: Documentation for the persistent option.

2003-04-01  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/syntheth.c (synth_eth_init): Set the flag IFF_ALLMULTI when
	the underlying device supports multicast so eth_drv correctly sets
	mutlicast filtering.  
	* cdl/syntheth.cdl: This driver implements multicast.

2003-02-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/syntheth.sgml: Declare as <part> not <reference> to get
	correct TOC numbering.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/syntheth.cdl: Add doc link.

	* doc/syntheth.sgml: Comment out DOCTYPE for now to allow building
	with standard doc build.
	Add an enclosing <reference> so it's structured better with standard
	doc build.

2003-02-13  Bart Veer  <bartv@ecoscentric.com>

	* src/syntheth.c, cdl/syntheth.cdl: add dependency on errno.h for
	error codes, and avoid memset() warning

2003-02-12  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.in, host/configure:
	Regenerate after toplevel acinclude.m4 update

2003-02-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/syntheth.cdl (CYGPKG_DEVS_ETH_ECOSYNTH_CFLAGS_ADD):
	Define -D_KERNEL -D__ECOS in line with other drivers. Fixes build
	issue with freeBSD stack.

2002-09-25  Bart Veer  <bartv@ecoscentric.com>

	* host/configure.in, host/rawether.c, doc/syntheth.sgml: 
	Only support the tap device if running a recent Linux kernel

2002-09-22  Bart Veer  <bartv@ecoscentric.com>

	* host/configure.in:
	Remove Tcl-related checks, the ethernet package only requires
	the functionality of the architectural HAL support

2002-08-07  Bart Veer  <bartv@ecoscentric.com>

	* synthetic target ethernet driver package created

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2002, 2003 Free Software Foundation, Inc.                  
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================