2009-04-28  John Dallaway  <john@dallaway.org.uk>

	* cdl/watchdog_lpc2xxx.cdl: Give CYGIMP_WATCHDOG_HARDWARE a default
	value rather than a calculated value to accommodate other
	implementations of CYGINT_WATCHDOG_IMPLEMENTATIONS.

2009-02-09  Bart Veer  <bartv@ecoscentric.com>

	* src/watchdog_lpc2xxx.cxx: switch init priority to
	CYG_INIT_INTERRUPTS.

2008-11-23  Sergei Gavrikov <sergei.gavrikov@gmail.com>
            Andrew Lunn     <andrew@lunn.ch>
	
	* src/watchdog_lpc2xxx.cxx: Since CYG_HAL_ARM_LPC2XXX_PCLK()
	macro has been removed from lpc2xxx_misc.h, insert a definition here.

2008-09-03  Sergei Gavrikov <sergei.gavrikov@gmail.com>

	* src/watchdog_lpc2xxx.cxx: Since CYG_HAL_ARM_LPC2XXX_PCLK()
	macro had been gone away from lpc2xxx_misc.h, it is replaced by
	an equal CYGNUM_HAL_ARM_LPC2XXX_PCLK constant.

2007-08-19  Sergei Gavrikov  <sg@sgs.gomel.by>

	* src/watchdog_lpc2xxx.cxx: Fixed to work properly in WDINT mode.
	
2004-10-04 Jani Monoses <jani@iv.ro>

	* Added watchdog driver for ARM LPC2XXX based on the AT91 code.

// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2003, 2004, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####