2009-07-14  Bart Veer  <bartv@ecoscentric.com>

	* host/configure.in: allow builds on x86_64 machines.

	* host/configure, host/Makefile.in, host/aclocal.m4: regenerate.

2009-02-04  Bart Veer  <bartv@ecoscentric.com>

	* src/synth_watchdog.cxx: use the generic watchdog package's
	prioritized constructor.

2008-08-18  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am: update host-side configury
	* host/Makefile.in, host/aclocal.m4, host/configure: regenerate.

2003-03-23  Iztok Zupet<iz@vsr.si>

	* doc/synth_watchdog.sgml: Replaced .gif with .png to allow for
	PDF build.

	* doc/asleep.gif, doc/awake.gif: Converted to *.png and deleted.
	* doc/asleep.png, doc/awake.png: New files.

2003-02-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/synth_watchdog.sgml: Declare as <part> not <reference> to get
	correct TOC numbering.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/synth_watchdog.cdl: Add doc link.

	* doc/synth_watchdog.sgml: Comment out DOCTYPE for now to allow
	building with standard doc build.
	Add an enclosing <reference> so it's structured better with standard
	doc build.

2003-02-12  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.in:
	Regenerate after toplevel acinclude.m4 update

2002-09-16  Bart Veer  <bartv@ecoscentric.com>

	* cdl/synth_watchdog.cdl:
	Synthetic watchdog device should only be active if the
	generic watchdog support is present

2002-09-04  Bart Veer  <bartv@ecoscentric.com>

	* Synthetic target watchdog package created

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2002, 2003, 2009 Free Software Foundation, Inc.                  
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================