2009-10-16  John Dallaway  <john@dallaway.org.uk>

	* cdl/hal_arm_xscale_ixdp425.cdl: Parent under
	CYGPKG_HAL_ARM_XSCALE_IXP425.

2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_xscale_ixdp425.cdl: update compiler flags for gcc 4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_xscale_ixdp425.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc.

2006-08-02  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/ixdp425_strataflash.c: In CYG_FLASH_FUNS, replace query
        function with generic nop version.
        Remove hwr_map_error: it no longer exists for CYG_FLASH_FUNS.

2006-03-01  Mark Salter  <msalter@sadr.localdomain>

	* include/hal_platform_setup.h: Fix DELAY macro.

2006-01-31  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_xscale_ixdp425.cdl
	(CYGHWR_HAL_ARM_XSCALE_IXDP425_FLASH): New option to support
	v2 Flash driver.
	* src/ixdp425_strataflash.c: New v2 flash driver.
	* include/hal_platform_setup.h: Add uncached Flash mapping.
	* include/ixdp425.h: Add uncached flash mappings.
	* include/plf_io.h: Provide CYGARC_UNCACHED_ADDRESS.
	* misc/redboot*.ecm: Use Strata V2 Flash driver.

2004-09-27  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROMRAM.ecm: Remove CYGHWR_HAL_IXP425_PCI_NP_WORKAROUND.
	* misc/redboot_ROMRAMLE.ecm: Ditto.

2004-09-20  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_xscale_ixdp425.cdl: Add -mcpu=xscale to LDFLAGS.

2004-09-19  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_xscale_ixdp425.cdl: Add -mcpu=xscale to CFLAGS.

	* misc/redboot_ROM.ecm: Add CYGSEM_REDBOOT_NETWORK_INIT_ONE_DEVICE.
	* misc/redboot_RAM.ecm: Ditto.
	* misc/redboot_ROMRAM.ecm: Ditto.
	* misc/redboot_ROMLE.ecm: Ditto.
	* misc/redboot_RAMLE.ecm: Ditto.
	* misc/redboot_ROMRAMLE.ecm: Ditto.

2004-09-07  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROM.ecm (CYGBLD_REDBOOT_MIN_IMAGE_SIZE): Set to 0x80000.
	* misc/redboot_RAM.ecm: Ditto.
	* misc/redboot_ROMLE.ecm: Ditto.
	* misc/redboot_RAMLE.ecm: Ditto.
	
	* include/pkgconf/mlt_arm_xscale_ixdp425_ram.mlt: Move .text to 0x80000.
	* include/pkgconf/mlt_arm_xscale_ixdp425_ram.ldi: Ditto.

	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.h: New file.
	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.ldi: Ditto.
	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.mlt: Ditto.
	* misc/redboot_ROMRAM.ecm: Ditto.
	* misc/redboot_ROMRAMLE.ecm: 

	* include/hal_platform_setup.h: Support ROMRAM.

2004-09-02  Mark Salter  <msalter@redhat.com>

	* src/ixdp425_pci.c: Fix compilation when not configured for PCI.
	* include/ixdp425.h: Add some defines for use in page table setup.
	* include/hal_platform_extras.h: Removed.
	* misc/redboot_ROMLE.ecm: New file.
	* misc/redboot_RAMLE.ecm: New file.
	* cdl/hal_arm_xscale_ixdp425.cdl: Add little-endian support.
	* misc/redboot_RAM.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.
	* include/hal_platform_setup.h: Ditto.

2003-06-30  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Fix CYGINT_HAL_ARM_BIGENDIAN test.
	Remove unused ROMRAM cruft.

2003-05-15  Mark Salter  <msalter@redhat.com>

	* src/ixdp425_misc.c (plf_hardware_init): Set EEPROM_SCL line high.
	(eeprom_stop): Leave EEPROM_SCL line high.

2003-04-04  Mark Salter  <msalter@redhat.com>

	* include/hal_plf_ints.h: Add GPIO IRQ defines.
	* include/ixdp425.h: Add GPIO line definitions.
	* src/ixdp425_misc.c (plf_hardware_init): Setup GPIO IRQ lines.
	Add support to read/write serial EEPROM. Add support for
	getting/setting NPE ethernet addresses from EEPROM.

2003-04-02  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROM.ecm: Don't set I82559_WRITE_EEPROM.
	* misc/redboot_RAM.ecm: Ditto.

2003-03-26  Mark Salter  <msalter@redhat.com>

	* src/ixdp425_misc.c (plf_hardware_init): Set up NPE PHY chip
	selects and clocks.

	* include/hal_plf_ints.h: Define interrupts for NPE PHYs.

2003-02-22  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROM.ecm: Fix linux exec address.
	* misc/redboot_RAM.ecm: Ditto

	* cdl/hal_arm_xscale_ixdp425.cdl: Fix HAL_PLATFORM_MACHINE_TYPE.

2003-02-13  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_extras.h: Move uncached area. Create RAM
	alias area.

2003-02-12  Mark Salter  <msalter@redhat.com>

	* misc/*.ecm: Turn on CYGPKG_DEVS_ETH_INTEL_I82559_WRITE_EEPROM.

2003-01-28  Mark Salter  <msalter@redhat.com>

	* misc/redboot_RAM.ecm: Turn on fileio support.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_ROMRAM.ecm: Ditto.

2003-01-22  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Tweak LED display.

2002-12-20  Mark Salter  <msalter@redhat.com>

	* include/hal_plf_ints.h: Don't use watchdog reset (CPU errata).

2002-12-19  Mark Salter  <msalter@redhat.com>

	* include/ixdp425.h (IXP425_EXP_CS0_INIT): Add in bit to allow
	8-bit access to 16-bit device.

	* cdl/hal_arm_xscale_ixdp425.cdl: Add back ROM startup now that
	bus controller supports 8-bit access to flash.

	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.h: Add.
	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.ldi: Ditto.
	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.mlt: Ditto.
	
	* misc/redboot_RAM.ecm: Allow flash verify.
	* misc/redboot_ROMRAM.ecm: Ditto.
	* misc/redboot_ROM.ecm: Add.

2002-12-18  Mark Salter  <msalter@redhat.com>

	* src/ixdp425_pci.c (cyg_hal_plf_pci_translate_interrupt): Fix
	interrupt vector determination.

	* include/pkgconf/mlt_arm_xscale_ixdp425_ram.mlt: Adjust start to
	work with romram startup.
	* include/pkgconf/mlt_arm_xscale_ixdp425_ram.ldi: Ditto.

2002-12-17  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROMRAM.ecm: New file.
	* misc/redboot_ROM.ecm: Remove.

	* include/ixdp425.h: Don't define DCACHE_FLUSH_AREA.

	* include/hal_platform_setup.h: Support ROMRAM.
	* include/hal_platform_extras.h: Ditto.
	* cdl/hal_arm_xscale_ixdp425.cdl: Ditto.

	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.h: Remove.
	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.ldi: Ditto.
	* include/pkgconf/mlt_arm_xscale_ixdp425_rom.mlt: Ditto.
	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.h: New file.
	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.ldi: Ditto.
	* include/pkgconf/mlt_arm_xscale_ixdp425_romram.mlt: Ditto.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2003, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================