2010-08-29  John Dallaway  <john@dallaway.org.uk>

	* misc/redboot_JTAG.ecm, misc/redbooot_ROM.ecm:
	Inhibit the FIS directory entry for RedBoot and management of the
	internal flash. Issues reported by Carlo Caione.

2009-02-04  Nick Garnett  <nickg@ecoscentric.com>

	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_jtag.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_sram.ldi:
	Add .sram section to linker scripts.

2009-02-07  Chris Holgate  <chris@zynaptic.com>

	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.ldi:
	Modified SRAM section so that initialisation data is placed in ROM.

2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_cortexm_stm32_stm3210e_eval.cdl: update compiler flags for gcc 4.x

2008-12-10  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_cortexm_stm32_stm3210e_eval.cdl: Switch value for
	CYGHWR_MEMORY_LAYOUT to calculated, so that changes to startup
	type are correctly propagated.

2008-11-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_cortexm_stm32_stm3210e_eval.cdl: Remove doc link
	to doc that doesn't exist.

2008-11-19  Nick Garnett  <nickg@ecoscentric.com>

	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.ldi (hal_startup_stack):
	Adjust initial stack to top of external SRAM.

2008-10-10  Nick Garnett  <nickg@ecoscentric.com>

	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.h:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.h:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_jtag.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_jtag.h:	
	* include/pkgconf/mlt_cortexm_stm3210e_eval_sram.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_sram.h:
	Update RAM/SRAM upper limits to account for interrupt/init
	stack.

	* src/stm3210e_eval_flash.c: Use generic null functions for
	external flash lock operations.

2008-10-06  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_cortexm_stm32_stm3210e_eval.cdl:
	* include/plf_arch.h:
	* include/plf_intr.h:
	* include/plf_io.h:
	* src/stm3210e_eval_misc.c:
	* src/stm3210e_eval_flash.c:
	* misc/redboot_ROM.ecm:
	* misc/redboot_JTAG.ecm:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_rom.h:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_ram.h:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_jtag.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_jtag.h:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_sram.ldi:
	* include/pkgconf/mlt_cortexm_stm3210e_eval_sram.h:
	New package -- ST STM3210E EVAL board HAL.
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2008, 2009, 2010 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================