2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_openrisc_orp.cdl: update compiler flags for gcc 4.x

2003-07-18  Nick Garnett  <nickg@balti.calivar.com>

	* cdl/hal_openrisc_orp.cdl:
        Changed values for CYGNUM_HAL_RTC_NUMERATOR,
        CYGNUM_HAL_RTC_DENOMINATOR and CYGNUM_HAL_RTC_PERIOD to
        "default_value" from "calculated". This makes it easier
        to change these values globally.
        
2003-04-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_openrisc_orp.cdl: CYGSEM_HAL_USE_ROM_MONITOR need only be a
	bool.
	CYGSEM_HAL_ROM_MONITOR should be default off (should be used later...)
	* include/pkgconf/mlt_openrisc_orp_ram.ldi: Add sections as per
	changes to arch HAL's openrisc.ld.
	* include/pkgconf/mlt_openrisc_orp_rom.ldi: Ditto.

2003-03-06  Scott Furman <sfurman@rosum.com>

        Initial port of eCos to OpenRISC Reference Platform (ORP)

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================