2011-01-02  Sergei Gavrikov  <sergei.gavrikov@gmail.com>

	* cdl/hal_sparc.cdl: Eliminate some warnings. [ Bugzilla 1001083 ]

2004-04-22  Jani Monoses <jani@iv.ro>

	 * cdl/hal_sparc.cdl :
	 Invoke tail with stricter syntax that works in latest coreutils. 

2003-04-10  Nick Garnett  <nickg@balti.calivar.com>

	* src/sparc.ld: 
	Added libsupc++.a to GROUP() directive for GCC versions later than
	3.0.

2002-10-19  Jonathan Larmour  <jifl@eCosCentric.com>

	Patch from Jiri Gaisler:
	* src/context.S (hal_thread_load_context): Wait a little after writing
	psr.
	(hal_setjmp): Ditto.
	* src/vectors.S (genuine_reset): Reorder window setup writes to
	streamline.
	

2002-04-29  Jonathan Larmour  <jlarmour@redhat.com>

	* src/vectors.S:
	* src/vec_xvsr.S:
	* src/vec_ivsr.S:
	Don't use .file as it can confuse debugging since the .file
	doesn't contain the path and therefore the debugger will never
	know where it lives! This conflicts with using -Wa,--gstabs.

2002-03-18  Hugo Tyson  <hmt@redhat.com>

	* src/vectors.S: Add CYGPKG_HAL_SPARC_ERC32 to list of ifdefs.

2002-03-14  Jiri Gaisler  <jiri@gaisler.com>

	* Initial version based on the SPARClite HAL.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================

//EOF ChangeLog