2010-10-26  John Dallaway  <john@dallaway.org.uk>

	* src/usbs.c, include/usbs.h: Extend usbs_control_endpoint struct and
	provide usbs_get_*_endpoint() functions to facilitate dynamic data
	endpoint configuration. Contributed by Chris Holgate.
	[ Bugzilla 1001024]
	* doc/usbs.sgml: Document the above changes.
	* cdl/usbs.cdl: Fix erroneous CYGPKG_IO_USB_SLAVE_TESTS display
	string.

2008-08-28  Bart Veer  <bartv@ecoscentric.com>

	* host/configure: regenerate after update of Tcl macro

2008-08-20  Bart Veer  <bartv@ecoscentric.com>

	* host/configure: regenerate after update of Tcl macro

2008-08-18  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am, host/configure.in: update host-side configury
	* host/Makefile.in, host/aclocal.m4, host/config.h.in,
	host/configure, host/stamp-h.in: regenerate.
	* host/acconfig.h: removed, no longer needed.

2008-08-13  Bart Veer  <bartv@ecoscentric.com>

	* host/usbhost.c: insist on the GNU version of strerror_r().
	Use the right header file for current Linux systems.
	* host/usbchmod.c: avoid compiler warning.

2006-05-07  Andrew Lunn  <andrew.lunn@ascom.ch>

	* host/bulk-boundaries.tcl(New): test bulk transfers at
	boundary cases.
	* doc/usbs.sgml: Documentation of bulk-boundaries.tcl test.

2006-04-23  Andrew Lunn  <andrew.lunn@ascom.ch>

	* doc/usbs-testing.html: Correct "format" for "data" when
	specifiying what the data in the USB message will contain.

2006-04-16  Andrew Lunn  <andrew.lunn@ascom.ch>

	* host/usbhost.c (tcl_run): Fix compiler warnings
	* host/usbhost.c (pool_function): sem_wait can exit with a
	EINTR. If so loop and try again.

	* host/usbchmod.c (usb_scan_devices) propergate previous fix from
	usbhost.c

2006-04-16  Frank Pagliughi <fpagliughi@mindspring.com>

	*host/usbhost.c (usb_scan_devices) Fix parsing EOL for FC4 and
	others.

2006-03-10  Bart Veer  <bartv@ecoscentric.com>

	* src/usbs.c (usbs_devtab_cwrite, usbs_devtab_cwrite): add
	DSR locking

2005-06-26  Bart Veer  <bartv@ecoscentric.com>

	* host/usbhost.c, host/configure.in: cope with incompatible
	changes to the system header <linux/usbdevice_fs.h>

	* host/acconfig.h: new file to support the above

	* host/Makefile.in, host/aclocal.m4, host/config.h.in,
	host/configure, host/stamp-h.in: regenerate

2003-03-27  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am, host/Makefile.in:
	$(bindir) may not exist yet, so create it if necessary.

2003-02-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/usbs.sgml: Declare as <part> not <reference> to get
	correct TOC numbering.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/usbs.cdl: Update doc links.

	* doc/usbs.sgml: Comment out DOCTYPE for now to allow building
	with standard doc build.

2003-02-12  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.in, host/configure:
	Regenerate after toplevel acinclude.m4 update

2002-09-23  Bart Veer  <bartv@ecoscentric.com>

	* host/configure.in:
	Only build if the required Linux kernel support is present.

2002-09-21  Bart Veer  <bartv@ecoscentric.com>

	* host/usbhost.c:
	Avoid const compatibility problems with Tcl 8.4

2002-01-23  Bart Veer  <bartv@redhat.com>

	* host/Makefile.am, host/Makefile.in, host/acinclude.m4,
	  host/aclocal.m4, host/configure, host/configure.in,
	  host/usbhost.c, host/usbhost.tcl, host/verbose.tcl
        Host-side support for USB testing
	
	* tests/usbtarget.c, tests/common.c, tests/protocol.h:
	New files containing the target-side testing support and
	support files.

	* cdl/usbs.cdl:
	Add a configuration option to build the target-side testing
	support.

	* doc/usbs.sgml, doc/*.html:
	Document the testing support. Regenerate html.

2001-09-14  Bart Veer  <bartv@redhat.com>

	* doc/usbs.sgml, doc/*.html:
	Fix the example strings in the enumeration data.
	Regenerate html.

	* include/usbs.h:
	Update the USB testing data structure	

	* src/usbs.c (usbs_handle_standard_control):
	Fix an assertion for the special case of a USB configuration that
	defines no endpoints.

2001-08-06  Bart Veer  <bartv@redhat.com>

	* include/usbs.h:
	Define additional data structures required for USB testing.

2001-06-19  Bart Veer  <bartv@redhat.com>

	* src/usbs.c, include/usbs.h (usbs_devtab_cread):
	read operations should not take a const buffer

2001-02-02  Bart Veer  <bartv@redhat.com>

	* cdl/usbs.cdl:
	Add doc property to point at the HTML

	* doc/usbs.sgml, *.html:
	Incorporate changes from docs department, regenerate HTML

2001-01-25  Bart Veer  <bartv@redhat.com>

	* src/usbs.c: 
	* include/usbs.h:
	Only declare the devtab support functions if the I/O package is
	present, since that provides required data types.

	* cdl/usbs.cdl:
	devtab support should be enabled by default iff the I/O package is
	present. 

2001-01-22  Bart Veer  <bartv@redhat.com>

	* doc/usbs.sgml, doc/makefile:
	Added documentation

2001-01-16  Bart Veer  <bartv@redhat.com>

	* include/usbs.h:
	* src/usbs.c:
	Update the start() and poll() functions to match the documentation.

2000-12-15  Bart Veer  <bartv@redhat.com>

	* src/usbs.c:
	Fix missing return statements.

2000-11-28  Bart Veer  <bartv@redhat.com>

	* cdl/usbs.cdl
	* include/usbs.h:
	* usbs.c
	Update interface to USB device drivers

2000-11-22  Bart Veer  <bartv@redhat.com>

	* include/usbs.h: Fix nested #include protection

2000-11-21  Bart Veer  <bartv@redhat.com>

	* First check-in of eCos USB support.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2010 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================