These are very preliminary notes on the design and use of the object loader.
Users should be aware that the package is still undergoing some changes.
Feedback is appreciated.

--------------------------------------------------------------------------------
Creating libraries
--------------------------------------------------------------------------------
Libraries can be created by simply compiling the sources into .o files.
The typical command line will look something like this:

<toolchain>-gcc -c -I$(ECOS_DIRECTORY)/include -Wall hello.c

The eCos "include" directory is needed to get the header files for the API.
Multiple object files can be compiled into a single object with the

<toolchain>-ld -r -o out.o file1.o file2.o file3.o

It must be noted that the use of a linker to collect multiple object files
into a single one considerably increases the size of the symbol table.

--------------------------------------------------------------------------------
Init/fini functions
--------------------------------------------------------------------------------
When the library is loaded the loader will look for a symbol with the name of 
"library_open" and, if found, will call the symbol with a prototype of

void library_open(void)

When the cyg_ldr_close_library() function is called, the loader will also 
look for a function called library close() and call it. The prototype is the 
same as library_open().

--------------------------------------------------------------------------------
External references.
--------------------------------------------------------------------------------
External references are the calls that the library makes to the eCos. These
calls are resolved by the loader if the function name is available in a table
provided by the user which maps a function name with its pointer. The loader
provides an empty table so that the user need only provide additional entry
required by the relocator.

In order to keep the size of the table to a minimum, the user can selectively 
include only those functions that are expected to be used by the loader to 
resolve all references.

The following is an example of how to add an entry to the external references 
table:

CYG_LDR_TABLE_ENTRY(diag_printf_entry, "diag_printf", diag_printf);

The first parameter is a unique identifier, the second is a string containing
the name of the function, and the third is the pointer to the function itself.
The entries can be added anywhere in the file.

The objelf.h file contains a number of macros that collect groups of
functions together as a convenient way to include blocks of
functionality.


--------------------------------------------------------------------------------
Writing the relocator for a new architecture
--------------------------------------------------------------------------------
A relocator for a new architecture must provide a function with the following
prototype:

cyg_int32 
cyg_ldr_relocate(cyg_int32 sym_type, cyg_uint32 mem, cyg_int32 sym_value)

The sym type is the type of relocation to apply. This value is architecture
dependent and it is obtained from the r_info field of the relocation entry.
The mem address is the memory location to relocate. The sym_value is the
value to use for the relocation. The size of the write operation is dependent
on the sym_type value.

The relocate_xxx.h file must provide definitions for:

1) the machine ELF type
2) the endianness of the architecture
           ELFDATA2MSB : Big endian
           ELFDATA2LSB : Little endian
3) The relocation type
           Elf_Rela    : With addend
           Elf_Rel     : Without addend

An example of the definition for the PowerPC processor is the following:

#define ELF_ARCH_MACHINE_TYPE         20              // PowerPC.
#define ELF_ARCH_ENDIANNESS           ELFDATA2MSB     // Big Endian.
#define ELF_ARCH_RELTYPE              Elf_Rela        // With explicit addend.

These definitions can be found in the relocate_ppc.h file.

The user must also provide a function with the following prototype:

void cyg_ldr_flush_cache(void)

tha is used to flush the data and address caches. This is architecture
dependent and usually the macros to do this are already part of the eCos HAL.
An empty function can be used is caches are not available.

--------------------------------------------------------------------------------
CDL File
--------------------------------------------------------------------------------

The CDL file allows the selective compilation of the architecture dependent
file. If a new architecture is added or a new loader is added, the CDL file
must be updated to include the architecture dependent files.

--------------------------------------------------------------------------------
Test program
--------------------------------------------------------------------------------

The 'tests' directory contains a simple/sample application that shows how to
use the object loader. The application loads a couple of symbols and runs
the functions pointed by those symbols. In particular, the second symbol is
a function which, in the library, is declared with the CYGBLD_ATTRIB_WEAK. If
the entry 

CYG_LDR_TABLE_ENTRY( weak_function_entry, "weak_function", weak_function );

is found in the application then the function in the application is called.
Otherwise, the function in the library is.

The source code for the library used for this example can be found under the 
'library' directory.

The library shows a number of concepts, including external references and WEAK 
references. The ubiquitous "twothreads' application is also included, and run
by the main application. Notice the initialization of the semaphore in the 
library_open() call.

The library can be compiled with the command

<toolchain>-gcc -c -Wall -o hello.o hello.c

and then be put into some file system and loaded. In the specific example 
provided, the library was placed in the root directory of a FAT partition.
JFFS2 is also an option.

If the CDL option CYGBLD_SERVICES_OBJLOADER_BUILD_TESTS is enabled,
then the test program and the library will be compiled automatically
and placed in the install tree bin directory.

--------------------------------------------------------------------------------
Final musings
--------------------------------------------------------------------------------

The cyg_ldr_open_library() call can be modified so that the user can use a 
library that is already in memory, or one that must be retrieved via ftp or
tftp. In order to do this some functions must be added:

- A function to open the file. In the simplest case of a file system, this
   function would be a wrapper for fopen(). See loader_fs.c for a possible
   implementation for a file system
- Function to read, seek and close the library. 
- In case you have a statically allocated memory pool, you might want to
  define your own cyg_ldr_malloc() and cyg_ldr_free(). Currently they are
  defined as weak bindings to wrappers of the malloc() and free() functions
- The relocator for the ARM architecture only works for ARMv4T cores and
   later ones. The problem arises from the fact that without the Thumb
   instruction set the loader should replace every "BX Rm" in the library
   with "MOV PC, Rm". This assumes that the library can find out what core it
   is running on at runtime, which is not possible at the moment. Given that
   ARMv4T cores are the ones used by most IC suppliers (Atmel, NXP, ST just
   to name a few) it is expected that the current code will work for nearly
   everyone.