Callbacks

Table of Contents
tcp_arg() -- Set the application connection state

Program execution is driven by callbacks. Each callback is an ordinary C function that is called from within the TCP/IP code. Every callback function is passed the current TCP or UDP connection state as an argument. Also, in order to be able to keep program specific state, the callback functions are called with a program specified argument that is independent of the TCP/IP state.

The tcp_arg() function is used for setting the application connection state.