netconn_bind()

Name

netconn_bind() -- Set local IP address/port of a netconn

Synopsis

err_t netconn_bind(struct netconn *conn, struct ip_addr *addr, u16_t port);

Description

Binds the connection conn to the local IP address addr and TCP or UDP port port. If addr is NULL, the local IP address is determined by the networking system.