fs cd

Name

fs cd -- Change filesystem directory

Synopsis

fs cd [directory]

Arguments

NameTypeDescriptionDefault
directoryStringPathname to directory to change to.Root directory

Description

This command changes the current filesystem directory. Subsequent filesystem commands will be executed in the new directory. If no argument is given, then the current directory is set back to the root of the filesystem name space.

Examples

Change current directory:
RedBoot> fs list
212416 d---------  3 size    128 .
212416 d---------  3 size    128 ..
211392 d---------  2 size     96 tests
210368 ----------  1 size   4096 image
RedBoot> fs cd tests
RedBoot> fs list
211392 d---------  2 size     96 .                                              
212416 d---------  3 size    128 ..                                             
205760 ----------  1 size  16384 test1                                          
RedBoot>