This command prints information about the filesystems that are available. Three lists are produced. The first is a list of the filsystem implementations available in RedBoot; names from this list may be used in the -t option to the fs mount command. The second list describes the block devices that are available for mounting a filesystem; names from this list may be used in the -d option to the fs mount command. The last list describes the filesystems that are already mounted.