fs list

Name

fs list -- List filesystem directory

Synopsis

fs list [directory]

Arguments

NameTypeDescriptionDefault
directoryStringPathname to directory to list.Current directory

Description

This command prints a list of the contents of the named directory. Each line of the listing starts with the file's inode number, which is its address in the filesystem. Following is a set of UNIX-like access flags, the first character of this will be a ”d“ if this entry is a directory. The third item indicates the number of links to the file. Following this is the size of the file in bytes and the last item is its name.

Examples

List the current directory:
RedBoot> fs list
212416 d---------  3 size    128 .                                              
212416 d---------  3 size    128 ..                                             
211392 ----------  1 size   4096 image                                          
206784 d---------  2 size     96 tests
RedBoot>

List a subdirectory:
RedBoot> fs list tests                                                            
206784 d---------  2 size     96 .                                              
212416 d---------  3 size    128 ..                                             
205760 ----------  1 size  16384 test1                                          
RedBoot>