ARM/ARM7+ARM9 ARM Integrator

Overview

RedBoot supports both serial ports for communication and downloads. The default serial port settings are 38400,8,N,1.

The following RedBoot configurations are supported:

ConfigurationModeDescriptionFile
ROM[ROM]RedBoot running from the board's flash boot sector.redboot_ROM.ecm
RAM[RAM]RedBoot running from RAM with RedBoot in the flash boot sector.redboot_RAM.ecm
ROMRAM[ROMRAM]RedBoot running from RAM, but contained in the board's flash boot sector.redboot_ROMRAM.ecm

Initial Installation

RedBoot is installed using the on-board bootPROM environment. See the user manual for full details.

Quick download instructions

Here are quick start instructions for downloading the prebuilt Redboot image:

Special RedBoot Commands

None.

Memory Maps

RedBoot sets up the following memory map on the Integrator board.

NOTE: The virtual memory maps in this section use a C and B column to indicate whether or not the region is cached (C) or buffered (B).


ARM7TDMI
--------

Physical Address Range  C B  Description
----------------------- - -  -----------
0x00000000 - 0x0007ffff N N  SSRAM
0x00080000 - 0x0fffffff N N  SDRAM (depends on part fitted)
0x10000000 - 0x1fffffff N N  System control and peripheral registers
0x20000000 - 0x23ffffff N N  Boot ROM (contains boot Monitor)
0x24000000 - 0x27ffffff N N  FLASH ROM (contains RedBoot)
0x28000000 - 0x2bffffff N N  SSRAM echo area
0x40000000 - 0x5fffffff N N  PCI Memory access windows
0x60000000 - 0x60ffffff N N  PCI IO access window
0x61000000 - 0x61ffffff N N  PCI config space window
0x62000000 - 0x6200ffff N N  PCI bridge register window
0x80000000 - 0x8fffffff N N  SDRAM echo area (used for PCI accesses)


ARM966E
-------

Physical Address Range  C B  Description
----------------------- - -  -----------
0x00000000 - 0x000fffff N N  SSRAM
0x00100000 - 0x0fffffff N N  SDRAM (depends on part fitted)
0x10000000 - 0x1fffffff N N  System control and peripheral registers
0x20000000 - 0x23ffffff N N  Boot ROM (contains boot Monitor)
0x24000000 - 0x27ffffff N N  FLASH ROM (contains RedBoot)
0x28000000 - 0x2bffffff N N  SSRAM echo area
0x40000000 - 0x5fffffff N N  PCI Memory access windows
0x60000000 - 0x60ffffff N N  PCI IO access window
0x61000000 - 0x61ffffff N N  PCI config space window
0x62000000 - 0x6200ffff N N  PCI bridge register window
0x80000000 - 0x8fffffff N N  SDRAM echo area (used for PCI accesses)

Rebuilding RedBoot

These shell variables provide the platform-specific information needed for building RedBoot according to the procedure described in Chapter 3:
export TARGET=integrator
export ARCH_DIR=arm
export PLATFORM_DIR=integrator

The names of configuration files are listed above with the description of the associated modes.