The mount table records the filesystems that are actually active. These can be seen as being analogous to mount points in Unix systems.
There are two sources of mount table entries. Filesystems (or other
components) may export static entries to the table using the
MTAB_ENTRY() macro. Alternatively, new entries may
be installed at run time using the mount()
function. Both types of entry may be unmounted with the
umount() function.
A mount table entry has the following structure:
struct cyg_mtab_entry
{
const char *name; // name of mount point
const char *fsname; // name of implementing filesystem
const char *devname; // name of hardware device
const char *options; // mount option string
CYG_ADDRWORD data; // private data value
cyg_bool valid; // Valid entry?
cyg_fstab_entry *fs; // pointer to fstab entry
cyg_dir root; // root directory pointer
}; |
The name field identifies the mount
point. This is used to direct rooted filenames (filenames that
begin with "/") to the correct filesystem. When a file
name that begins with "/" is submitted, it is matched
against the name fields of all valid mount
table entries. The entry that yields the longest match terminating
before a "/", or end of string, wins and the appropriate
function from the filesystem table entry is then passed the remainder
of the file name together with a pointer to the table entry and the
value of the root field as the directory
pointer.
For example, consider a mount table that contains the following entries:
{ "/", "fatfs", "/dev/hd0", ... }
{ "/fd", "fatfs", "/dev/fd0", ... }
{ "/rom", "romfs", "", ... }
{ "/tmp", "ramfs", "", ... }
{ "/dev", "devfs", "", ... } |
An attempt to open "/tmp/foo" would be directed to the RAM filesystem while an open of "/bar/bundy" would be directed to the hard disc FATFS filesystem. Opening "/dev/tty0" would be directed to the device management filesystem for lookup in the device table.
Unrooted file names (those that do not begin with a '/') are passed straight to the filesystem that contains the current directory. The current directory is represented by a pair consisting of a mount table entry and a directory pointer.
The fsname field points to a string that
should match the name field of the
implementing filesystem. During initialization the mount table is
scanned and the fsname entries looked up in
the filesystem table. For each match, the filesystem's _mount_
function is called and if successful the mount table entry is marked
as valid and the fs pointer installed.
The devname field contains the name of the
device that this filesystem is to use. This may match an entry in the
device table (see later) or may be a string that is specific to the
filesystem if it has its own internal device drivers.
The data field is a private data value. This
may be installed either statically when the table entry is defined, or
may be installed during the mount() operation.
The valid field indicates whether this mount
point has actually been mounted successfully. Entries with a false
valid field are ignored when searching for a
name match.
The fs field is installed after a successful
mount() operation to point to the implementing
filesystem.
The root field contains a directory pointer
value that the filesystem can interpret as the root of its directory
tree. This is passed as the dir argument of
filesystem functions that operate on rooted filenames. This field must
be initialized by the filesystem's mount()
function.