This section describes the main HAL interfaces.
These are definitions that characterize the properties of the base architecture that are used to compile the portable parts of the kernel. They are concerned with such things a portable type definitions, endianness, and labeling.
These definitions are supplied by the cyg/hal/basetype.h header file which is supplied by the architecture HAL. It is included automatically by cyg/infra/cyg_type.h.
This defines the byte order of the target and must be set to either CYG_LSBFIRST or CYG_MSBFIRST.
CYG_LABEL_NAME(name) This is a wrapper used in some C and C++ files which
use labels defined in assembly code or the linker script.
It need only be defined if the default implementation in
cyg/infra/cyg_type.h, which passes the name
argument unaltered, is inadequate. It should be paired with
CYG_LABEL_DEFN().
CYG_LABEL_DEFN(name)This is a wrapper used in assembler sources and linker scripts which define labels. It need only be defined if the default implementation in cyg/infra/cyg_type.h, which passes the name argument unaltered, is inadequate. The most usual alternative definition of this macro prepends an underscore to the label name.
cyg_halint8 cyg_halint16 cyg_halint32 cyg_halint64 cyg_halcount8 cyg_halcount16 cyg_halcount32 cyg_halcount64 cyg_halbool |
These macros define the C base types that should be used to define variables of the given size. They only need to be defined if the default types specified in cyg/infra/cyg_type.h cannot be used. Note that these are only the base types, they will be composed with signed and unsigned to form full type specifications.
cyg_halatomic CYG_ATOMIC |
These types are guaranteed to be read or written in a single uninterruptible operation. It is architecture defined what size this type is, but it will be at least a byte.