#include <cyg/io/strata_dev.h>
|
int cyg_strata_init_nop(struct cyg_flash_dev* device);
int cyg_strata_init_check_devid_XX(struct cyg_flash_dev* device);
int cyg_strata_init_cfi_XX(struct cyg_flash_dev* device);
int cyg_strata_erase_XX(struct cyg_flash_dev* device, cyg_flashaddr_t addr);
int cyg_strata_program_XX(struct cyg_flash_dev* device, cyg_flashaddr_t addr, const void* data, size_t len);
int cyg_strata_bufprogram_XX(struct cyg_flash_dev* device, cyg_flashaddr_t addr, const void* data, size_t len);
int cyg_strata_lock_j3_XX(struct cyg_flash_dev* device, const cyg_flashaddr_t addr);
int cyg_strata_unlock_j3_XX(struct cyg_flash_dev* device, const cyg_flashaddr_t addr);
int cyg_strata_lock_k3_XX(struct cyg_flash_dev* device, const cyg_flashaddr_t addr);
int cyg_strata_unlock_k3_XX(struct cyg_flash_dev* device, const cyg_flashaddr_t addr);
The Strata family contains a number of different devices, all supporting the same basic set of operations but with various common or uncommon extensions. The range includes:
These support 8 8K boot blocks as well as the usual 64K blocks. There is no buffered write capability. The only locking mechanism available involves manipulating voltages on certain pins.
These also have boot blocks. There is no buffered write capability. Individual blocks can be locked and unlocked in software.
These are uniform devices where all blocks are 128K. Buffered writes are supported. Blocks can be locked individually, but the only unlock operation is a global unlock-all.
These are also uniform devices with 128K blocks. Buffered writes are supported. Individual blocks can be locked and unlocked in software.
Each of these comes in a range of sizes and bus widths. There are also platform-specific issues such as how many devices are actually present on the board and where they are mapped in the address space. The Strata driver package cannot know all this information. Instead it is the responsibility of another package, usually the platform HAL, to instantiate some flash device structures. Two pieces of information are especially important: the bus configuration and the boot block layout.
Flash devices are typically 8-bits, 16-bits, or 32-bits wide (64-bit devices are not yet in common use). Most 16-bit devices will also support 8-bit accesses, but not all. Similarly 32-bit devices can be accessed 16-bits at a time or 8-bits at a time. A board will have one or more of these devices on the bus. For example there may be a single 16-bit device on a 16-bit bus, or two 16-bit devices on a 32-bit bus. The processor's bus logic determines which combinations are possible, and usually there will be a trade off between cost and performance. For example two 16-bit devices in parallel can provide twice the memory bandwidth of a single device. The driver supports the following combinations:
A single 8-bit flash device on an 8-bit bus.
A single 16-bit flash device on a 16-bit bus.
A single 32-bit flash device on an 32-bit bus.
Two parallel 8-bit devices on an 16-bit bus.
Four parallel 8-bit devices on a 32-bit bus.
Two parallel 16-bit devices on a 32-bit bus, with one device providing the bottom two bytes of each 32-bit datum and the other device providing the upper two bytes.
A single 16-bit flash device connected to an 8-bit bus.
These configuration all require slightly different code to manipulate
the hardware. The Strata driver package provides separate functions
for each configuration, for example
cyg_strata_erase_16 and
cyg_strata_program_1616.
| Caution |
At the time of writing not all the configurations have been tested. |
The second piece of information is the boot block layout. Flash devices are subdivided into blocks (also known as sectors, both terms are in common use). Some operations such as erase work on a whole block at a time, and for most applications a block is the smallest unit that gets updated. A typical block size is 64K. It is inefficient to use an entire 64K block for small bits of configuration data and similar information, so some flash devices also support a number of smaller boot blocks. A typical 2MB flash device could have eight 8K blocks and 31 full-size 64K blocks. The boot blocks may appear at the bottom or the top of the device. So-called uniform devices do not have boot blocks, just full-size ones. The driver needs to know the boot block layout. With modern devices it can work this out at run-time, but often it is better to provide the information statically.
Flash support is usually specific to each platform. Even if two platforms happen to use the same flash device there are likely to be differences such as the location in the address map. Hence there is little possibility of re-using the platform-specific code, and this code is generally placed in the platform HAL rather than in a separate package. Typically this involves a separate file and a corresponding compile property in the platform HAL's CDL:
cdl_package CYGPKG_HAL_M68K_KIKOO {
…
compile -library=libextras.a kikoo_flash.c
…
}
|
The contents of this file will not be accessed directly, only indirectly via the generic flash API, so normally it would be removed by link-time garbage collection. To avoid this the object file has to go into libextras.a.
The actual file kikoo_flash.c will look something like:
#include <pkgconf/system.h>
#ifdef CYGPKG_DEVS_FLASH_STRATA_V2
#include <cyg/io/flash.h>
#include <cyg/io/strata_dev.h>
static const CYG_FLASH_FUNS(hal_kikoo_flash_strata_funs,
&cyg_strata_init_check_devid_16,
&cyg_flash_devfn_query_nop,
&cyg_strata_erase_16,
&cyg_strata_bufprogram_16,
(int (*)(struct cyg_flash_dev*, const cyg_flashaddr_t, void*, size_t))0,
&cyg_strata_lock_j3_16,
&cyg_strata_unlock_j3_16);
static const cyg_strata_dev hal_kikoo_flash_priv = {
.manufacturer_code = CYG_FLASH_STRATA_MANUFACTURER_INTEL,
.device_code = 0x0017,
.bufsize = 16,
.block_info = {
{ 0x00020000, 64 } // 64 * 128K blocks
}
};
CYG_FLASH_DRIVER(hal_kikoo_flash,
&hal_kikoo_flash_strata_funs,
0,
0x60000000,
0x601FFFFF,
1,
hal_kikoo_flash_priv.block_info,
&hal_kikoo_flash_priv
);
#endif
|
The bulk of the file is protected by an ifdef for the Strata flash
driver. That driver will only be active if the generic flash support
is enabled. Without that support there will be no way of accessing
the device so there is no point in instantiating the device. The rest
of the file is split into three definitions. The first supplies the
functions which will be used to perform the actual flash accesses,
using a macro provided by the generic flash code in cyg/io/flash_dev.h. The
relevant ones have an _16 suffix, indicating that
on this board there is a single 16-bit flash device on a 16-bit
bus. The second definition provides information specific to Strata
flash devices. The third provides the
cyg_flash_dev structure needed by the generic
flash code, which contains pointers to the previous two.
All eCos flash device drivers must implement a standard interface,
defined by the generic flash code CYGPKG_IO_FLASH.
This interface includes a table of 7 function pointers for various
operations: initialization, query, erase, program, read,
locking and unlocking. The query operation is optional and
the generic flash support provides a dummy implementation
cyg_flash_devfn_query_nop. Strata flash devices
are always directly accessible so there is no need for a separate read
function. The remaining functions are more complicated.
Usually the table can be declared const. In a ROM startup application this avoids both ROM and RAM copies of the table, saving a small amount of memory. const should not be used if the table may be modified by a platform-specific initialization routine.
There is a choice of three main initialization functions. The simplest
is cyg_flash_devfn_init_nop, which does nothing. It
can be used if the cyg_strata_dev and
cyg_flash_dev structures are fully
initialized statically and the flash will just work without special
effort. This is useful if it is guaranteed that the board will always
be manufactured using the same flash chip, since the nop function
involves the smallest code size and run-time overheads.
The next step up is
cyg_strata_init_check_devid_XX, where
XX will be replaced by the suffix appropriate for
the bus configuration. It is still necessary to provide all the device
information statically, including the devid
field in the cyg_strata_dev structure.
However this initialization function will attempt to query the flash
device and check that the provided manufacturer and device codes
matches the actual hardware. If there is a mismatch the device will be
marked uninitialized and subsequent attempts to manipulate the flash
will fail.
If the board may end up being manufactured with any of a number of
different flash chips then the driver can perform run-time
initialization, using a cyg_strata_init_cfi_XX
function. This queries the flash device as per the Common Flash Memory
Interface Specification, supported by all current devices (although
not necessarily by older devices). The
block_info field in the
cyg_strata_dev structure and the
end and
num_block_infos fields in the
cyg_flash_dev structure will be filled in.
It is still necessary to supply the start
field statically since otherwise the driver will not know how to
access the flash device. The main disadvantage of using CFI is that it
will increase the code size.
A final option is to use a platform-specific initialization function.
This may be useful if the board may be manufactured with one of a
small number of different flash devices and the platform HAL needs to
adapt to this. The Strata driver provides a utility function to
read the device id, cyg_strata_read_devid_XX:
static int
kikoo_flash_init(struct cyg_flash_dev* dev)
{
int manufacturer_code, device_code;
cyg_strata_read_devid_1616(dev, &manufacturer_code, &device_code);
if (manufacturer_code != CYG_FLASH_STRATA_MANUFACTURER_STMICRO) {
return CYG_FLASH_ERR_DRV_WRONG_PART;
}
switch(device_code) {
case 0x0042 :
…
case 0x0084 :
…
default:
return CYG_FLASH_ERR_DRV_WRONG_PART;
}
}
|
There are many other possible uses for a platform-specific initialization function. For example initial prototype boards might have only supported 8-bit access to a 16-bit flash device rather than 16-bit access, but this was fixed in the next revision. The platform-specific initialization function could figure out which model board it is running on and replace the default 16as8 functions with 16 ones.
The Strata driver provides erase and program functions appropriate for the various bus configurations. On most targets these can be used directly. On some targets it may be necessary to do some extra work before and after the erase and program operations. For example if the hardware has an MMU then the part of the address map containing the flash may have been set to read-only, in an attempt to catch spurious memory accesses. Erasing or programming the flash requires write-access, so the MMU settings have to be changed temporarily. For another example some flash device may require a higher voltage to be applied during an erase or program operation. or a higher voltage may be desirable to make the operation proceed faster. A typical platform-specific erase function would look like this:
static int
kikoo_flash_erase(struct cyg_flash_dev* dev, cyg_flashaddr_t addr)
{
int result;
… // Set up the hardware for an erase
result = cyg_strata_erase_32(dev, addr);
… // Revert the hardware change
return result;
}
|
There are two versions of the program function.
cyg_strata_bufprogram_xx uses the buffered write
capability of some strata chips. This allows the flash chip to perform
the writes in parallel, thus greatly improving performance. It
requires that the bufsize field of the
cyg_strata_dev structure is set correctly to
the number of words in the write buffer. The usual value for this is
16, corresponding to a 32-byte write buffer. The alternative
cyg_strata_program_xx writes the data one word at
a time so is significantly slower. It should be used only with strata
chips that do not support buffered writes, for example the b3 and c3
series.
There are two configuration options which affect the erase and program functions, and which a platform HAL may wish to change: CYGNUM_DEVS_FLASH_STRATA_V2_ERASE_TIMEOUT and CYGNUM_DEVS_FLASH_STRATA_V2_PROGRAM_TIMEOUT. The erase and program operations both involve polling for completion, and these timeout impose an upper bound on the polling loop. Normally these operations should never take anywhere close to the timeout period, and hence a timeout probably indicates a catastrophic failure that should really be handled by a watchdog reset. A reset is particularly appropriate because there will be no clean way of aborting the flash operation. The main reason for the timeouts is to help with debugging when porting to new hardware. If there is a valid reason why a particular platform needs different timeouts then the platform HAL's CDL can require appropriate values for these options.
Current Strata devices implement locking in three different ways, requiring different sets of functions:
There is no software locking support. The
cyg_flash_devfn_lock_nop and
cyg_flash_devfn_unlock_nop functions should be used.
These support locking and unlocking individual blocks. The
cyg_strata_lock_k3_XX and
cyg_strata_unlock_k3_XX functions should be used.
All blocks are locked following power-up or reset, so the unlock
function must be used before any erase or program operation.
Theoretically the lock function is optional and
cyg_flash_devfn_lock_nop can be used instead, saving a
small amount of code space.
Individual blocks can be locked using
cyg_strata_lock_j3_XX, albeit using a slightly
different algorithm from the C3 and K3 series. However the only unlock
support is a global unlock of all blocks. Hence the only way to unlock
a single block is to check the locked status of every block, unlock
them all, and relock the ones that should still be locked. This
time-consuming operation is implemented by
cyg_strata_unlock_j3_XX. Worse, unlocking all
blocks can take approximately a second. During this time the flash is
unusable so normally interrupts have to be disabled, affecting
real-time responsiveness. There is no way of suspending this
operation.
Unlike the C3 and K3 chips, on a J3 blocks are not automatically
locked following power-up or reset. Hence lock and unlock support is
optional, and cyg_flash_devfn_lock_nop and
cyg_flash_devfn_unlock_nop can be used.
If real locking functions are used then the platform HAL's CDL script should implement the CDL interface CYGHWR_IO_FLASH_BLOCK_LOCKING. Otherwise the generic flash package may believe that none of the flash drivers in the system provide locking functionality and disable the interface functions.
The cyg_strata_dev structure provides
information specific to Strata flash devices, as opposed to the
more generic flash information which goes into the
cyg_flash_dev structure. There are only two
fields: devid and
block_info.
manufacturer_code and
device_code are needed only if the driver's
initialization function is set to
cyg_strata_init_check_devid_XX. That function
will extract the actual device info from the flash chip and compare it
with these fields. If there is a mismatch then subsequent operations
on the device will fail. Definitions of
CYG_FLASH_STRATA_MANUFACTURER_INTEL and
CYG_FLASH_STRATA_MANUFACTURER_STMICRO are provided
for convenience.
The bufsize field is needed only if a
buffered program function
cyg_strata_bufprogram_XX is used. It should give
the size of the buffer in words. Typically Strata devices have a
32-byte buffer, so when attached to an 8-bit bus
bufsize should be 32 and when attached to a
16-bit bus it should be 16.
The block_info field consists of one or
more pairs of the block size in bytes and the number of blocks of that
size. The order must match the actual hardware device since the flash
code will use the table to determine the start and end locations of
each block. The table can be initialized in one of three ways:
If the driver initialization function is set to
cyg_strata_init_nop or
cyg_strata_init_check_devid_XX then the block
information should be provided statically. This is appropriate if the
board will also be manufactured using the same flash chip.
If cyg_strata_init_cfi_XX is used then this
will fill in the block info table. Hence there is no need for static
initialization.
If a platform-specific initialization function is used then either this should fill in the block info table, or the info should be provided statically.
The size of the block_info table is
determined by the configuration option
CYGNUM_DEVS_FLASH_STRATA_V2_ERASE_REGIONS.
This has a default value of 2, which should suffice for nearly all
Strata flash devices. If more entries are needed then the platform
HAL's CDL script should require a larger value.
If the cyg_strata_dev structure is
statically initialized then it can be const. This
saves a small amount of memory in ROM startup applications. If the
structure may be updated at run-time, either by
cyg_strata_init_cfi_XX or by a
platform-specific initialization routine, then it cannot be
const.
Internally the flash code works in terms of
cyg_flash_dev structures, and the platform
HAL should define one of these. The structure should be placed in the
cyg_flashdev table. The following fields need to be
provided:
funsThis should point at the table of functions.
startThe base address of the flash in the address map. On
some board the flash may be mapped into memory several times, for
example it may appear in both cached and uncached parts of the address
space. The start field should correspond to
the cached address.
endThe address of the last byte in the flash. It can
either be statically initialized, or
cyg_strata_init_cfi_XX will calculate
its value at run-time.
num_block_infosThis should be the number of entries in the
block_info table. It can either be
statically initialized or it will be filled in by
cyg_strata_init_cfi_XX.
block_infoThe table with the block information is held in the
cyg_strata_dev structure, so this field
should just point into that structure.
privThis field is reserved for use by the device driver. For the Strata
driver it should point at the appropriate
cyg_strata_dev structure.
The cyg_flash_dev structure contains a number
of other fields which are manipulated only by the generic flash code.
Some of these fields will be updated at run-time so the structure
cannot be declared const.
A board may have several flash devices in parallel, for example two
16-bit devices on a 32-bit bus. It may also have several such banks
to increase the total amount of flash. If each device provides 2MB,
there could be one bank of 2 parallel flash devices at 0xFF800000 and
another bank at 0xFFC00000, giving a total of 8MB. This setup can be
described in several ways. One approach is to define two
cyg_flash_dev structures. The table of
function pointers can usually be shared, as can the
cyg_strata_dev structure. Another approach
is to define a single cyg_flash_dev
structure but with a larger block_info
table, covering the blocks in both banks of devices. The second
approach makes more efficient use of memory.
Many variations are possible, for example a small slow flash device
may be used for initial bootstrap and holding the configuration data,
while there is also a much larger and faster device to hold a file
system. Such variations are usually best described by separate
cyg_flash_dev structures.
If more than one cyg_flash_dev structure is
instantiated then the platform HAL's CDL script should implement the
CDL interface CYGHWR_IO_FLASH_DEVICE once for every
device past the first. Otherwise the generic code may default to the
case of a single flash device and optimize for that.
The Strata driver source code includes the header files cyg/hal/hal_arch.h and cyg/hal/hal_io.h, and hence indirectly the corresponding platform header files (if defined). Optionally these headers can define macros which are used inside the driver, thus giving the HAL limited control over how the driver works.
By default the strata driver assumes that the flash can be accessed
uncached, and it will use the HAL
CYGARC_UNCACHED_ADDRESS macro to map the cached
address in the start field of the
cyg_flash_dev structure into an uncached
address. If for any reason this HAL macro is inappropriate for the
flash then an alternative macro
HAL_STRATA_UNCACHED_ADDRESS can be defined
instead. However fixing the
CYGARC_UNCACHED_ADDRESS macro is normally the
better solution.
If there is no way of bypassing the cache then the platform HAL should implement the CDL interface CYGHWR_DEVS_FLASH_STRATA_V2_CACHED_ONLY. The flash driver will now disable and re-enable the cache as required. For example a program operation will involve the following:
STRATA_INTSCACHE_STATE;
STRATA_INTSCACHE_BEGIN();
while ( ! finished ) {
write a burst of CYGNUM_DEVS_FLASH_STRATA_V2_PROGRAM_BURST_SIZE
STRATA_INTSCACHE_SUSPEND();
STRATA_INTSCACHE_RESUME();
}
STRATA_INTSCACHE_END();
|
The default implementations of these INTSCACHE macros are as follows:
STATE defines any local variables that may be
needed, e.g. to save the current interrupt state;
BEGIN disables interrupts, synchronizes the data
caches, disables it, and invalidates the current contents;
SUSPEND re-enables the data cache and then
interrupts; RESUME disables interrupts and the
data cache; END re-enables the cache and then
interrupts. The cache is only disabled when interrupts are disabled,
so there is no possibility of an interrupt handler running or a
context switch occurring while the cache is disabled, potentially
leaving the system running very slowly. The data cache synchronization
ensures that there are no dirty cache lines, so when the cache is
disabled the low-level flash write code will not see stale data in
memory. The invalidate ensures that at the end of the operation
higher-level code will not pick up stale cache contents instead of the
newly written flash data. The SUSPEND and
RESUME macros only re-enable and disable the data
cache. An interrupt and possibly a context switch may occur between
these macros and use the cache normally. It is assumed that any code
which runs at this time will not touch the memory being used by the
flash operation, so as far as the low-level program code is concerned
it can just continue to use the uncached memory contents as set up by
the BEGIN macro. If any code modifies the const
data currently being written to a flash block or tries to read the
flash block being modified then the system's behaviour is undefined.
Theoretically a more robust approach is possible, synchronizing and
invalidating the cache again in every RESUME.
However these cache operations can be expensive and
RESUME may get invoked some thousands of times
for every flash block, so this alternative approach would cripple the
driver's performance.
Some implementations of the HAL cache macros may not provide the exact
semantics required by the flash driver. For example
HAL_DCACHE_DISABLE may have an unwanted side
effect, or it may do more work than is needed here. The driver will
check for alternative macros
HAL_STRATA_INTSCACHE_STATE,
HAL_STRATA_INTSCACHE_BEGIN,
HAL_STRATA_INTSCACHE_SUSPEND,
HAL_STRATA_INTSCACHE_RESUME and
HAL_STRATA_INTSCACHE_END, using these instead of
the defaults.
On some platforms it may be necessary to perform some additional
action in the middle of a lengthy erase or program operation. For
example, consider a platform with a watchdog device that cannot be
disabled: when running in a polled environment such as RedBoot
the flash operation run will run to completion, and there will be no
opportunity for higher-level code to reset the watchdog; if the flash
operation takes long enough the watchdog will trigger. To avoid
problems in such scenarios, the platform HAL can define a macro
HAL_STRATA_POLL. The macro is optional: if absent
then the driver will automatically substitute a no-op.