2009-06-24  Bart Veer  <bartv@ecoscentric.com>

	* tests/signal2.c (cause_unaligned_access): fix coldfire support

2009-04-02  Nick Garnett  <nickg@ecoscentric.com>

	* tests/pmutex5.c (thread1): Increase timeout to 2s. This may fix
	some unusual failures in the farm.

	* tests/signal2.c: Add Cortex-M to set of targets for which
	unaligned exception is not supported.

2008-12-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/tm_posix.cxx: In line with kernel tm_basic test, macro called
	max should actually be called min.

2008-09-11  Bart Veer  <bartv@ecoscentric.com>

	* tests/signal2.c (cause_illegal_access): when defined, use HAL
	macro to provoke exception.

2008-09-10  Bart Veer  <bartv@ecoscentric.com>

	* src/startup.cxx (cyg_posix_startup_dummy_constructor_class):
	initialize the clock support ifdef CYGPKG_POSIX_CLOCKS, not
	CYGPKG_POSIX_TIMERS.

2008-03-28  John Dallaway  <jld@ecoscentric.com>

	* tests/tm_basic.cxx: Rename test to tm_posix.cxx.
	* tests/mqueue1.c: Rename test to pmqueue1.c.
	* tests/mqueue2.c: Rename test to pmqueue2.c.
	* tests/mutex3.c: Rename test to pmutex3.c.
	* tests/mutex5.c: Rename test to pmutex5.c.
	* cdl/posix.cdl: Accommodate the above renaming. Test names must be
	globally unique.

2007-11-27  Bart Veer  <bartv@ecoscentric.com>

	* tests/tm_basic.cxx: cope with ports which cannot implement
	HAL_CLOCK_READ() 

2007-06-12  Richard.Yuan <lemonskin@tom.com>

	* src/except.cxx (install_handlers): Fixed typo. Bug #1000373
	
2007-05-25  Nick Garnett  <nickg@ecoscentric.com>

	* src/time.cxx: Move timer_mutex out of ifdef for
	CYGPKG_POSIX_TIMERS since it is now used by the clock routines
	too.
	(clock_settime): Add ifdef around access to timers in
	clock_settime().

	* tests/timer2.c (sigusr2): Timeout validity test comparison was
	the wrong way round.

2007-05-23  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/posix.cdl: Add option for linking CLOCK_REALTIME to the
	wallclock device, if it is present.

	* src/time.cxx: Add support for linking CLOCK_REALTIME to the
	wallclock. 

	* tests/timer2.c: New test for clock_realtime() functionality.

2007-02-21  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/posix.cdl: mutex5 test depends on POSIX signals, so only build
	this test if signals are enabled.

2007-01-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/posix.cdl: Add _POSIX_THREAD_PRIO_NONE as a non-standard feature
	test, in symmetry with the others, since it depends on
	CYGSEM_KERNEL_SYNCH_MUTEX_PRIORITY_INVERSION_PROTOCOL_NONE, which
	may not otherwise be defined if the kernel has non-dynamic 
	protocol other than 'none'.
	Mutex5 test needs pthreads.
	* include/muttypes.h: Conditionalise PTHREAD_PRIO_NONE definition.
	* src/mutex.cxx: Allow mutex functions to adapt better to changes
	in config which may result in dynamic protocol support being
	disabled, and thus having to deal with a single fixed protocol.

2006-10-06  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/pprivate.h: Add signal_count member to pthread_info, to count
	the number of signals handled by a thread and so know when it has
	changed.
	* src/pthread.c ( cyg_posix_pthread_release_thread): Don't release
	current thread, and comment why.
	* src/signal.cxx (cyg_deliver_signals): Increment this thread's
	signal_count.
	(cyg_posix_thread_siginit): Init signal_count.
	(pause): Use signal_count to determine when a signal was handled
	by _this_ thread, irrespective of where cyg_deliver_signals was
	called (e.g. the ASR).
	* tests/signal1.c: Expand some info messages to make them unambiguous.
	Must wait for thread1 to reach pause before we can call kill()
	with SIGUSR2.

2006-07-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/pthread.cxx (pthread_create): name_template can be const.

2006-07-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/signal.cxx (pause): Although already POSIX compliant, if we wait
	for all signals, behaviour is more Linux-like.

2006-06-13  Dan Jakubiec  <dan.jakubiec@systech.com>

	* src/time.cxx: (nanosleep): Fixed to return EINTR when it is
	interrupted by a signal.  This in turn fixed sleep() to return the
	number of unelapsed seconds when interrupted by a signal.

2006-06-12  Klaas Gadeyne  <klaas.gadeyne@fmtc.be>

	* src/pthread.cxx (pthread_create): name is only defined if
	CYGVAR_KERNEL_THREADS_NAME is set to 1

2006-01-10  Nick Garnett  <nickg@ecoscentric.com>

	* tests/mutex5.c: Fixed some bugs with this test.

2006-01-05  Nick Garnett  <nickg@ecoscentric.com>

	* doc/posix.sgml: 
	* src/mutex.cxx (pthread_mutex_timedlock): 
	* include/mutex.h: Added pthread_mutex_timedlock().

	* tests/mutex5.c: 
	* cdl/posix.cdl: Added mutex timeout test.

2005-10-23  Andrew Lunn  <andrew.lunn@ascom.ch>
2005-10-18  Alexander Neundorf <neundorf@kde.org>

	* src/time.cxx: add gettimeofday() implementation
	* cdl/posix.cdl: make some descriptions a bit more verbose.  move
	mutex.cxx into its own component (CYGPKG_POSIX_PTHREAD_MUTEX).
	move compilation of mqueue.cxx into the CYGPKG_POSIX_MQUEUES
	component.  Fixed the tests so that only the ones which stand a
	chance of compling are compiled.
	* include/sys/time.h (new): Header file which implements sys/time.h 
	* include/pthread.h: Include time.h for struct timespec
	* include/mutex.h: Include time.h for struct timespec

2005-05-27  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/time.cxx (cyg_timespec_to_ticks): Only add half the number of
	ticks per us to round up, since the clock converters themselves
	round off. Otherwise nanosleep's for short periods like 10ms (which
	is 1 tick), always actually wait 2 ticks (20ms).
	(tickns): Rename to halftickns.
	(init_converters): Init halftickns by dividing what was tickns by 2.

2005-04-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/signal2.c (cause_unaligned_access): Unaligned access test not
	appropriate for M68K Coldfire.	

2004-10-01  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* src/signal.cxx:  place the CYGBLD_ATTRIB_INIT_PRI such that it
	compiles for gcc 3.4.2 which is more picky about its placement.

2004-08-02  Nick Garnett  <nickg@ecoscentric.com>

	* src/pthread.cxx (pthread_create): Append zero to end of name string.

2003-12-02  Sandeep  <sandeep@codito.com>

	* src/mqueue.cxx (new): define a placement new instead of using <new>

2003-11-19  Rickard Westman <rickard.westman@27m.se>
	
	* src/mqueue.cxx: Fix problem with mq_timedsend() and
	mq_timedreceive() timing out with zero timeouts even when there is
	room in the queue.

2003-11-17  Dan Jakubiec <djakubiec@yahoo.com>

	* src/pthread.cxx (pthread_exit): Added code to disable cancellation
	requests during thread exit.  This allows thread cleanup handlers
	to issue system calls when cleaning up thread resources.

2003-06-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/pthread.cxx (pthread_self_info): Just add some comments so
	no-one's tempted to uncomment assert.
	(pthread_create): Verify that self is a valid POSIX thread when
	needed.

2003-03-20  Mark Salter  <msalter@redhat.com>

	* include/pthread.h: Avoid conflict with recently introduced gcc
	__thread keyword.

2003-03-13  Bart Veer  <bartv@ecoscentric.com>

	* include/export.h: Only export signal-related functions if
	CYGPKG_POSIX_SIGNALS is enabled.

2003-03-04  Gary Thomas  <gary@mlbassoc.com>

	* include/pthread.h: Rework prototypes to minimize namespace problems.

2003-03-03  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/signal2.c (cause_illegal_access): PowerPC only generates
	alignment exceptions in little-endian mode, so make that a special
	case.

	* tests/mutex3.c: Include POSIX headers before feature tests to
	prevent spurious CYG_TEST_NA.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/posix.sgml: Expunge EL/IX. Dead standard.
	* cdl/posix.cdl: Add doc link.

2003-02-13  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/mutex.cxx: Include sched.hxx for scheduler lock/unlock primitives.
	Reported by Jani Monoses.

2003-02-10  Gary Thomas  <gary@mlbassoc.com>

	* tests/signal3.c (main): Reorg code so it builds with older GCC.

2003-01-31  Nick Garnett  <nickg@calivar.com>

	* src/time.cxx (alarm_action): Added call to
	cyg_posix_signal_sigwait() to wake up any sigwait()ing threads.

	* src/signal.cxx (cyg_posix_signal_sigwait): Added this function
	to export access to signal_sigwait conditional variable.
	(sigtimedwait): Added call to cyg_posix_timer_asr() to allow timer
	signals to be delivered here.

	* src/pprivate.h: Added prototype for cyg_posix_signal_sigwait().

	* cdl/posix.cdl:
	* tests/signal3.c: Added this program to test interaction of
	timers and signals, particularly sigwait(). Based on a test
	program from N.Suresh <nsuresh@cdotb.ernet.in>.

2003-01-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/signal.cxx (cyg_posix_deliver_signals): silence warning.

	* src/time.cxx (cyg_timespec_to_ticks): Remove use of default arg in
	definition.

2003-01-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/mqueue.cxx: Fix multi-line string literal warning.

2003-01-13  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/posix.sgml: Document them.

	* src/mqueue.cxx (mq_timedreceive): Make fully compliant by dealing
	with bogus timeouts.
	(mq_timedsend): Ditto.

2003-01-13  Dmitriy Korovkin  <dkorovkin@rambler.ru>

	* src/mqueue.cxx (mq_timedsend): New function. Implementing POSIX
	1003.1d draft definition.
	(mq_timedreceive): Ditto.

2002-12-10  Wade Jensen  <waj4news@cox.net>
2002-12-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/mutex.cxx (pthread_cond_timedwait): Initialize clock converters
	only once ever.

2002-11-26  Nick Garnett  <nickg@ecoscentric.com>

	* src/signal.cxx: Changed the three routines added in the last
	change so that they can be called safely from non-POSIX threads.

2002-11-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/signal.cxx: Added three exportable routines that may be used
	by other packages to manipulate the signal mask, test for
	deliverable signals, and have signals delivered at controlled
	points.

	* include/export.h: Added macros to export signal mask management,
	detection and delivery to other packages.

2002-11-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/tm_basic.cxx: Use <cyg/infra/diag.h> for diag_printf
	prototype.

2002-05-23  Jesper Skov  <jskov@redhat.com>

	* cdl/posix.cdl: Don't build tests using signals when posix
	signals are disabled.

2002-05-21  Jesper Skov  <jskov@redhat.com>

	* tests/mutex3.c: Added an NA check.

2002-04-09  Jonathan Larmour  <jlarmour@redhat.com>

	* src/signal.cxx (cyg_deliver_signals): Don't assert here for an
	unhandled signal (unless there's no _exit). Trace it though.

2002-04-08  Jonathan Larmour  <jlarmour@redhat.com>

	* src/sem.cxx (sem_getvalue): return 0, and put value in *sval.

2002-04-03  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/posix.cdl: Allow clocks to be configured again.

2002-03-05  Jesper Skov  <jskov@redhat.com>

	* src/pprivate.h: Correct conditional declaration of timespec
	functions.

	* src/sched.cxx (sched_rr_get_interval): Return ENOSYS when
	CYGPKG_POSIX_CLOCKS disabled.

2002-02-27  Robin Farine  <robin.farine@terminus.org>

	* src/pthread.cxx (pthread_exit): While running thread static
	storage destructors, set the thread's value associated with the
	current key to NULL before invoking the destructor.

2002-02-14  Nick Garnett  <nickg@redhat.com>

	* doc/posix.sgml: Generally fixed up and reformatted to make this
	file readable by mere humans. Some omissions and outdated
	information fixed, but not substantially changed from the
	original.

	* cdl/posix.cdl: Changed some definitions and dependencies so that
	disabling the timers does not disable threads too. This was
	largely a consequence of trying to document the behaviour of these
	options.
	
2002-02-14  Jonathan Larmour  <jlarmour@redhat.com>

	* doc/posix.sgml: New file, originally accompanied by this ChangeLog:
	2001-12-22  Jonathan Larmour  <jlarmour@redhat.com>
	
		* ecos-elix.sgml: Do a minor cleanup of the function prototype
		layouts.
		Should be done better than this, but this is at least not
		_completely_ wrong any more.
		Also several more layout problems due to incorrect tags fixed.
	
	2001-12-07  Jonathan Larmour  <jlarmour@redhat.com>
	
		* ecos-elix.sgml: Add getcwd as supported now.
	
	2001-12-06  Jonathan Larmour  <jlarmour@redhat.com>
	
		* ecos-elix.sgml: Created from old framemaker version.
	
2002-01-21  Jonathan Larmour  <jlarmour@redhat.com>

	* src/sched.cxx (sched_get_priority_min): Don't allow idle thread
	priority as a valid priority.
	Case #106952.

2001-12-11  Nick Garnett  <nickg@redhat.com>

	* tests/mqueue2.c (cyg_user_start): Added CYG_TEST_INIT() to
	NOTAPPLICABLE variant, otherwise the order of breakpoints are all
	wrong and the testfarm registers a failure.

2001-11-06  Gary Thomas  <gthomas@redhat.com>

	* include/muttypes.h: Need <pkgconf/kernel.h> configuration info,
	otherwise structures defined here could have the wrong size.

2001-10-25  I-Jui Sung <ijsung@csie.nctu.edu.tw>

	* src/mqueue.cxx (do_mq_unlink): Nullify table entries' mq as this
	is used by mq_open to see if the entry is used.

2001-10-11  Jesper Skov  <jskov@redhat.com>

	* tests/mutex3.c: Fixed warning. 
	(new_thread): Fixed allocation: increase counter
	before starting threads which have been allocated resources.

	* tests/signal2.c (cause_illegal_access): Fix warning.

2001-10-10  Jesper Skov  <jskov@redhat.com>

	* cdl/posix.cdl: Only build sem.cxx when the semaphores component
	is enabled.

2001-10-09  Jonathan Larmour  <jlarmour@redhat.com>

	* src/pprivate.h (pthread_info): Conditionalize signal specific
	members. Conditionalize declaration of 
	cyg_posix_pthread_release_thread().	

	* cdl/posix.cdl (CYGPKG_POSIX_CLOCKS): new option to separately
	configure posix clocks from timers.
	(CYGPKG_POSIX_TIMERS): require clocks and signals.

	* include/time.h: Make proper ISO C. Conditionalize on
	CYGPKG_POSIX_TIMERS correctly wrt the above change.

	* src/pthread.cxx (posix_asr): Call signal and timer subsystems
	conditionally.

	* src/pthread.cxx (pthread_reap): Don't destroy signal handling
	fields if there is no signal handling subsystem.
	(cyg_posix_pthread_release_thread): Conditionalize on signals.
	(pthread_create): Init signal subsys conditionally.

	* src/signal.cxx (sleep): Move to...

	* src/time.cxx: ...here.
	Conditionalize throughout depending on whether it's POSIX clocks
	or more specifically POSIX timers.
	(nanosleep): Use PTHREAD_TESTCANCEL() not pthread_testcancel().
	Get current thread from kernel not pthreads to remove pthread
	dependency.

2001-10-09  Jesper Skov  <jskov@redhat.com>

	* tests/signal2.c: Also do NA check for signals.

2001-10-01  Jonathan Larmour  <jlarmour@redhat.com>

	* src/mqueue.cxx (mq_open): Conditionalize use of sigev correctly.
	(mq_close): Similarly.

2001-09-28  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/pthread.cdl (CYGNUM_POSIX_MAIN_DEFAULT_PRIORITY): Clarify
	POSIX thread priority description.

2001-09-28  Jesper Skov  <jskov@redhat.com>

	* cdl/pthread.cdl: Changed default priority of POSIX main to
	16. This allows service threads (such as DHCP thread) to run when
	started from main().

2001-09-10  Jonathan Larmour  <jlarmour@redhat.com>

	* include/pthread.h: Separate mutex and condvar API into separate
	header file to fix configury problems.
	* include/mutex.h: New file for the above.
	* cdl/posix.cdl: provide the correct configury for the isoinfra
	package to include the above file.
	* cdl/pthread.cdl: Move _POSIX_PTHREAD_PRIO_INHERIT and
	_POSIX_THREAD_PRIO_PROTECT to cdl/posix.cdl.
	
2001-09-07  Jonathan Larmour  <jlarmour@redhat.com>

	* src/sem.cxx (sem_trywait): Actually use the return value.

	* src/sched.cxx (sched_get_priority_max): Use MAX not MIN
	(sched_get_priority_min): Use MIN not MAX.

2001-09-06  Jesper Skov  <jskov@redhat.com>

	* cdl/posix.cdl: Moved signal implements statements to the
	CYGPKG_POSIX_SIGNALS component.

2001-08-06  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/posix.cdl: Reorganize dependencies so that signals, timers
	and pthreads really can be disabled, and the relevant files don't
	get built.
	Build new mutex.cxx file.
	Remove duplicate CYGPKG_POSIX_SCHED dependency for pthreads.

	* include/limits.h: Don't include irrelevant header dependencies.

	* include/muttypes.h: New type defining mutex/cond var types separately
	from other pthread types.

	* include/types.h: Remove mutex/cond var types.

	* include/signal.h: Conditionalize on CYGPKG_POSIX_SIGNALS

	* include/sigsetjmp.h: Don't include irrelevant header dependencies.
	Rewrite sigsetjmp in a much more compiler friendly (and readable)
	way with less type punning.

	* src/misc.cxx: Don't include sysconf cases when pthreads or
	CYGPKG_POSIX_TIMERS not enabled.

	* src/mutex.cxx: New file, broken out of pthreads.cxx, as most
	of it is not fixed to the pthreads implementation, and I've fixed
	the bits that were too tied to it.

	* src/pprivate.h: Conditionalize definitions that are specific
	to CYGPKG_POSIX_PTHREAD. Ditto for prototypes for CYGPKG_POSIX_SIGNALS
	and CYGPKG_POSIX_TIMERS. Move PTHREAD_ENTRY/RETURN etc. macros
	here so they can be used throughout the package.

	* src/pthread.cxx: Remove mutex/cond var implementation, and
	entry/return macros, as per above.

	* src/signal.cxx (cyg_sigqueue): Don't just set non-queueable signals 
	pending - also forcibly wake up any blocked threads.
	(siglongjmp): Use new layout of sigjmp_buf.

	* tests/mutex3.c:
	* tests/pthread1.c:
	* tests/pthread2.c:
	* tests/pthread3.c:
	* tests/signal1.c:
	* tests/sigsetjmp.c:
	* tests/timer1.c:
	* tests/tm_basic.cxx:
	Correct configuration dependencies, and do NA appropriately.
	
2001-08-03  Nick Garnett  <nickg@cygnus.co.uk>

	Imported from a development branch:
	
	2001-06-27  Nick Garnett  <nickg@cygnus.co.uk>

		* tests/pthread3.c:
		Modified the loop that waits for the threads to get going so that
		it will function correctly in an SMP system, where the threads
		will run in parallel.

		* tests/mutex3.c: Disabled this test for SMP systems. It depends
		too much on predicting the priority-driven execution order of the
		threads. In an SMP system, some threads will run in parallel and
		falsify the assumptions.

	2001-05-25  Nick Garnett  <nickg@cygnus.co.uk>

		* src/signal.cxx (siglongjmp): Minor change to satisfy latest C++
		compiler.

2001-06-14  Jonathan Larmour  <jlarmour@redhat.com>

	* src/pthread.cxx (pthread_attr_setstacksize): Correct stack
	size assertion.

2001-06-12  Jonathan Larmour  <jlarmour@redhat.com>

	* src/pthread.cxx (MAIN_DEFAULT_STACK_SIZE): Define to use at
	least PTHREAD_STACK_MIN for main_stack.

2001-05-01  Nick Garnett  <nickg@cygnus.co.uk>

	[x86 branch]
	* tests/signal2.c (cause_illegal_access): Added code for I386
	architecture to provoke General Protection Fault. 

	* src/except.cxx: Removed some extraneous diag_printf()s.

2001-04-25  Bart Veer  <bartv@redhat.com>

	* tests/tm_basic.cxx:
	This test is now functional on the synthetic target.

2001-04-20  Jonathan Larmour  <jlarmour@redhat.com>

	* src/time.cxx (cyg_ticks_to_timespec): Actually don't bother
	with working out seconds using convertors. Instead just divide
	down ns from a long long.

2001-04-19  Jonathan Larmour  <jlarmour@redhat.com>

	* src/time.cxx (cyg_ticks_to_timespec): Clock convertors round off,
	so adjust timespec accordingly.

2001-02-14  Jonathan Larmour  <jlarmour@redhat.com>

	* include/pthread.h: Remove pthread_canceled() and
	pthread_testcancel_unlock().
	
	* src/pthread.cxx: Ditto.
	(pthread_join): Restructure to have function exit only at function end
	(pthread_cond_timedwait): Check for timeouts and return ETIMEDOUT

	* src/signal.cxx (sigtimedwait): Restructure cancellation testing

	* src/time.cxx (nanosleep): test for cancellation at the end of the
	function to keep Nick happy ;).

2001-02-11  Jonathan Larmour  <jlarmour@redhat.com>

	* include/pthread.h: Add new pthread_testcancel_unlock and
	pthread_canceled functions as eCos extensions.
	Rename existing pthread_canceled variable to pthread_cancelled_dummy_var
	
	* src/pthread.cxx (pthread_canceled): New function to interrogate if
	current thread has deferred cancel pending
	(pthread_testcancel_unlock): New function. Like testcancel, but unlocks
	a mutex before exitting the thread.
	(checkforcancel): New internal function
	(pthread_join): Add thread cancellation checks.
	(pthread_cond_wait): Ditto.
	(pthread_cond_timedwait): Ditto.
	(pthread_testcancel): Use checkforcancel()
	
	* src/sem.cxx (sem_wait): Add thread cancellation checks
	* src/signal.cxx (sigtimedwait): Ditto.
	Also make compilation of this file conditional on CYGPKG_POSIX_SIGNALS
	* src/time.cxx (nanosleep): Ditto.
	Also make compilation of this file conditional on CYGPKG_POSIX_TIMERS

	* cdl/posix.cdl (CYGPKG_POSIX_TIMERS): Implements POSIX timer ops.
	Add explicit kernel and pthread dependencies.

	* tests/sigsetjmp.c (pthread_entry1): Fix incorrect thread no. output

	* tests/pthread3.c: Add deferred cancellation test.

2001-01-11  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pthread.cxx (pthread_testcancel): Added test for self !=
	NULL in case this gets called from a non-pthread.

2000-12-22  Jonathan Larmour  <jlarmour@redhat.com>

	* src/pthread.cxx (pthread_measure_stack_usage): New function
	to measure stack usage.

	* include/pthread.h: Prototype it.

	* cdl/pthread.cdl: remove CYGNUM_POSIX_MAIN_DEFAULT_STACK_SIZE and
	instead implement CYGINT_LIBC_STARTUP_EXTERNAL_INVOKE_MAIN_POSSIBLE

	* src/pthread.cxx: Use stack size for main from libc_startup package
	to prevent confusion
	(cyg_posix_pthread_start): Likewise

2000-12-06  Jonathan Larmour  <jlarmour@redhat.com>

	* src/signal.cxx: include unistd.h for _exit

2000-11-20  Nick Garnett  <nickg@cygnus.co.uk>

	* src/signal.cxx (cyg_deliver_signals): Added else in code to
	handle SIG_DFL. Otherwise if the SA_SIGINFO bit is set we call the
	signal handler twice!

2000-11-07  Jonathan Larmour  <jlarmour@redhat.com>

	* src/signal.cxx (cyg_posix_thread_siginit): Add extra thread
	argument so that threads can inherit parent's sigmask.

	* src/pthread.cxx (pthread_create): Call with parent thread

	* src/pprivate.h: Change cyg_posix_thread_siginit prototype to take
	parent thread argument

	* tests/signal1.c: Add more checking of sigwaits, and fix so that it's
	only called when the signal is masked. Check errno values too
	sometimes.

2000-11-02  Jonathan Larmour  <jlarmour@redhat.com>

	* src/signal.cxx (sigtimedwait): return signal number on success,
	not 0
	(SIGNAL_RETURN_VALUE): New macro for returning from functions with
	valid non-zero returns
	(sigwaitinfo): Pass on sigtimedwait result with SIGNAL_RETURN_VALUE
	macro as it may return the signal number.

2000-11-01  Jonathan Larmour  <jlarmour@redhat.com>

	* src/signal.cxx (sigtimedwait): Check for SIGALRMs as a special
	case when looping as it won't have been set pending if it was
	masked.
	(check_sigalarm): New function extracted from the posix signal ASR
	(sigalrm_action): Unconditionally wake up threads waiting in sigwait
	so that they can check for pending SIGALRMs even if they were
	masked.
	(cyg_deliver_signals): Handle SIG_DFL signals properly, and check
	for bad signal handlers.
	(cyg_posix_signal_start): Initialize default signal actions to SIG_DFL

2000-10-27  Jesper Skov  <jskov@redhat.com>

	* tests/signal2.c (cause_illegal_access): Don't loop forever.

2000-10-16  Jonathan Larmour  <jlarmour@redhat.com>

	* include/sigsetjmp.h (sigsetjmp): Various fixes to make portable
	across all HALs (by avoiding CYGARC_JMP_BUF_SIZE) and remove warnings.
	* src/signal.cxx (siglongjmp): Likewise

2000-10-12  Nick Garnett  <nickg@cygnus.co.uk>

	* include/sigsetjmp.h: Added this header to define
	sigjmp_buf,sigsetjmp() and siglongjmp().

	* cdl/posix.cdl:
	Added support for providing sigsetjmp implementation and header.
	Added sigsetjmp test.

	* src/signal.cxx: Added siglongjmp().

	* tests/sigsetjmp.c: Added this test for sigsetjmp(), siglongjmp()
	functionality. This is also a test for longjmping out of signal
	handlers.

	* tests/signal2.c:
	Ifdeffed around cause_* functions to avoid compiler warnings when
	they are not needed.
	Changed CYG_TEST_NA() calls to CYG_TEST_INFO() and changed
	CYG_TEST_FINISH() to CYG_TEST_PASS_FINISH(). With the _NA's there,
	the first unsupported exception just terminates the program, and
	does not give any subsequent supported ones a chance to run.

2000-10-12  Jesper Skov  <jskov@redhat.com>

	* tests/timer1.c (main): Fix exit check.

2000-10-11  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pthread.cxx: Fixed cyg_posix_pthread_release_thread() to
	work for _DETACHED threads as well as for _RUNNING ones. Also
	fixed a bug in test to decrement counter in this routine.

	* src/pprivate.h: Added note about retaining numerical order of
	PTHREAD_STATE_* defines.

	* tests/timer1.c: Fixed some bugs of the how-did-it-ever-work
	variety.

2000-10-05  Nick Garnett  <nickg@cygnus.co.uk>

	* src/misc.cxx:
	Added a set of compatibility functions to aid portability and
	improve standards compliance.
	Added cyg_posix_function_[start|finish] to set up and terminate
	POSIX API functionality wrt signal and cancellation behaviour.
	(Lots more to do here).

	* include/export.h:
	Added this file to contain definitions that can be exported from
	the POSIX package to others.

	* src/pprivate.h: Added include of export.h
	
2000-09-11  Jonathan Larmour  <jlarmour@redhat.com>

	* include/limits.h (OPEN_MAX): Don't define here - let FS infra do
	that.
	(LINK_MAX): Ditto
	(NAME_MAX): Ditto
	(PATH_MAX): Ditto

2000-09-04  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/pthread2.c: 
	* tests/pthread3.c:
	Fixed bug in calculation of thread stack addresses.

	* src/misc.cxx (sysconf): Change zero returns to -1 when a feature
	is not supported.

2000-08-08  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/limits.h: Don't define SSIZE_MAX here, leave it to the
	isoinfra default.

2000-07-27  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/signal2.c: NA if no setjmp/longjmp

2000-07-26  Nick Garnett  <nickg@cygnus.co.uk>

	* include/pthread.h:
	* src/pthread.cxx (pthread_testcancel): Reversed addition of cyg_
	to this symbol.

2000-07-25  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/pthread.cxx: Define main_stack and main_thread as static
	Rename pthread_canceled -> cyg_pthread_canceled - pthread_ may be
	a reserved name space but this makes explicit it is implementation-
	and not standard-defined
	(PTHREAD_ENTRY_VOID): Define for funcs that take no args
	(pthread_testcancel): Call PTHREAD_ENTRY_VOID()

	* include/pthread.h: Rename pthread_canceled -> cyg_pthread_canceled

2000-07-20  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/pthread.cxx: Use isoinfra to determine presence of malloc()
	Define pthread_malloc() and pthread_free() as inlines

	* cdl/posix.cdl: Shouldn't define _POSIX_MESSAGE_PASSING at all - that
	happens in isoinfra.

2000-07-20  Nick Garnett  <nickg@cygnus.co.uk>

	* cdl/posix.cdl: Added misc.cxx to compile list. Added option to
	define _POSIX_MESSAGE_PASSING. Added configury for utsname
	structure.

	* include/utsname.h: Added this file to define struct utsname and
	uname() function prototype.

	* include/mqueue.h: Moved definition of _POSIX_MESSAGE_PASSING to
	CDL.

	* include/limits.h: Added NGROUPS_MAX definition.

	* src/pthread.cxx:
	Added support for malloced() thread stacks.
	Added implementations of pthread_mutex_setprioceiling() and
	pthread_mutex_getprioceiling().
	Changed implementations of pthread_mutex_destroy(),
	pthread_mutex_lock() and pthread_mutex_trylock() to conform more
	closely to the standard.
	Changed pthread_key_create() to assign NULL to all valid thread
	slots that correspond to a newly allocated key.

	* src/pprivate.h: Added freestack and stackmem members to manage
	malloced thread stacks.

	* src/misc.cxx: Added this file to contain functions that do not
	belong in any other files. Currently contains uname() and
	sysconf().

2000-07-19  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/startup.cxx: Remove unnecessary includes
	Use dummy object constructor to do initialization

	* cdl/posix.cdl: 
	Don't need main.cxx any more
	Build startup.cxx into extras.o (via libextras.a)

	* cdl/pthread.cdl (CYGPKG_POSIX_MAIN_THREAD):
	Integrate with CYGPKG_LIBC_STARTUP - tell CYGPKG_LIBC_STARTUP to
	let pthreads set up main thread

	* src/pthread.cxx: Integrate with CYGPKG_LIBC_STARTUP rather than
	calling main() directly.
	Track number of threads waiting to be joined, so we can tell in
	pthread_exit() if this is the last thread, and therefore whether
	to call exit()

	* src/main.cxx: obsolete, removed

2000-07-13  Nick Garnett  <nickg@cygnus.co.uk>

	* src/signal.cxx: Added ISO C compatibility functions signal() and
	raise().

2000-06-21  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pthread.cxx: Added for(;;) loop to end of pthread_exit().
	pthread_exit() is marked with the noreturn attribute, and without
	this some compilers generate a call to abort() here in case
	Cyg_Thread::exit() returns. The loop avoids this.

2000-06-06  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/mqueue.cxx (mq_receive): Fix non-portable treatment of mode flags
	(mq_send):  Ditto
	* tests/mqueue2.c (main): Ditto

2000-05-24  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/pthread2.c: Added this program to test per-thread data
	handling.

	* tests/pthread3.c: Added this program to test execution of
	cancellation handler.

	* src/pthread.cxx: Fixed some bugs revealed by new test programs.

	* cdl/posix.cdl: Added two new pthread tests.

2000-05-22  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/posix.cdl (CYGPKG_POSIX): Require
	CYGIMP_KERNEL_SCHED_SORTED_QUEUES

2000-05-20  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/mqueue1.c (cyg_user_start): Define correctly
	* tests/mqueue2.c (cyg_user_start): Likewise

	* src/pprivate.h (cyg_sigqueue): Make struct sigevent * arg const since
	it is, and it prevents warnings elsewhere
	* src/signal.cxx (cyg_sigqueue): ditto

	* tests/signal2.c: Use CYG_TEST_NA, not CYG_TEST_INFO (otherwise
	the test farm may fail the tests because there are no PASSes or NAs)

	* cdl/posix.cdl (CYGPKG_POSIX): We need errno and error codes, so
	require them
	Move some of the package implements into the components
	Add message queue configuration, build mqueue.cxx and the mqueue1 and
	mqueue2 tests
	Move some calculated options into isoinfra, implemented as interfaces
	so that unistd.h and limits.h can get the values

	* include/limits.h: Move _POSIX_* macros into isoinfra limits.h
	since they are implementation independent

	* src/mqueue.cxx: Add POSIX message queue implementation
	* tests/mqueue1.c, tests/mqueue2.c: and tests

2000-05-18  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pprivate.h:
	* src/pthread.cxx:
	* src/signal.cxx:
	* src/time.cxx:
	Added prioritization of static kernel objects.

2000-05-17  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pthread.cxx:
	To reduce the static memory required by this code, the
	pthread_info structure for a pthread is now allocated in the stack
	memory for that thread, and not in a static table. The table is
	now just an array of pointers. The per-thread data array is now
	also allocated onto the stack only when first required.

	* include/pthread.h: Removed some redundant code.

	* include/limits.h: Added PTHREAD_STACK_OVERHEAD to record
	management overhead imposed on POSIX threads stacks. This is added
	to the HAL minimum requirement to generate PTHREAD_STACK_MIN.

	* src/pprivate.h (pthread_info):
	* include/types.h (pthread_attr_t): Converted a number of integer
	state and boolean fields to bitfields.

	* cdl/pthread.cdl:
	Added requirement for CYGFUN_KERNEL_THREADS_STACK_LIMIT.

2000-05-16  Nick Garnett  <nickg@cygnus.co.uk>

	* include/types.h: Added stacksize_valid to pthread_attr_t
	structure.

	* include/signal.h:
	Added SI_EXCEPT to mark any signals that were caused by an
	exception. Removed conditions around SIGBUS.

	* src/startup.cxx (cyg_posix_start):
	Added call to cyg_posix_exception_start(). 

	* src/signal.cxx:
	Rearranged cyg_deliver_signals() so that it is possible to
	longjmp() out of a signal handler without leaving signal handling
	code in an inconsistent state.
	Added handling of SIG_IGN in sigaction().

	* src/pthread.cxx: Added setting and checking of stacksize_valid.

	* src/pprivate.h: Added cyg_deliver_signals() as an export of
	signal system. Added exports from except.cxx.

	* src/except.cxx: Added this file to handle delivery of exceptions
	into the POSIX signal mechanism.

	* cdl/posix.cdl: Added except.cxx to compile list, added signal2
	to tests. Added requirement on kernel exception processing.

	* tests/tm_basic.cxx: Tidied up a compilation warning.

	* tests/signal2.c: Added this test for exception signal generation.

	* tests/mutex3.c: Fixed stupid bug.
	
2000-05-10  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pprivate.h: Added cyg_posix_clock_start() prototype.

	* src/startup.cxx: Added call to cyg_posix_clock_start().

	* src/time.cxx: Added startup routine to initialize
	converters. Fixed error result bug in timer_delete().

	* include/signal.h: Removed some configuration tests which are now
	done in CDL.

	* cdl/posix.cdl: Added configury for the signals component. Added
	tm_basic to tests.

	* tests/tm_basic.cxx:
	Added this POSIXized version of the tm_basic test. Note that this
	has not been entirely converted. While the code being tested is
	POSIX, the timing infrastructure remains a mish-mash of kernel,
	KAPI and HAL code.

2000-05-04  Nick Garnett  <nickg@cygnus.co.uk>

	* src/time.cxx:
	Many changes to implement the delivery of signals on timer expiry.
	Also added timer_delete().

	* src/signal.cxx:
	cyg_sigqueue() and cyg_deliver_signals() may now only be called
	from within the context of a POSIX thread, either from an API call
	or an ASR.
	cyg_deliver_signals() can now cope with a signal that has
	SA_SIGINFO set but no signals queued. It also determines
	dynamically whether to lock the signal_mutex.
	cyg_deliver_signals() is no longer called implicitly from
	cyg_sigqueue() - so a number of expicit calls have been added.
	
	* src/sched.cxx:
	Added this file to implement scheduling API.

	* src/pthread.cxx:
	Moved priority translation macros to pprivate.h.
	Removed errno handling, now done in isoinfra package.
	Added iterative calls to per-thread data destructors.

	* src/pprivate.h:
	Removed error field from pthread_info structure.
	Moved priority translation macros here.
	Removed prototype for cyg_deliver_signals().
	Added prototype for cyg_posix_timer_asr().

	* include/time.h: Added timer_delete() which was mysteriously
	omitted.

	* cdl/posix.cdl: Added sched.cxx to compile list and timer1.c to
	tests.

	* tests/signal1.c: 
	* tests/pthread1.c:
	Fixed bug in use of stack sizes.

	* tests/timer1.c: 
	Added test for use of timers.
		
2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/sched.h: No longer needed - just use the default definition
	in isoinfra

	* include/errno.h: No longer needed - errno provision now comes from
	CYGPKG_ERROR
	
	* include/sys/types.h: Moved to include/types.h
	
	* cdl/posix.cdl, cdl/pthread.cdl: Put include files in cyg/posix, and
	configure CYGPKG_ISOINFRA to include the appropriate headers
	
	* include/semaphore.h: Don't need to check kernel - including
	pkgconf/kernel.h would already fail
	Give SEM_FAILED a type so casting behaves in C++
	
	* include/signal.h: This uses pid_t etc., so include <sys/types.h>
	Add signal() and raise() prototypes (to allow libc compilation, even
	though they aren't implemented yet)
	
	* include/time.h: Remove unnecessary includes. Move clockid_t and
	timer_t definitions here from sys/types.h since this is where the
	standard says they must live. 
	
	* src/pprivate.h: Include signal.h and limits.h since their contents
	are used later in the file.	

2000-04-28  Nick Garnett  <nickg@cygnus.co.uk>

	* src/signal.cxx:
	Added implementations of alarm(), pause() and sleep().
	Modified cyg_sigqueue() so that it could be called from an ASR.
	Added cyg_posix_signal_asr() to do signal processing in ASRs.
	Miscellaneous bug fixes.

	* src/pthread.cxx:
	Added pthread_count to count number of threads created.
	Added call to signal ASR function in main ASR.
	Added cyg_posix_pthread_release_thread() to seek out and kick a
	thread to which a given set of signals may be delivered.

	* src/pprivate.h:
	Added some more functions that are shared between POSIX
	subsystems.

	* include/signal.h:
	Added alarm(), pause() and sleep() prototypes. 

	* tests/signal1.c: Added this test for various aspects of signal
	handling.

	* cdl/posix.cdl: Added signal1 test.

2000-04-20  Nick Garnett  <nickg@cygnus.co.uk>

	* src/signal.cxx: Added this file to contain signal handling code.

	* src/time.cxx: Made tick<->timespec converters exported to
	rest of POSIX subsystem. Enabled interface to signal mechanism for
	notifying timer expiration.

	* src/pthread.cxx:
	Made pthread_mutex exported to rest of POSIX subsystem.
	Exported pthread_info_id().
	Added thread init and destroy functions for signal subsystem.

	* src/startup.cxx: Added call to cyg_posix_signal_start().

	* src/pprivate.h: Added signal handling fields support to
	pthread_info structure. Added extra internal interfaces to support
	signal handling code.

	* include/signal.h: Added _how_ argument values for the sigmask
	functions.

	* cdl/posix.cdl: Added signal.cxx to compile list.

2000-04-13  Nick Garnett  <nickg@cygnus.co.uk>

	* include/time.h: 
	* src/time.cxx:
	Added implementation of clock and timer functions. These are
	currently untested since they need working signals.

2000-04-12  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pprivate.h: Added cancellation support fields to
	pthread_info structure. Made pthread_self_info() exported.

	* include/semaphore.h: Added SEM_FAILED plus misc. tidies.

	* include/pthread.h: Added PTHREAD_CANCELED.

	* include/errno.h: Fixed cyg_pthread_errno_p() return type.

	* src/pthread.cxx:
	Added pthread_reap() to clean up exited threads.
	Added support for cancellation.
	Added cyg_posix_errno_p().

	* src/time.cxx:
	Added this file to implement time functionality. At present only
	nanosleep() is actually implemented.

	* src/sem.cxx:
	Added this file to implement semaphore functionality.

	* cdl/pthread.cdl:
	Added some extra configuration requirements.

	* cdl/posix.cdl:
	Added some more files to compile.
	Added semaphore configuration.

	* tests/mutex3.c:
	Added this test program. This is actually a POSIXized version of
	Hugo's splendid kernel test of the same name. It exercises quite a
	lot of the pthread infrastructure and is thus a good test to run.

	* tests/pthread1.c:
	Added proper comment headers and added full testing stuff.
	
2000-04-10  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pprivate.h: 
	* src/pthread.cxx:
	Added per-thread data support.

2000-04-06  Nick Garnett  <nickg@cygnus.co.uk>

	* src/pthread.cxx:
	Filled in implementations of lots of functions.

	* src/main.cxx:
	Added this file to contain a default main. This is currenly just a
	duplicate of the same file from the C library. Work is needed to
	combine these.

	* include/sys/types.h:
	Modified pthread_mutex_t to conform to kernel structure.

	* cdl/pthread.cdl:
	Added support for main thread.

	* cdl/posix.cdl:
	Added main.cxx to compile list.

2000-03-31  Nick Garnett  <nickg@cygnus.co.uk>

	* cdl/pthread.cdl: 
	* cdl/posix.cdl:
	Added CDL files to configure POSIX subsystem.

	* src/pprivate.h: 
	* src/pthread.cxx: 
	* src/startup.cxx: 
	Added these files to begin implementation of POSIX package.
	
	* include/pthread.h: 
	* include/sched.h: 
	* include/signal.h: 
	* include/time.h: 
	* include/sys/types.h: 
	Many changes needed by implementation work.
	
	* include/limits.h: 
	* include/errno.h: 
	Added these header files.
	
2000-03-24  Nick Garnett  <nickg@cygnus.co.uk>

	* include/sys/types.h: 
	* include/time.h: 
	* include/sched.h: 
	* include/pthread.h: 
	* include/signal.h:
	* include/semaphore.h: 
	* include/mqueue.h: 
	Roughed out (most of) the set of POSIX headers for the
	functionality we are currently going to support. These files are
	currently neither fully standard conformant nor implementation
	ready. Much work is still needed to make them so. Watch this
	space.

## ####GPLCOPYRIGHTBEGIN####                                                
## -------------------------------------------                              
## This file is part of eCos, the Embedded Configurable Operating System.   
## Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004, 2005, 2006, 2007 Free Software Foundation, Inc.
## Copyright (C) 2004, 2005, 2006, 2007 eCosCentric Limited                 
##
## This program is free software; you can redistribute it and/or modify     
## it under the terms of the GNU General Public License as published by     
## the Free Software Foundation; either version 2 or (at your option) any   
## later version.                                                           
##
## This program is distributed in the hope that it will be useful, but      
## WITHOUT ANY WARRANTY; without even the implied warranty of               
## MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
## General Public License for more details.                                 
##
## You should have received a copy of the GNU General Public License        
## along with this program; if not, write to the                            
## Free Software Foundation, Inc., 51 Franklin Street,                      
## Fifth Floor, Boston, MA  02110-1301, USA.                                
## -------------------------------------------                              
## ####GPLCOPYRIGHTEND####