2006-09-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/arm_cerf_disk_cf_drivers.inl (IDE_DISK_INSTANCE):
	DISK_CHANNEL and DISK_CONTROLLER are now implicitly static.
	Update DISK_CHANNEL for new io/disk macro definition.

2004-04-15  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/arm_cerf_disk_drivers.cdl: 	
	* include/arm_cerf_disk_cf_drivers.inl:
	Moved interrupt to GPIO22. However, this does not seem to work
	very well, so at present the device is polled only.

2004-02-16  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/arm_cerf_disk_drivers.cdl: 
	* include/arm_cerf_disk_cf_drivers.inl: 
	New package. Contains confguration and platform dependent code for
	CerfCube Compact Flash devices.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2006 Free Software Foundation, Inc.                  
// Copyright (C) 2004, 2006 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================