2008-08-19  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/synthdisk.cdl: Renamed the disk device to /dev/synthdiskX to
	be unique with respect to other disk drivers. Remove the test
	configury which is not used anywhere.
	
2008-04-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/synthdisk.cdl (CYGNUM_IO_DISK_ECOSYNTH_DISK0_SIZE): Increase
	upper limit on size to near 4GB to allow for multi-gig "disks".

2007-06-27  Nick Garnett  <nickg@ecoscentric.com>

	* src/synthdisk.c (synth_disk_lookup): Initialize ident.sector_size.

2006-02-03  Nick Garnett  <nickg@ecoscentric.com>

	* src/synthdisk.c: Updated to match changes in io/disk package.

2004-07-01  Savin Zlobec  <savin@elatec.si> 

        * src/synthdisk.c:
        Updated to work with the new DISK_CHANNEL macro definition.

2004-04-15  Nick Garnett  <nickg@ecoscentric.com>

	* src/synthdisk.c: Mildly reorganized to support changeable
	media. Added synth_disk_change() function to allow us to fake a
	disk change for testing purposes.

2004-02-05  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/synthdisk.cdl: Added testing config options, plus
	define_proc to export CYGDAT_DEVS_DISK_CFG include file name.

2004-01-30  Nick Garnett  <nickg@ecoscentric.com>

	* src/synthdisk.c: Updated to latest disk device specification.

2004-01-15  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/synthdisk.cdl:
	* src/synthdisk.c: 	
	Added _FILENAME option for disk instances to map device to an
	arbitrary configured file.
	
	* src/synthdisk.c: Removed block_pos arguments from read
	and write calls: it is not necessary.

2003-09-01 Savin Zlobec <savin@elatec.si>

        * cdl/synthdisk.cdl: 
        * src/synthdisk.c: 
        Updated to work with the current disk interface.

2003-08-19 Savin Zlobec <savin@elatec.si>

        * cdl/synthdisk.cdl:
        * src/synthdisk.c:
        A synthetic block device driver.



//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2003, 2004, 2006, 2007, 2008 Free Software Foundation, Inc.
// Copyright (C) 2004, 2006, 2007, 2008 eCosCentric Limited                 
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================