2008-12-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_cs8900a.c (cs8900a_send): Add timeout limit after transmission.

 2009-02-28  Sergei Gavrikov  <sergei.gavrikov@gmail.com>
	
        * src/if_cs8900a.c: Fixed interrupt hooking block in cs8900a_init() to
        prevent assertion fail on cyg_interrupt_attach() when interrupt is not
        used.
	
2008-11-07  Sergei Gavrikov <sergei.gavrikov@gmail.com>

	* cdl/cl_cs8900a_eth_drivers.cdl: Added
	CYGIMP_DEVS_ETH_CL_CS8900A_DATABUS_8BIT option to manage chip in 8-bit
	mode.
	* include/cs8900.h
	* src/if_cs8900a.c: Added a support for the 8-bit access for CS8900A.
	All access to CS8900A registers wrapped via CS_IN, CS_OUT macros (the
	macros were defined in past, but, still not used).  In common way the
	macros use the eCos macros: HAL_READ_UINT16, HAL_WRITE_UINT16 , but,
	in other (rare) conditions they can use 8-bit access too.

2007-09-04  Stephen Finney <shf@pfinc.com>

	* add timeout to potential infinite loop in cs8900a_send per 
	bugzilla report 1000281

2005-11-10  Laurent Gonzalez <laurent.gonzalez@trango-systems.com>

	* include/cs8900a.h:
	* src/if_cs8900a.c: Added a priority field in cpd
	that makes interrupt priority configurable

2005-05-04  Ian Campbell  <icampbell@arcom.com>

	* cdl/cl_cs8900a_eth_drivers.cdl: Added
	CYGSEM_DEVS_ETH_CL_CS8900A_WRITE_EEPROM

	* src/if_cs8900a.c: Added debug statements to print out where the
	driver is obtaining its ESA from. Implement
	ETH_DRV_SET_MAC_ADDRESS and ETH_DRV_GET_MAC_ADDRESS.

2004-07-16  Nick Garnett  <nickg@ecoscentric.com>

	* include/cs8900.h: Added extra fields to cs8900a_priv_data_t
	structure to record all parameters of current transmission for
	cs8900a_send_data(). Added event counters.

	* src/if_cs8900a.c: Several general changes: added event counters
	in various places; added further debug messages.
	(cs8900a_int_vector): Fixed return value.
	(cs8900a_init): Added loop to wait for link to come up or timeout
	and return false. This speeds up RedBoot startup both when the
	ethernet is unplugged and when it is slow to negotiate.
	(cs8900a_BufEvent): 
	(cs8900a_send_data): 
	(cs8900a_send): Changed to use Rdy4Tx interrupt when transmitter
	not ready. In non-interrupt case, handle completion of
	transmission when interrupts are disabled.
	(cs8900a_start): Only set transmit interrupt enable bits for
	interrupt based systems. Receive interrupts remain enabled to
	handle Ctrl-C from GDB.

2004-06-29  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/if_cs8900a.c: Added missing include of cyg_ass.h.

2004-05-07  Bob Koninckx <bob.koninckx@o-3s.com>

	* src/if_cs8900a.c: Drop "ghost" frames with zero length

2004-04-19  Bob Koninckx <bob.koninckx@o-3s.com>

	* src/if_cs8900a.c: function cs8900a_int_vector, return the vector
	instead of a boolean.

2004-04-08  Bob Koninckx <bob.koninckx@o-3s.com>
	* cdl/cl_cs8900a_eth_drivers.cdl
	* include/if_cs8900a.c
	* src/if_cs8900a.c: Made hardware swapping or software swapping of
	data bytes (mostly relevant to big endian machines) a
	configuration option

2003-11-05  Bob Koninckx <bob.koninckx@mech.kuleuven.ac.be>

	* src/if_cs8900a.c: Fix handling of odd bytes on big endian machines

2003-04-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_cs8900a.c (cs8900a_send): Allow for data not being 16-bit
	aligned. Thanks to Laurent Gonzalez <laurent.gonzalez@ri.silicomp.fr>
	for reporting this and his initial patch.

2003-03-03  Bob Koninckx  <bob.koninckx@mech.kuleuven.ac.be>
	
	* src/if_cs8900a.c:
	* include/cs8900a.h:
	Changes to support both little and big endian targets

2002-06-14  Gary Thomas  <gary@chez-thomas.org>

	* src/if_cs8900a.c: 
	Need to include <pkgconf/io_eth_drivers.h> for proper configuration
	of stand-alone (polled) vs. system (interrupt driven) mode.

2002-05-30  Jonathan Larmour  <jlarmour@redhat.com>

	* include/cs8900.h: Check for lost ints if we can - when kernel present.
	* src/if_cs8900a.c: Use CYGINT_IO_ETH_INT_SUPPORT_REQUIRED where
	appropriate.

2002-03-20  Gary Thomas  <gthomas@redhat.com>
2002-03-06  Pieter Truter <ptruter@intrinsyc.com>

	* src/if_cs8900a.c (cs8900a_isr): Need to acknowledge interrupt
	here (in case DSR/poll causes a new one to occur).	

2002-02-18  Gary Thomas  <gthomas@redhat.com>

	* cdl/cl_cs8900a_eth_drivers.cdl: 
	Add new interface CYGINT_IO_ETH_MULTICAST which is used to
	insure that drivers support multicast addresses if IPv6 is used.

2002-02-15  Gary Thomas  <gthomas@redhat.com>

	* include/cs8900.h: 
	* src/if_cs8900a.c (cs8900a_control): Support multicast addresses.

2002-02-04  Gary Thomas  <gthomas@redhat.com>

	* src/if_cs8900a.c: 
	* include/cs8900.h: Add CYGHWR_CL_CS8900A_PLF_POST_RESET() macro.

2001-11-29  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c (cs8900a_init): Changed order of ESA source
	checking so user can always override at RedBoot runtime.

2001-11-20  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c: Added some more debug output. Set all 4 LAF
	registers. Don't reset device to stop it - just disable TX & RX.

2001-11-16  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c (cs8900a_send): Wait for controller ready
	signal before starting transmission.

2001-11-14  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c: Use platform init, reset and int_clear
	macros.
	* include/cs8900.h: Tidy up those (default) macros.

2001-11-09  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c (cs8900a_init): Rewrote ESA setup to be more
	consistent.

	* include/cs8900.h: Added provide_esa field to driver structure.

2001-11-08  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c: Made it build with faked interrupts.

	* include/cs8900.h: Added debug output for put/get functions.

	* src/if_cs8900a.c: Made it build when NET package enabled.

	* include/cs8900.h: Added tab field.

	* src/if_cs8900a.c: Renamed broken ints option, more diag_printf
	#ifdefing and removed RedBoot ESA option code.

2001-11-07  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c: Interrupt stuff cleaned up. Fix device
	probing. Make driver fail when no ESA available and none has been
	configured. Compiler warning fixes and some printout cleanups.

	* src/if_cs8900a.c: Platform driver provides device
	information. Renamed functions and definitions. Init code changed
	some.

	* include/cs8900.h: Renaming some definitions.

	* cdl/cl_cs8900a_eth_drivers.cdl: Platform driver provides
	options.

2001-11-06  Jesper Skov  <jskov@redhat.com>

	* src/if_cs8900a.c: Assorted hacking.
	* include/cs8900.h: Same.

2001-11-02  Jesper Skov  <jskov@redhat.com>

	* Cloned from edb7xxx driver.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
// Copyright (C) 2004 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================