2004-10-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (pci_init_find_21143s): Allow device specific
	drivers to override initial interrupt priority.

2004-09-23  John Dallaway  <jld@ecoscentric.com>

	* src/if_i21143.c (i21143_reset): Revert to longer PHY link timeout.

2004-09-22  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (i21143_reset): Use smaller PHY link timeout.

2004-09-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (i21143_init): Allow device specific drivers to
	provide functions to provide an ESA override, primarily to allow
	RedBoot configuration of ESA in Flash.

2004-09-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (i21143_reset): Decrease wait for link.

2004-09-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (find_21143s_match_func): Allow device specific
	drivers to supply extra PCI IDs to match.
	Avoid memcpy undeclared warning.
	(eth_set_mac_address): Allow device specific drivers to override ESA
	set.
	(i21143_init): Allow device specific drivers to override ESA get.
	Use a less ambiguous default ESA if the retrieved one is bad.
	(i21143_send): Fall back to HAL_DCACHE_FLUSH or HAL_DCACHE_SYNC if
	HAL_DCACHE_STORE isn't defined but they are.
	Give option of dumping tx packet data.

2004-09-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c: Support device specific override of PHY/MII
	access.
	(find_21143s_match_func): Recognise STE10/100A PCI ID.

2004-09-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/if_i21143.c (i21143_send): Only call HAL_DCACHE_STORE if defined.

2001-10-05  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c (MII_DELAY): Greatly reduce this, now it's
	working, so that we can poll for link status changes.  I don't see
	any other way to do this, since we would not necessarily be
	transmitting (to get a link fail code) when a person re-plugs the
	line.
	(i21143_status_changed): New function; a quicker test for
	negotiated line status changed.  Polled from the deliver routine.

2001-10-05  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c (i21143_ioctl): Implement SNMP statistics.
	(i21143_can_send): Enable the "unsticking" poll of tx and rx
	states; it seems not necessary, but it's also definitely not
	harmful.
	(generally): manage getting the link status better; it takes time
	so cache the answer.  Reset the system if it changed between
	_stop() and _start().

2001-10-04  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c (i21143_reset): Set the "store and forward" bit
	so that we can keep up with large transmits at 100Mbit.  Otherwise
	it underflows for packets of 700 bytes or so.

2001-10-04  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c: Got ESA filtering set up OK by using perfect
	filtering instead, with all the broadcast address except one with
	our true ESA.  Various changes to the debug printing too.

2001-09-28  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c (i21143_init): Read the good ESA (MAC address)
	from the serial EEPROM (or ROM) and use it if valid.

2001-09-28  Hugo Tyson  <hmt@redhat.com>

	* src/if_i21143.c: Duh.  Fix dangerously aliased local variable.
	Having a thing like int fred[0] on the stack tends to screw up
	other random variables.

2001-09-27  Hugo Tyson  <hmt@redhat.com>

	* cdl/intel_i21143_eth_drivers.cdl: New file.

	* src/if_i21143.c: New file.  Not working yet.
	Reception only occurs if "Receive All" CSR_OPMODE_RA is set.
	No transmission occurs to the wire though the machinery all works
	beautifully.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
// Copyright (C) 2004 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================