2008-11-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_intel_28fxxx.cdl: Indicate that this driver uses
	the legacy flash device API.

2008-09-04  Dave Lawrence <dlawrence@ad-holdings.co.uk>

	* include/flash_28fxxx.inl: 
	* include/flash_28fxxx_parts.inl: Support write buffering. Add an
	entry to the parts table indicating the size of the buffer and
	copy it into the device table during initialization. 

2006-12-14  Yoshinori Sato <ysato@users.sourceforge.jp>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx_parts.inl: Add
	Intel 28F320J3 part.

2006-11-28  Sergei Gavrikov  <sg@sgs.gomel.by>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx_parts.inl:
	Add Intel 28F160C3-B part.

2006-11-21  Alexander Neundorf <alexander.neundorf@jenoptik.com>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx_parts.inl:
	Add Intel 28F128K3, 28F128P30 and 28F128J3 parts.

2006-11-17  Alexander Neundorf <alexander.neundorf@jenoptik.com>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx.inl: 
	Make the timeout configurable by adding a new CDL-option 
	CYGNUM_DEVS_FLASH_INTEL_28FXXX_TIMEOUT

2006-05-10  Sergei Gavrikov <sg@belvok.com>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx_parts.inl: Add
	Intel 28F160B3-T part.

2005-09-15  Nick Garnett  <nickg@ecoscentric.com>

	* include/flash_28fxxx_parts.inl: Fixed up some errors in ST
	M58WR064 part description.

2005-08-17  Nick Garnett  <nickg@ecoscentric.com>

	* include/flash_28fxxx.inl: Modified to support multi-bank
	devices.

	* cdl/flash_intel_28fxxx.cdl: 
	* include/flash_28fxxx_parts.inl: Added ST M58WR064 part.
	
2005-04-22  David Vrabel  <dvrabel@arcom.com>

	* cdl/flash_intel_28fxxx.cdl, include/flash_28fxxx_parts.inl: Add
	Intel 28F800B5-T and 28F800B5-B parts.
	
2004-08-03  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/flash_intel_28fxxx.cdl: Indicate we need the legacy device API

2002-12-12  Gary Thomas  <gthomas@ecoscentric.com>
2002-12-12  Patrick Doyle <wpd@delcomsys.com>

	* include/flash_28fxxx_parts.inl: 
	* include/flash_28fxxx.inl: 
	* cdl/flash_intel_28fxxx.cdl: Add SHARP 28F016 parts.

2002-08-05  Gary Thomas  <gary@chez-thomas.org>
2002-08-05  Jani Monoses <jani@iv.ro>	

	* include/flash_28fxxx_parts.inl: 
	* cdl/flash_intel_28fxxx.cdl: Add support for 28F320B3.

2002-03-06  Nick Garnett  <nickg@redhat.com>

	* include/flash_28fxxx.inl: 
	Added CYGHWR_FLASH_WRITE_ENABLE() and CYGHWR_FLASH_WRITE_DISABLE()
	macro calls to enable and disable FLASH writing in platform
	hardware. Some platforms have extra protection for the FLASH
	beyond that provided for the FLASH itself.
	
	* include/flash_28fxxx_parts.inl: 
	* cdl/flash_intel_28fxxx.cdl:
	Added support for the 28f320S3 part. This mainly differs from the
	C3 in that it does not have any bootblocks.

2001-10-17  Jonathan Larmour  <jlarmour@redhat.com>

	* include/flash_28fxxx_parts.inl: Fix boot block start address.

2001-08-15  Jesper Skov  <jskov@redhat.com>
	[from branch]
	* include/flash_28fxxx_parts.inl: Set correct bootblock sub-block
	sizes.

	* include/flash_28fxxx.inl (nDEBUG): Added some debug code.
	(flash_unlock_block, flash_lock_block): Iterate properly over
	bootblock sub-blocks.

2001-08-10  Jesper Skov  <jskov@redhat.com>

	* cdl/flash_intel_28fxxx.cdl: Added options for variants.

	* include/flash_28fxxx.inl: Support bootblock parts. Support
	locking. Buffered writes are broken though.
	Which affects the Malta, which uses them.

	* include/flash_28fxxx_parts.inl: Created.

2001-06-29  Jesper Skov  <jskov@redhat.com>

	* include/flash_28fxxx.inl: Fix 28F160 block size.

2001-06-20  Jesper Skov  <jskov@redhat.com>

	* include/flash_28fxxx.inl (flash_hwr_init): Fix bad size
	calculations.

2001-05-23  Jesper Skov  <jskov@redhat.com>

	* cdl/flash_intel_28fxxx.cdl: Links flash functions to RAM. IO
	driver should not copy them there.

2001-03-23  Jesper Skov  <jskov@redhat.com>

	* include/flash_28fxxx.inl (flash_program_buf): Calculate correct
	wc for buffered writes.
	(flash_query): Don't return until flash is safely back in data
	mode.

2001-03-21  Jesper Skov  <jskov@redhat.com>

	* Package cloned from at29cxxxx driver. Changed to support Intel
	FlashFile.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================