2009-02-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/flash2.c (cyg_user_start): Call cyg_flash_init() with
	NULL argument.
	* tests/flash3.c (cyg_user_start): Ditto.

2009-02-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/flash2.c (cyg_user_start): Update for minor flash API
	mod to call cyg_flash_set_global_printf() to set printf
	function.
	* tests/flash3.c (cyg_user_start): Ditto.

2008-12-23  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/synth.c: Implemented simulation of proper NOR flash writes.
	General cleanup.

2008-12-18  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/synth.c: Fixed error check of mmap call.

2008-11-28  Sergei Gavrikov  <sergei.gavrikov@gmail.com>

	* tests/flash[23].c: Fixed copy'n'paste typos in a naming: flash1 ->
	flash{2,3}.

2008-11-19  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/synth.c: Removed cyg_hal_sys_do_mmap() wrapper function.
	* tests/flash1.c, tests/flash2.c, tests/flash3.c:
	Fixed a few compiler warnings.

2007-01-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_synth.cdl: Add optional delays for programming
	(CYGNUM_FLASH_SYNTH_V2_PROGRAM_DELAY) and erasing
	(CYGNUM_FLASH_SYNTH_V2_ERASE_DELAY), to	better mimic real flash
	devices.

	* src/synth.c: Add optional delays for programming and erasing, to
	better mimic real flash devices.

2004-12-02  Bart Veer  <bartv@ecoscentric.com>

	* include/synth.h, src/synth.c: explicitly include
	<cyg/io/flash_dev.h> rather than just defining _FLASH_PRIVATE_

2004-11-29  Bart Veer  <bartv@ecoscentric.com>

	* src/synth.c: eliminate hwr_map_error() support, no longer needed
	
	* src/synth.c: use the dummy lock/unlock functions provided by the
	generic flash package.

2004-11-22  Bart Veer  <bartv@ecoscentric.com>

	* include/synth.h, src/synth.c, tests/flash3.c: merge the config
	and priv structures. Adjust device driver API as per changes to
	the generic flash code.
	* tests/flash2.c, tests/flash3.c: do not depend on both synthetic
	flash drivers being loaded.
	* include/synth.h (struct cyg_flash_synth_priv): rename
	cyg_block_info to cyg_flash_block_info

2004-11-21  Bart Veer  <bartv@ecoscentric.com>

	* tests/flash1.c (cyg_user_start):
	CYGSEM_IO_FLASH_LEGACY_DEVICE_API has been removed, use
	CYGHWR_IO_FLASH_DEVICE_LEGACY instead
	* cdl/flash_synth.cdl: CYGHWR_IO_FLASH_DEVICE_V2 is now implicit

2004-09-14  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/synth.c (synth_flash_erase_block): Remove asserts which are
	no longer true.

2004-09-09  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/flash_synth.c: Allow the use of arbitary sized block.
	* test/flash3.c: Allow the use of small blocks

2004-08-21  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/flash[23].c: Removed calls to cyg_flash_get_block_info()
	and cyg_flash_get_limits() which have been removed. 

2004-08-03  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/flash_synth.cdl: Indicate we use the V2 device API.

2004-07-17  Andrew Lunn  <andrew.lunn@ascom.ch>

	* First version. Implements synthetic flash using the new flash
	API.
 	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
// Copyright (C) 2004, 2007 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================