2008-12-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/ser_arm_lpc2xxx.cdl: Use new
	CYGPKG_IO_SERIAL_GENERIC_16X5X_XMIT_REQUIRE_PRIME option to kick off
	TX interrupts when device is idle (previously this was forced as
	standard behaviour).

2008-02-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/ser_arm_lpc2xxx.cdl: Allow platform to override default serial1
	state, to indicate that RTS/CTS or modem control lines are not
	in practice physically connected.

2004-09-01  John Dallaway  <jld@ecoscentric.com>

	* cdl/ser_arm_lpc2xxx.cdl: Make CYGPRI_SER_TEST_TTY_DEV configurable.

2004-08-04  Jonathan Larmour  <jlarmour@ecoscentric.com>

	* New package -- serial driver for Philips LPC2xxx on-chip UARTs.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2008 Free Software Foundation, Inc.                  
// Copyright (C) 2004, 2008 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================