2006-10-05  Nick Garnett  <nickg@ecoscentric.com>

	* include/spi_atmel_at91rm9200_kits.h: Added additional bus number
	parameter to relevant macros.

2006-05-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/spi_atmel_at91rm9200_kits.h: Tweaks that may allow use of
	NPCS0 in future. But for now these are not properly enabled yet in
	the absence of a supporting device..

2005-09-28  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/spi_atmel_at91rm9200-kits.cdl: Use new
	CYGBLD_HAL_SPI_PLF_DEFINITIONS_H define to indicate header for SPI
	to include.

	* include/spi_atmel_at91rm9200_kits.h (CYGHWR_SPI_DETECT_DATAFLASH):
	New macro to allow for detection of dataflash in socket.

2005-08-18  Nick Garnett  <nickg@ecoscentric.com>

	* src/spi_atmel_at91rm9200_kits.c: 
	* include/spi_atmel_at91rm9200_kits.h: 
	* cdl/spi_at91rm9200-kits.cdl:
	New package -- SPI customization for Atmel AT91RM9200
	Evaluation/Development Kits.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2005, 2006 Free Software Foundation, Inc.
// Copyright (C) 2005, 2006 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================