2009-05-12  Ross Younger  <wry@eCosCentric.com>

	* src/strerror.cxx: Add missing ENOTEMPTY.

2008-07-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/strerror.cxx (__strerror): Silence warnings on newer
	GCC by assigning string literals to a const char * var.

2006-10-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/codes.h (EFAULT): Add.
	* src/strerror.cxx (__strerror): Add EFAULT.

2003-06-24  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/codes.h (ENOTEMPTY): Needed by the sysctl call in the
	freeBSD stack.

2001-11-29  Jonathan Larmour  <jlarmour@redhat.com>

	* include/errno.h: Don't use 'const' type qualifier any more. It
	gives warnings in new compilers now.
	* src/errno.cxx (cyg_error_get_errno_p): Ditto.

2000-06-19  Nick Garnett  <nickg@cygnus.co.uk>

	* include/errno.h (errno): Added extern modifier to non-per-thread
	instance of errno.

2000-06-07  Nick Garnett  <nickg@cygnus.co.uk>

	* src/strerror.cxx: 
	* include/codes.h: Added ESPIPE.

2000-06-02  Nick Garnett  <nickg@cygnus.co.uk>

	* include/codes.h:
	* src/strerror.cxx: Added some more codes.
	
2000-05-31  Nick Garnett  <nickg@cygnus.co.uk>

	* src/strerror.cxx: 
	* include/codes.h:  Added EXDEV.

2000-05-20  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/codes.h: Add EDEADLOCK synonym for EDEADLK
	Add ENFILE
	* src/strerror.cxx: Add blurb for ENFILE, ENOSPC, EDEADLK and ENOTSUP

2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/codes.h: No need to conditionalize codes on CYGPKG_NET
	Tidy a bit.
	* src/errno.cxx: Move here from libc. Use kernel constant
	per-thread data slot, not a dynamic one. Generally tidy.
	* src/strerror.cxx: No need to conditionalize codes on CYGPKG_NET.
	Tidy a bit.	

2000-03-31  Nick Garnett  <nickg@cygnus.co.uk>

	* include/codes.h: Added some further codes.

2000-01-11  Gary Thomas  <gthomas@cygnus.co.uk>

	* src/strerror.cxx (_strerror): 
	* include/codes.h: Add in additional errors require to support
	networking.

1999-04-14  John Dallaway  <jld@cygnus.co.uk>

	* include/pkgconf/error.h: Add cdl_package doc attribute.

1998-09-11  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/error.h:
	Sorting out dependencies for error package.

Mon Aug 24 17:51:08 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/error.h: 
	Add CDL for this package, for the configuration system.

Wed Aug 12 11:04:27 BST 1998  Chris Provenzano  <proven@cygnus.com>

        * Changelog: Initial ChangeLog entry.
	* include/codes.h: #include <cyg/infra/cyg_type.h> for define
	of externC.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2006, 2008 Free Software Foundation, Inc.
// Copyright (C) 2006, 2008 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================