2009-08-28  Nick Garnett  <nickg@ecoscentric.com>

	* src/lm3s_misc.c (hal_lm3s_gpio_set): Fix some problems in GPIO
	configury.

	* include/var_io.h (CYGHWR_HAL_LM3S_GPIO): Add drive parameter,
	and change all calls to match.
	Add I2C, SPI and ethernet definitions.
	
	* src/lm3s_i2c.c: 
	* cdl/hal_cortexm_lm3s.cdl: Add I2C support.

	* doc/lm3s.sgml: Add variant documentation.

2009-07-30  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_cortexm_lm3s.cdl:
	* include/hal_cache.h:
	* include/hal_diag.h:
	* include/plf_stub.h:
	* include/var_arch.h:
	* include/var_intr.h:
	* include/var_io.h:
	* include/variant.inc:
	* src/hal_diag.c:
	* src/lm3s_misc.c:
	New package -- Luminary Micro LM3S variant HAL.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2008, 2009 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================