2008-10-27  Nick Garnett  <nickg@ecoscentric.com>

	* include/config_keys.h (CYG_IO_SET_CONFIG_SERIAL_TERMINALREADY):
	Add this option to permit control of DTR line.

2008-05-14  Nick Garnett  <nickg@ecoscentric.com>

	* include/config_keys.h	(CYG_IO_GET_CONFIG_SERIAL_CARRIERDETECT):
	Add this for serial line DCD polling.
	(CYG_IO_GET_CONFIG_ADC_*): Add config keys for ADC devices.

2007-08-13  Alexey Shusharin <mrfinch@mail.ru>

	* include/config_keys.h: Added key set setting CAN callback
	configuration.
	
2007-05-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/config_keys.h (CYG_IO_GET_CONFIG_FLASH_DEVADDR):
	Add this new key.

2007-04-30  Nick Garnett  <nickg@ecoscentric.com>

	* include/config_keys.h (CYG_IO_GET_CONFIG_DISK_EVENT) 
	(CYG_IO_SET_CONFIG_DISK_EVENT): Added new keys for disk event
	function registration.

2006-09-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/config_keys.h: Merge from eCosCentric repository.
	ChangeLogs incorporated in correct location below.

2006-04-05  John Dallaway  <jld@ecoscentric.com>

	* doc/io.sgml: Correct values for CYG_TTY_IN_FLAGS_BINARY and
	CYG_TTY_IN_FLAGS_ECHO.

2006-02-15  Uwe Kindler  <uwe_kindler@web.de>

	* include/config_keys.h Replaced CAN configuration keys
	CYG_IO_SET_CONFIG_CAN_REMOTE_BUF, 
	CYG_IO_SET_CONFIG_CAN_FILTER_ALL and
	CYG_IO_SET_CONFIG_CAN_FILTER_MSG with new single config key
	CYG_IO_SET_CONFIG_CAN_MSGBUF

2005-12-02  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/iosys.c: 
	* include/devtab.h: Add comments that bread/bwrite takes there
	parameters in blocks, not bytes.

2005-09-11  Uwe Kindler  <uwe_kindler@web.de>

	* include/config_keys.h Configuration keys for CAN driver added. 
	
2005-01-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/config_keys.h: Add device close key.

2004-12-23  Peter Korsgaard  <jacmet@sunsite.dk>

	* doc/io.sgml: Match CYG_TTY_IN_FLAGS_ECHO and
	CYG_TTY_IN_FLAGS_BINARY values with source code.

2004-09-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/io.sgml: Rename incorrect cyg_drv_mutex to cyg_drv_mutex_t.
	Ditto cyg_drv_cond and cyg_drv_cond_t.

2004-04-16  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/iosys.c (cyg_io_lookup): Use union to avoid aliasing problems
	with compiler.

2004-04-15  Nick Garnett  <nickg@ecoscentric.com>

	* include/config_keys.h: Added CYG_IO_SET_CONFIG_DISK_MOUNT and
	CYG_IO_SET_CONFIG_DISK_UMOUNT keys.

2004-01-19  Nick Garnett  <nickg@ecoscentric.com>

	* include/config_keys.h (CYG_IO_GET_CONFIG_DISK_INFO): Added DISK
	IO config key base definition.

2003-11-27  David Woodhouse  <dwmw2@infradead.org>

	* include/config_keys.h: Add CYG_IO_SET_CONFIG_FLASH_FIS_NAME

2003-11-06   Billy <billy@babababa.net>

	* doc/io.sgml: In the TTY section swap "\n\r" to "\r\n" to match
	reality.
	
2003-03-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/config_keys.h: Define CYG_IO_SET_CONFIG_SERIAL_OUTPUT_FLUSH
	to be same as CYG_IO_GET_CONFIG_SERIAL_OUTPUT_FLUSH.
	Ditto for ..._INPUT_FLUSH.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/io.cdl: Fix doc link.

2002-03-12  Nick Garnett  <nickg@redhat.com>

	* doc/io.sgml: Generally sorted out, reformetted, folded. SMP
	considerations added to various parts of the document.

2002-01-23  Jonathan Larmour  <jlarmour@redhat.com>

	* include/config_keys.h: Add config keys for flash block drivers.

2001-09-27  Jonathan Larmour  <jlarmour@redhat.com>

	* src/io_diag.c: Delete. No longer used.
	* cdl/io.cdl: Don't build io_diag.c.

2001-04-18  Jesper Skov  <jskov@redhat.com>
	Case 105926
	* src/io_file.c (falloc): Don't return -EMFILE, but EMFILE. Found
	by Andrew Lunn.

2000-11-22  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/io.cdl: Only put ioinit.cxx in extras.o. Build others normally.
	* src/iosys.c: Move devtab table definition from here....
	* src/ioinit.cxx: .... to here

2000-11-21  Bart Veer  <bartv@redhat.com>

	* src/iosys.c: 
	* include/devtab.h:
	Add dummy implementations for select, get_config and set_config

2000-09-07  Jesper Skov  <jskov@redhat.com>

	* include/devtab.h (cyg_devtab_entry_t): Fix syntax problem.

2000-09-04  Jonathan Larmour  <jlarmour@redhat.com>

	* include/devtab.h (cyg_devtab_entry_t): Apply CYG_HAL_TABLE_TYPE	

2000-08-01  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/config_keys.h: 
	Add keys to support flow control, line status callbacks,
	hardware breaks and termios.

2000-07-31  Nick Garnett  <nickg@cygnus.co.uk>

	* include/config_keys.h: Added generic keys for controlling
	BLOCKING behaviour, and added aliases to retain compatibility.

2000-07-25  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/devtab.h: Define cyg_devio_cwrite, _cread, _bwrite and _bread
	with C linkage

2000-07-21  Nick Garnett  <nickg@cygnus.co.uk>

	* include/io.h: 
	* include/devtab.h: 
	* src/iosys.c:
	Added support for block devices. At present this is really just
	exploiting the perturbations that the EL/IX branch merge will
	cause to add placeholders for future developments.
	These changes consist mainly of adding bwrite() and bread()
	entries in the cyg_devio_table_t structure and adding a char/block
	discriminator flags to the devtab entry status field. API calls
	cyg_io_bwrite() and cyg_io_bread() have also been added.
	Suitable definition of macros means that no existing driver code
	needs to be changed to accomodate this addition.

2000-06-19  Nick Garnett  <nickg@cygnus.co.uk>

	* src/iosys.c: 
	* include/devtab.h:
	Converted to new table construction mechanism.

2000-06-15  Nick Garnett  <nickg@cygnus.co.uk>

	* include/io.h: 
	* src/iosys.c: Added cyg_io_select().

	* include/devtab.h: Added select() support function to
	cyg_devio_table_t structure. Modified DEVIO_TABLE() macro
	to match.

2000-06-09  Nick Garnett  <nickg@cygnus.co.uk>

	* include/file.h: Added redefinition of CYG_SELINFO_TAG.

2000-06-07  Nick Garnett  <nickg@cygnus.co.uk>

	* include/file.h: Added definitions to make this header work with
	the fileio package.

	* cdl/io.cdl: Moved support for files into a sub-component that is
	only active if the FILEIO package is not present.

2000-05-05  Grant Edwards  <grante@visi.com>

	* include/config_keys.h: Add key to inquire about serial buffer info

2000-05-03  Jesper Skov  <jskov@redhat.com>

	* include/config_keys.h: Added keys for DSP io.
	Added key for overflow reset.

2000-05-01  Jesper Skov  <jskov@redhat.com>

	* include/config_keys.h: Added keys for read/write blocking.

2000-03-28  John Dallaway  <jld@cygnus.co.uk>

	* cdl/io.cdl:

	Adjust documentation URLs.

2000-03-18  Gary Thomas  <gthomas@redhat.com>

	* include/file.h: Add additional flags for nonblocking and
	async modes (used in network support).

2000-03-04  Gary Thomas  <gthomas@redhat.com>

	* include/file.h: Add function prototypes.

2000-02-17  Gary Thomas  <gthomas@cygnus.co.uk>

	* src/io_file.c: Use eCos error list <cyg/error/codes.h>.	

2000-02-15  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/io_file.c: Use standard errno.h, not sys/errno.h

2000-01-31 Simon FitzMaurice  <sdf@cygnus.co.uk>

  	* cdl/io.cdl:  Adjust help URLs in line with new doc layout.
  
2000-01-28  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/file.h: 
	* src/io_file.c: New file(s)

	* cdl/io.cdl: Add generic file I/O support.

2000-01-28 Simon FitzMaurice  <sdf@cygnus.co.uk>

  	* cdl/io.cdl:  Adjust help URLs in line with new doc layout.
  
1999-04-28  Bart Veer  <bartv@cygnus.co.uk>

	* src/PKGconf.mak (EXTRAS_COMPILE):
	Use the new rules for generating libextras.a

1999-04-15  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/iosys.c (cyg_io_set_config): Only dereference len if non-NULL
	(cyg_io_get_config): Ditto
	(cyg_io_read): Ditto
	(cyg_io_write): Ditto
	Fix for PR 19856

1999-04-12  Jesper Skov  <jskov@cygnus.co.uk>

	* src/ioinit.cxx: Use new device IO init priority.

	* src/io_diag.c:      [added]
	* include/io_diag.h:  [added]
	* src/PKGconf.mak:
	Added io_diag functionality.

1999-03-18  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/config_keys.h (CYG_IO_GET_CONFIG_SERIAL_ABORT): 
	New funtion which aborts (cancels) any pending I/O on a channel.

1999-03-15  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/pkgconf/io.h: Add 'CYGDBG_IO_INIT' for control of
	init messages.

1999-03-10  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/pkgconf/io.h: Improve CDL description.

1999-03-05  Nick Garnett  <nickg@cygnus.co.uk>

	* include/io.h:
	Changed include files used to permit non-kernel configurations to
	be built.

1999-02-25  Gary Thomas  <gthomas@cygnus.co.uk>

	* serial/current/src/common/tty.c (tty_set_config): 
	Fix problem when passing through to lower level driver.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004, 2006, 2007 Free Software Foundation, Inc.
// Copyright (C) 2004, 2006, 2007 eCosCentric Limited                       
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================