2009-05-07  Bart Veer  <bartv@ecoscentric.com>

	* include/framebuf.h, include/framebuf.inl: fix FLUSHABS() macros

2009-02-09  Bart Veer  <bartv@ecoscentric.com>

	* doc/framebuf.sgml: clarify the meaning of the true colour
	formats.

2009-02-07  John Dallaway  <john@dallaway.org.uk>

	* cdl/framebuf.cdl: Pass gen_framebufs.tcl to tclsh directly.

2009-01-08  John Dallaway  <john@dallaway.org.uk>

	* src/gen_framebufs.tcl: Specify script interpreter via /usr/bin/env.

2008-11-09  Bart Veer  <bartv@ecoscentric.com>

	* src/linear.c: fix the block move operations (new_y > y) overlap
	handling.

2008-10-06 Bart Veer  <bartv@ecoscentric.com>

	* src/gen_framebufs.tcl, cdl/framebuf.cdl, tests/*: add some
	examples/testcases.

2007-10-11  Bart Veer  <bartv@ecoscentric.com>

	* include/framebuf.h: fix 555 true colour manipulation macros.

2006-04-05  John Dallaway  <jld@ecoscentric.com>

	* cdl/framebuf.cdl: Add reference to package documentation.

2005-11-21  Bart Veer  <bartv@ecoscentric.com>

	* include/framebuf.h, src/framebuf.c: fix aliasing of the
	make/break colour functions, needed with more recent compilers.

	* doc/framebuf.sgml: fix blanking support typo

	* cdl/framebuf.cdl: run gen_framebufs.tcl slightly later
	in the build process in case other packages create framebuf header
	files at build-time.

	* src/gen_framebufs.tcl: fix typo in diagnostic.

	* src/framebuf.c (cyg_fb_synch), include/framebuf.h
	(CYG_FB_FRAMEBUFFER): fix double buffer support.

2005-06-20  John Dallaway  <jld@ecoscentric.com>

	* doc/framebuf.sgml: Fix typographical errors.

2005-03-29  Bart Veer  <bartv@ecoscentric.com>

	* Generic framebuffer package created

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2008, 2009 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================