2009-02-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/wallclock/wallclock.inl: _simple_mkdate is used by RedBoot
	and possibly others, so don't make specific to SET_GET mode.
	(Suggested by Rene Nielsen).

2009-02-04  Bart Veer  <bartv@ecoscentric.com>

	* src/wallclock.cxx: switch to CYG_INIT_DEV_WALLCLOCK init
	priority.

2008-09-09  Gary Thomas  <gary@mlbassoc.com>

	* include/wallclock/wallclock.inl (_simple_mktime): Use signed
	integers for loops (more correct if input data is invalid and
	asserts aren't on)

2008-06-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/wallclock/wallclock.inl (_simple_mktime): Add asserts to
	ensure month and day are not 0.

2007-01-14  Gary Thomas  <gary@mlbassoc.com>

	* src/wallclock.cxx: Use a mutex for exclusion during get/set
	operations as the DSR lock may not be appropriate for systems
	that need to use interrupts to accomplish these functions,
	(e.g. I2C clock devices).

2003-09-23  Dan Jakubiec <firstname.lastname@systech.com>

	* src/emulate.cxx (get_hw_seconds): Modified the ticks-to-seconds
	conversion in the wallclock emulator's get_hw_seconds() function.
	The previous implementation would easily overflow for any
	reasonable date/tick-resolution combinations.

2003-09-19  Gary Thomas  <gary@mlbassoc.com>

	* tests/wallclock.cxx: Allow test to complete, even if it looses sync.
	This is useful to determine how much drift is present.

2003-03-25  Michael Checky <Michael_Checky@Thermoking.com>

	* include/wallclock/wallclock.inl: Added parens to TO_BCD() and TO_DEC()
	macros so macro argument is interpreted correctly.

2001-07-30  Jesper Skov  <jskov@redhat.com>

	* include/wallclock/wallclock.inl (_simple_mktime): Fix assertion
	for leap seconds.

2001-07-27  Jesper Skov  <jskov@redhat.com>

	* include/wallclock/wallclock.inl (_simple_mktime): Added some assertions.
	(_simple_mktime): Adjust assertions to correct and more sensible
	values.
	(_simple_mktime): A few more assertion tweaks.

2001-06-21  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/wallclock2.cxx: No need to check for CYGINT_LIBC_STARTUP_CONTEXT
	as it is required by CYGPKG_LIBC_STARTUP.

2001-04-06  Jonathan Larmour  <jlarmour@redhat.com>

	* include/wallclock/wallclock.inl (_simple_mkdate): Fix small
	operator precedence bug.

2001-04-05  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/wallclock.cxx: Don't run this test in any simulated
	environment. It just takes far too long and is always timed out by
	the testing infrastructure.

2000-11-22  Jesper Skov  <jskov@redhat.com>

	* src/wallclock.cxx: User driver API instead of scheduler lock.

	* cdl/wallclock.cdl: Emulation requires the kernel, as do the tests. 

2000-11-09  Jesper Skov  <jskov@redhat.com>

	* tests/wallclock2.cxx: Include string header.

2000-10-20  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/wallclock2.cxx: Play better with main() startup configury

	* tests/wallclock.cxx: Ensure default priority constructors
	are called.

2000-07-24  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/wallclock2.cxx: Depend on CYGPKG_LIBC_TIME not CYGPKG_LIBC

2000-05-30  Jesper Skov  <jskov@redhat.com>

	* include/wallclock/wallclock.inl (_simple_mktime): Replaced
	expression with algorithm.

	* tests/wallclock2.cxx: Test wallclock's conversion functions for
	Y2K safety.

2000-05-26  Jesper Skov  <jskov@redhat.com>

	* include/wallclock/wallclock.inl:
	(_simple_mkdate): Rewritten.

	* src/wallclock.cxx: 
	* include/wallclock.hxx: low-level driver may need init call also
	in set-get mode. Split helper functions out in new .inl header.
	
	* cdl/wallclock.cdl: Added set-get/init-get option.

	* tests/wallclock2.cxx: Allow HW calls to take one second.
	* tests/wallclock.cxx: Don't set clock.

2000-04-19  Jesper Skov  <jskov@cygnus.co.uk>

	* src/wallclock.cxx: Construct after kernel RTC since the
	emulation implementation may have to use the RTC.

2000-04-13  Jesper Skov  <jskov@redhat.com>

	* tests/wallclock.cxx: Use TEST_NA if N/A.
	Split in two separate parts (accuracy & info).

2000-04-12  Jesper Skov  <jskov@redhat.com>

	* cdl/wallclock.cdl: Don't let interfaces define anything.

2000-04-06  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/wallclock2.cxx: Test correct libc feature CDL

2000-04-05  John Dallaway  <jld@cygnus.co.uk>

	* cdl/wallclock.cdl:

	Implement wallclock implementations as radio buttons.

2000-04-05  Jesper Skov  <jskov@redhat.com>

	* tests/wallclock.cxx: 
	Increase precision of test.
	
	* src/wallclock.cxx: 
	* src/emulate.cxx: 
	* tests/wallclock.cxx: 
	* tests/wallclock2.cxx: 

	* Moved common code, emulation device and tests to io/wallclock.

2000-04-04  Jesper Skov  <jskov@redhat.com>

	* tests/wallclock2.cxx: Include testcase.h before conditional NA.

2000-03-29  Jesper Skov  <jskov@redhat.com>

	* tests/wallclock2.cxx:
	* include/wallclock.hxx:
	* src/sh3.cxx: 
	* src/wallclock.cxx: 
	* cdl/wallclock.cdl:
	Reworked WallClock API. It should now be simpler to add new
	wallclock drivers. Added a simple test to print out the current
	wallclock value so a human can verify battery backup works.

2000-03-17  Jesper Skov  <jskov@redhat.com>

	* cdl/wallclock.cdl: 
	* src/sh3.cxx: 
	Added wallclock driver for SH3 RTC module.

2000-01-31 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/wallclock.cdl:

  Adjust help URLs in line with new doc layout.

2000-01-28 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/wallclock.cdl:

  Adjust help URLs in line with new doc layout.

2000-01-19  Hugo Tyson  <hmt@cygnus.co.uk>

	* cdl/*.cdl: Add descriptions to a number of options &c which were
	lacking same, also tidied up other typos as noticed en passant.

1999-11-03  John Dallaway  <jld@cygnus.co.uk>

	* cdl/wallclock.cdl: Define build options.

1999-07-14  Jesper Skov  <jskov@cygnus.co.uk>

	* src/emulate.cxx: Include pkgconf/kernel.h.

1999-04-20  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/wallclock.cxx (cyg_start): Output message to show the test
	has started
	(wallclock_thread): Add call to CYG_TEST_STILL_ALIVE, so the user
	can see that the test is still running.
	Fix for PR 19870

1999-04-12  John Dallaway  <jld@cygnus.co.uk>

	* include/pkgconf/wallclock.h: Add cdl_package doc attribute.

1999-04-07  Jesper Skov  <jskov@cygnus.co.uk>
        PR 19667
	* tests/wallclock.cxx (cyg_start): 
	Changed to use the new Cyg_Thread constructor.

1999-03-22  Hugo Tyson  <hmt@cygnus.co.uk>

	* tests/wallclock.cxx: 
	Use CYGNUM_HAL_STACK_SIZE_TYPICAL for the stack size instead of
	CYGNUM_HAL_MINIMUM_STACK_SIZE.

1999-03-12  Hugo Tyson  <hmt@cygnus.co.uk>

	* tests/wallclock.cxx: 
	Deal with CYGNUM_HAL_MINIMUM_STACK_SIZE requirement.


1999-03-05  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/wallclock.hxx:
	Remove dependency on cyg/kernel/ktypes.h
	Tidy

	* src/emulate.cxx:
	Include cyg/kernel/ktypes.h since it isn't included in wallclock.hxx
	any more

1999-03-04  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/pkgconf/wallclock.h: Make package stand-alone (no "DEVICES").

1999-02-02  Jesper Skov  <jskov@cygnus.co.uk>
        PR 18970
	* tests/wallclock.cxx (LOOPS_SIM): Only do two loops on
	SIM. MN10300 sim takes 1min15secs to do one loop.

1999-01-26  Jesper Skov  <jskov@cygnus.co.uk>
        (PR 18305)
	* tests/wallclock.cxx: Removed MIPS specific hackery. Now
	dependent on cyg_test_is_simulator state.

1999-01-21  Jesper Skov  <jskov@cygnus.co.uk>
        PR 18847
	* tests/wallclock.cxx (LOOPS_HW): Reduce run-time to 20 seconds.

1999-01-19  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/wallclock.cxx: Added test of cyg_test_is_simulator to
	reduce time on simulated hardware. PR 18715.

1998-12-17  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/wallclock.cxx: Do NOP test if kernel RTC disabled.

1998-10-23  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/wallclock.cxx: Reduce test time on TX39 SIM.

Tue Oct 20 15:54:09 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/PKGconf.mak: 
	Remove unnecessary override of PKGCONF_CXXFLAGS

1998-09-26  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/wallclock.h:
	PR17501: When using the emulation there is a requirement on the
	kernel clock. This has been added to the configuration data.
	If real hardware were used then this dependency would disappear,
	but currently there is no easy way to express this, and there are
	no hardware implementations.

1998-09-12  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/wallclock.h:
	Added missing descriptions (PR 17184)

1998-09-02  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/wallclock.h:
	Added minimal configuration data.

Fri Aug 28 09:40:19 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/wallclock.cxx:
	Rename int main(argc, argv) to void cyg_start( void ) under the
	new entry point system. Therefore also remove return code.
	
Tue Aug 18 16:49:20 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/wallclock.cxx: 
	Move inclusion of thread.inl before sched.hxx to prevent inline
	warnings

1998-07-31  Nick Garnett  <nickg@cygnus.co.uk>

	* include/pkgconf/wallclock.h:
	Added this file to contain wallclock confiuration parameters.
	
	* src/emulate.cxx: 
	Now uses pkgconf/wallclock.h for configuration.

Wed Jul 22 21:04:15 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/emulate.cxx: 
	Remove unnecessary include of <cyg/devs/table.h> and remove an
	unused variable (result) from get_current_time()

// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
// Copyright (C) 2008 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####