2009-03-09  John Dallaway  <john@dallaway.org.uk>

	* cdl/compress_zlib.cdl: Reference test executable filenames for
	compatibility with the eCos Configuration Tool.

2007-10-11  John Dallaway  <jld@ecoscentric.com>

	* cdl/compress_zlib.cdl: Eliminate duplicated CDL options.

2005-10-16  Peter Korsgaard  <jacmet@sunsite.dk>

	* cdl/compress_zlib.cdl (CYGFUN_COMPRESS_ZLIB_GZIO): New option to
	include zlib stdio-like utility functions.

2005-07-27  Peter Korsgaard  <jacmet@sunsite.dk>

	* src/ChangeLog: 
	* src/configure: 
	* src/deflate.c: 
	* src/deflate.h: 
	* src/FAQ: 
	* src/gzio.c: 
	* src/Make_vms.com: 
	* src/adler32.c: 
	* src/compress.c: 
	* src/example.c: 
	* src/minigzip.c: 
	* src/infback.c: 
	* src/inffast.c: 
	* src/inflate.c: 
	* src/inflate.h: 
	* src/inftrees.c: 
	* src/inftrees.h: 
	* src/Makefile: 
	* src/Makefile.in: 
	* src/README: 
	* src/README.eCos: 
	* src/trees.c: 
	* src/zlib.3: 
	* src/zutil.c: 
	* src/zutil.h: 
	* include/zlib.h: 
	* include/zconf.h: Upgrade to zlib-1.2.3

2005-06-28  Peter Korsgaard  <jacmet@sunsite.dk>

	* src/ChangeLog: 
	* src/configure: 
	* src/deflate.c: 
	* src/deflate.h: 
	* src/FAQ: 
	* src/gzio.c: 
	* src/INDEX: 
	* src/infback.c: 
	* src/inffast.c: 
	* src/inflate.c: 
	* src/Makefile: 
	* src/Makefile.in: 
	* src/README: 
	* src/trees.c: 
	* src/zlib.3: 
	* src/zutil.h: 
	* include/zlib.h: 
	* include/zconf.h: Upgrade to zlib-1.2.2

2005-03-27  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/zlib1.c: Include diag.h for diag_printf proto.

2004-05-25  Gary Thomas  <gary@mlbassoc.com>

	* src/zutil.h: Fix redefine of 'crc32'
	
	* include/zconf.h: Force define of __ECOS__ to make it easier for
	applications to use this library.  Also define Z_PREFIX to minimize
	namespace pollution.  !CYGSEM_COMPRESS_ZLIB_DEFLATE_MAKES_GZIP now
	implies NO_GZCOMPRESS and NO_GZIP.

2004-05-24  Gary Thomas  <gary@mlbassoc.com>

	* tests/zlib2.c: 
	* tests/zlib1.c: 
	* src/zutil.h: 
	* src/zutil.c: 
	* src/zlib.3: 
	* src/uncompr.c: 
	* src/trees.c: 
	* src/minigzip.c: 
	* src/inftrees.h: 
	* src/inftrees.c: 
	* src/inflate.h: 
	* src/inflate.c: 
	* src/inffixed.h:
	* src/inffast.h: 
	* src/inffast.c: 
	* src/infback.c: 
	* src/gzio.c: 
	* src/example.c: 
	* src/deflate.h: 
	* src/deflate.c: 
	* src/configure: 
	* src/compress.c: 
	* src/algorithm.txt: 
	* src/adler32.c: 
	* src/README.eCos: 
	* src/README: 
	* src/Makefile.in: 
	* src/Makefile: 
	* src/INDEX: 
	* src/FAQ: 
	* include/zlib.h: 
	* include/zconf.h: 
	* cdl/compress_zlib.cdl: Upgrade to zlib-1.2.1

2004-04-29  Oyvind Harboe <oyvind.harboe@zylin.com>
	
	* src/inffixed.h: added "const" to tables that do not 
	change in order to save RAM. Ca. 4k.

2003-11-20  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/zlib[12].c: Modified the text to the gcc3.3 friendly.

2003-11-13  Daniel Nri  <daniel.neri@sigicom.se>

        * Upgrade to zlib 1.1.4 and additional fix for inflate bug on
        machines with 16-bit pointers.

2003-09-08  Thomas Koeller  <thomas.koeller@baslerweb.com>

	* cdl/compress_zlib.cdl : Displayed package name was wrong.

2002-10-10  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/zutil.h:
	* include/zlib.h:
	* src/inflate.c (inflate): Use the CRC function from the CRC
	package.
	* src/crc32.c: Removed.

2002-09-09  Mark Salter  <msalter@redhat.com>

	* inflate.c (inflate): Fix CRC calculation over multiple invocations
	with same output buffer. 
	
2002-02-18  Jesper Skov  <jskov@redhat.com>

	* src/infblock.c: Applied fix for double-free which could cause a
	zlib crash. Fixed indentation.

2001-10-15  Gary Thomas  <gthomas@redhat.com>

	* include/zconf.h: 
	* cdl/compress_zlib.cdl: 
	Define new interface CYGINT_COMPRESS_ZLIB_LOCAL_ALLOC which allows
	users of this code (applications) to provide their own allocators.

2001-04-02  Jesper Skov  <jskov@redhat.com>

	* tests/zlib2.c: Removed BAD_CRC state.

2001-03-12  Jesper Skov  <jskov@redhat.com>

	* src/inflate.c: Remove BAD_CRC state. Do separate CRC for
	gzippped data.
	* include/zlib.h: Removed Z_BAD_CRC hack. Rename crc32 function.
	* src/crc32.c: Include zlib.h header from
	include/cyg/compress. Rename function.
	* cdl/compress_zlib.cdl: Build the crc32.c file.

2001-03-09  Jesper Skov  <jskov@redhat.com>

	* src/compress.c: Include zlib.h header from include/cyg/compress.
	* src/uncompr.c: Same.	
	* tests/zlib1.c: Added.
	* tests/zlib2.c: Added.
	* cdl/compress_zlib.cdl: Compile tests. Compile
	files holding compress/uncompress functions.

	* cdl/compress_zlib.cdl: Don't warn about prototypes when building.

2001-03-08  Jesper Skov  <jskov@redhat.com>

	* cdl/compress_zlib.cdl: Add isoinfra requirement.

	* include/zconf.h: Override STDC check.

	* include/zlib.h: Added new BAD_CRC return type. Comment out crc32
	declaration.

	* src/inflate.c: Added additional states to allow for gzip header
	decoding.
	
	* src/adler32.c: Include zlib.h header from include/cyg/compress.
	* src/zutil.h: Same.
	
	* Import zlib 1.1.3 sources, but leave out some sub
	directories. See src/README.eCos for details.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2005, 2007 eCosCentric Limited                             
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================