2005-02-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* current.ect: Provide inferred default for
	CYGBLD_ISO_STDLIB_STRCONV_FLOAT_HEADER.

2004-04-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* current.ect: Provide default for CYGBLD_ISO_STDIO_FILEOPS_HEADER
	and CYGBLD_ISO_STDIO_FILEPOS_HEADER.

2003-02-25  Andrew Lunn  <andrew.lunn@ascom.ch>

	* Added the Simple Network Time Protocol (SNTP) Client

2003-02-14  Jonathan Larmour  <jifl@eCosCentric.com>

	* Move files from templates/new_net/ to templates/net/

	* current.ect: Update inferred values.

2002-01-28  Gary Thomas  <gthomas@redhat.com>

	* current.ect: New configuration, using new FreeBSD based stack.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================