2006-10-20  Nick Garnett  <nickg@ecoscentric.com>

	* current.ect: Reduced interrupt stack to 768 bytes to give some
	expansion headroom for the HAL. Added option to set
	CYGDBG_HAL_CRCTABLE_LOCATION to ROM by default.

2006-08-21  Nick Garnett  <nickg@ecoscentric.com>

	* current.ect: Removed some unnecessary packages. Added some
	options to enable virtual vectors and minimize RAM footprint.

2003-02-14  Jonathan Larmour  <jifl@eCosCentric.com>

	* current.ect: Update inferred values.

2002-03-13  Jesper Skov  <jskov@redhat.com>

	* current.ect: Fix _GDB_STUBS option name.

2000-11-03  Jonathan Larmour  <jlarmour@redhat.com>

	* current.ect: Add inferred values for CDL that confuses the
	config tool inference engine at present.

2000-07-20  Nick Garnett  <nickg@cygnus.co.uk>

	* current.ect: Added ISOINFRA package.

2000-04-07  Hugo Tyson  <hmt@cygnus.co.uk>

	* ecos.db: Re-organize device packages.  This is a massive change
	involving deleting all the sources for serial and ethernet drivers
	from where they used to live in
	    packages/io/serial/current/src/ARCH/PLATFORM.[ch]
	    packages/net/drivers/eth/PLATFORM/current/src/...
	and reinstating them in
	    packages/devs/serial/ARCH/PLATFORM/current/src/...
	    packages/devs/eth/ARCH/PLATFORM/current/src/...

	All these new packages are properly defined in ecos.db, and are
	all of type "hardware" so that a "target" can grab them.
	
	This directory layout is descriptive of the devices we have right
	now, arch and platform are separate levels just to make it easier
	to navigate in the filesystem and similar to the HAL structure in
	the filesystem.

	It is *not* prescriptive of future work; for example, the mythical
	common highly-portable 16550 serial driver which works on many
	targets would be called "devs/serial/s16550/current", or a serial
	device for a particular board (cogent springs to mind) that can
	work with different CPUs fitted is "devs/serial/cogent/current".

	Changelogs have been preserved and replicated over all the new
	packages, so that no history is lost.

	The contents of individual source files are unchanged; they build
	in just the same emvironment except for a very few cases where the
	config file name changed in this movement.

	Targets in ecos.db have been redefined to bring in all relevant
	hardware packages including net and serial drivers (but the newly
	included packages are only active if their desired parent is
	available.)
	
	The names of CDL options (and their #defines of course) stay the
	same for the serial drivers, for backward compatibility.

	* templates/*/current.ect: these have had CYGPKG_IO_SERIAL added
	rather than it being in (almost) all target definitions.
	
2000-02-18  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* current.ect: Shrink template so that it only enables a single option
	in the platform HAL, and it's completely up to the platform HAL to
	define the dependencies. This makes things more generic.

2000-02-15  Jesper Skov  <jskov@redhat.com>

	* current.ect: All targets use this template now.

2000-01-27  Jesper Skov  <jskov@redhat.com>

	* current.ect: AEB uses this now.

2000-01-26  Jesper Skov  <jskov@redhat.com>

	* current.ect: Added list of supportred targets.

2000-01-21  Jesper Skov  <jskov@cygnus.co.uk>

	* current.ect: Add description. Change to ROM startup. Set
	ROM_MONITOR option.

2000-01-20  Jesper Skov <jskov@cygnus.co.uk>

	* templates/stubs directory created
	

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2006 Free Software Foundation, Inc.
// Copyright (C) 2006 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================