0.2-Alpha
---------
Added the Ball 94 Instrumenting Algorithm.
I think it is probably better to use this
then the StateMachine.  (It is much slower
to get statistics.)

Also, have a prototype application JIPS,
which provides real-time instructions per
second.  (May not work right now.)

Build system has been moved to Jakarta
Maven (http://jakarta.apache.com/turbine/maven)

Some changes to the Ant task.  Should be
done pretty soon.

0.1.01-Alpha
------------
Fixed problem with instrumenting Loops.


0.1-Alpha
----------
Initial Version
State Machine coverage implemented
XMLSummary, XMLReport and TreeReport available.
Text UI and Ant task available.