View Javadoc
1 /*** 2 * SelectEdge 3 * 4 * This represents an edge that 5 * results from a switch statement. 6 */ 7 8 package junit.quilt.cover.generic; 9 10 import junit.quilt.exception.InvalidTransitionException; 11 import org.apache.bcel.generic.*; 12 13 public class SelectEdge 14 extends FlowControlEdge 15 { 16 private String expr = null; 17 private int value = -1; 18 19 private boolean isDefault = false; 20 21 public SelectEdge( BlockVertex source, 22 BlockVertex target, 23 String expr, 24 int value ) 25 { 26 super( source, target ); 27 this.isDefault = false; 28 this.expr = expr; 29 this.value = value; 30 } 31 32 public SelectEdge( BlockVertex source, 33 BlockVertex target, 34 String expr ) 35 { 36 super( source, target ); 37 this.isDefault = true; 38 this.expr = expr; 39 } 40 41 public void connect( MethodGen method, 42 InstructionList il, 43 InstructionHandle source, 44 InstructionHandle target ) 45 throws InvalidTransitionException 46 { 47 if (source.getInstruction() instanceof Select) { 48 Select select = 49 (Select) source.getInstruction(); 50 51 if (isDefault) { 52 select.setTarget( target ); 53 } else { 54 int matches[] = select.getMatchs(); 55 for (int i = 0; i < matches.length; i++) { 56 if (matches[i] == value) { 57 select.setTarget( i, target ); 58 } 59 } 60 } 61 } else { 62 throw new InvalidTransitionException("Select expected"); 63 } 64 } 65 66 67 public String toString() { 68 String RC = "[S: "; 69 if (isDefault) { 70 RC = RC + getTarget(); 71 } else { 72 RC = RC + expr + "=" + value + " -> " + getTarget(); 73 } 74 RC = RC + "]"; 75 return RC; 76 } 77 } 78 79 80 81

This page was automatically generated by Maven