#
# General architecture dependent options
#

config KPROBES
	bool "Kprobes"
	depends on KALLSYMS && MODULES
	depends on HAVE_KPROBES
	help
	  Kprobes allows you to trap at almost any kernel address and
	  execute a callback function.  register_kprobe() establishes
	  a probepoint and specifies the callback.  Kprobes is useful
	  for kernel debugging, non-intrusive instrumentation and testing.
	  If in doubt, say "N".

config HAVE_EFFICIENT_UNALIGNED_ACCESS
	bool
	help
	  Some architectures are unable to perform unaligned accesses
	  without the use of get_unaligned/put_unaligned. Others are
	  unable to perform such accesses efficiently (e.g. trap on
	  unaligned access and require fixing it up in the exception
	  handler.)

	  This symbol should be selected by an architecture if it can
	  perform unaligned accesses efficiently to allow different
	  code paths to be selected for these cases. Some network
	  drivers, for example, could opt to not fix up alignment
	  problems with received packets if doing so would not help
	  much.

	  See Documentation/unaligned-memory-access.txt for more
	  information on the topic of unaligned memory accesses.

config HAVE_SYSCALL_WRAPPERS
	bool

config KRETPROBES
	def_bool y
	depends on KPROBES && HAVE_KRETPROBES

config HAVE_IOREMAP_PROT
	bool

config HAVE_KPROBES
	bool

config HAVE_KRETPROBES
	bool

#
# An arch should select this if it provides all these things:
#
#	task_pt_regs()		in asm/processor.h or asm/ptrace.h
#	arch_has_single_step()	if there is hardware single-step support
#	arch_has_block_step()	if there is hardware block-step support
#	asm/syscall.h		supplying asm-generic/syscall.h interface
#	linux/regset.h		user_regset interfaces
#	CORE_DUMP_USE_REGSET	#define'd in linux/elf.h
#	TIF_SYSCALL_TRACE	calls tracehook_report_syscall_{entry,exit}
#	TIF_NOTIFY_RESUME	calls tracehook_notify_resume()
#	signal delivery		calls tracehook_signal_handler()
#
config HAVE_ARCH_TRACEHOOK
	bool

config HAVE_DMA_ATTRS
	bool

config USE_GENERIC_SMP_HELPERS
	bool

config HAVE_CLK
	bool
	help
	  The <linux/clk.h> calls support software clock gating and
	  thus are a key power management tool on many systems.

config HAVE_DMA_API_DEBUG
	bool

config HAVE_DEFAULT_NO_SPIN_MUTEXES
	bool

source "kernel/gcov/Kconfig"