#
# Input misc drivers configuration
#
menuconfig INPUT_MISC
	bool "Miscellaneous devices"
	help
	  Say Y here, and a list of miscellaneous input drivers will be displayed.
	  Everything that didn't fit into the other categories is here. This option
	  doesn't affect the kernel.

	  If unsure, say Y.

if INPUT_MISC

config INPUT_PCSPKR
	tristate "PC Speaker support"
	depends on PCSPKR_PLATFORM
	help
	  Say Y here if you want the standard PC Speaker to be used for
	  bells and whistles.

	  If unsure, say Y.

	  To compile this driver as a module, choose M here: the
	  module will be called pcspkr.

config INPUT_SPARCSPKR
	tristate "SPARC Speaker support"
	depends on PCI && SPARC64
	help
	  Say Y here if you want the standard Speaker on Sparc PCI systems
	  to be used for bells and whistles.

	  If unsure, say Y.

	  To compile this driver as a module, choose M here: the
	  module will be called sparcspkr.

config INPUT_M68K_BEEP
	tristate "M68k Beeper support"
	depends on M68K

config INPUT_APANEL
	tristate "Fujitsu Lifebook Application Panel buttons"
	depends on X86 && I2C && LEDS_CLASS
	select INPUT_POLLDEV
	select CHECK_SIGNATURE
	help
	 Say Y here for support of the Application Panel buttons, used on
	 Fujitsu Lifebook. These are attached to the mainboard through
	 an SMBus interface managed by the I2C Intel ICH (i801) driver,
	 which you should also build for this kernel.

	 To compile this driver as a module, choose M here: the module will
	 be called apanel.

config INPUT_IXP4XX_BEEPER
	tristate "IXP4XX Beeper support"
	depends on ARCH_IXP4XX
	help
	  If you say yes here, you can connect a beeper to the
	  ixp4xx gpio pins. This is used by the LinkSys NSLU2.

	  If unsure, say Y.

	  To compile this driver as a module, choose M here: the
	  module will be called ixp4xx-beeper.

config INPUT_COBALT_BTNS
	tristate "Cobalt button interface"
	depends on MIPS_COBALT
	select INPUT_POLLDEV
	help
	  Say Y here if you want to support MIPS Cobalt button interface.

	  To compile this driver as a module, choose M here: the
	  module will be called cobalt_btns.

config INPUT_WISTRON_BTNS
	tristate "x86 Wistron laptop button interface"
	depends on X86 && !X86_64
	select INPUT_POLLDEV
	select NEW_LEDS
	select LEDS_CLASS
	select CHECK_SIGNATURE
	help
	  Say Y here for support of Wistron laptop button interfaces, used on
	  laptops of various brands, including Acer and Fujitsu-Siemens. If
	  available, mail and wifi LEDs will be controllable via /sys/class/leds.

	  To compile this driver as a module, choose M here: the module will
	  be called wistron_btns.

config INPUT_ATLAS_BTNS
	tristate "x86 Atlas button interface"
	depends on X86 && ACPI
	help
	  Say Y here for support of Atlas wallmount touchscreen buttons.
	  The events will show up as scancodes F1 through F9 via evdev.

	  To compile this driver as a module, choose M here: the module will
	  be called atlas_btns.

config INPUT_ATI_REMOTE
	tristate "ATI / X10 USB RF remote control"
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to use an ATI or X10 "Lola" USB remote control.
	  These are RF remotes with USB receivers.
	  The ATI remote comes with many of ATI's All-In-Wonder video cards.
	  The X10 "Lola" remote is available at:
	     <http://www.x10.com/products/lola_sg1.htm>
	  This driver provides mouse pointer, left and right mouse buttons,
	  and maps all the other remote buttons to keypress events.

	  To compile this driver as a module, choose M here: the module will be
	  called ati_remote.

config INPUT_ATI_REMOTE2
	tristate "ATI / Philips USB RF remote control"
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to use an ATI or Philips USB RF remote control.
	  These are RF remotes with USB receivers.
	  ATI Remote Wonder II comes with some ATI's All-In-Wonder video cards
	  and is also available as a separate product.
	  This driver provides mouse pointer, left and right mouse buttons,
	  and maps all the other remote buttons to keypress events.

	  To compile this driver as a module, choose M here: the module will be
	  called ati_remote2.

config INPUT_KEYSPAN_REMOTE
	tristate "Keyspan DMR USB remote control (EXPERIMENTAL)"
	depends on EXPERIMENTAL
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to use a Keyspan DMR USB remote control.
	  Currently only the UIA-11 type of receiver has been tested.  The tag
	  on the receiver that connects to the USB port should have a P/N that
	  will tell you what type of DMR you have.  The UIA-10 type is not
	  supported at this time.  This driver maps all buttons to keypress
	  events.

	  To compile this driver as a module, choose M here: the module will
	  be called keyspan_remote.

config INPUT_POWERMATE
	tristate "Griffin PowerMate and Contour Jog support"
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to use Griffin PowerMate or Contour Jog devices.
	  These are aluminum dials which can measure clockwise and anticlockwise
	  rotation.  The dial also acts as a pushbutton.  The base contains an LED
	  which can be instructed to pulse or to switch to a particular intensity.

	  You can download userspace tools from
	  <http://sowerbutts.com/powermate/>.

	  To compile this driver as a module, choose M here: the
	  module will be called powermate.

config INPUT_YEALINK
	tristate "Yealink usb-p1k voip phone"
	depends on EXPERIMENTAL
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to enable keyboard and LCD functions of the
	  Yealink usb-p1k usb phones. The audio part is enabled by the generic
	  usb sound driver, so you might want to enable that as well.

	  For information about how to use these additional functions, see
	  <file:Documentation/input/yealink.txt>.

	  To compile this driver as a module, choose M here: the module will be
	  called yealink.

config INPUT_CM109
	tristate "C-Media CM109 USB I/O Controller"
	depends on EXPERIMENTAL
	depends on USB_ARCH_HAS_HCD
	select USB
	help
	  Say Y here if you want to enable keyboard and buzzer functions of the
	  C-Media CM109 usb phones. The audio part is enabled by the generic
	  usb sound driver, so you might want to enable that as well.

	  To compile this driver as a module, choose M here: the module will be
	  called cm109.

config INPUT_TWL4030_PWRBUTTON
	tristate "TWL4030 Power button Driver"
	depends on TWL4030_CORE
	help
	  Say Y here if you want to enable power key reporting via the
	  TWL4030 family of chips.

	  To compile this driver as a module, choose M here. The module will
	  be called twl4030_pwrbutton.

config INPUT_UINPUT
	tristate "User level driver support"
	help
	  Say Y here if you want to support user level drivers for input
	  subsystem accessible under char device 10:223 - /dev/input/uinput.

	  To compile this driver as a module, choose M here: the
	  module will be called uinput.

config INPUT_SGI_BTNS
	tristate "SGI Indy/O2 volume button interface"
	depends on SGI_IP22 || SGI_IP32
	select INPUT_POLLDEV
	help
	  Say Y here if you want to support SGI Indy/O2 volume button interface.

	  To compile this driver as a module, choose M here: the
	  module will be called sgi_btns.

config INPUT_WINBOND_CIR
	tristate "Winbond IR remote control"
	depends on X86 && PNP
	select NEW_LEDS
	select LEDS_CLASS
	select LEDS_TRIGGERS
	select BITREVERSE
	help
	  Say Y here if you want to use the IR remote functionality found
	  in some Winbond SuperI/O chips. Currently only the WPCD376I
	  chip is supported (included in some Intel Media series motherboards).

	  IR Receive and wake-on-IR from suspend and power-off is currently
	  supported.

	  To compile this driver as a module, choose M here: the module will be
	  called winbond_cir.

config HP_SDC_RTC
	tristate "HP SDC Real Time Clock"
	depends on (GSC || HP300) && SERIO
	select HP_SDC
	help
	  Say Y here if you want to support the built-in real time clock
	  of the HP SDC controller.

config INPUT_PCF50633_PMU
	tristate "PCF50633 PMU events"
	depends on MFD_PCF50633
	help
	 Say Y to include support for delivering  PMU events via  input
	 layer on NXP PCF50633.

config INPUT_GPIO_ROTARY_ENCODER
	tristate "Rotary encoders connected to GPIO pins"
	depends on GPIOLIB && GENERIC_GPIO
	help
	  Say Y here to add support for rotary encoders connected to GPIO lines.
	  Check file:Documentation/input/rotary-encoder.txt for more
	  information.

	  To compile this driver as a module, choose M here: the
	  module will be called rotary_encoder.

config INPUT_RB532_BUTTON
	tristate "Mikrotik Routerboard 532 button interface"
	depends on MIKROTIK_RB532
	depends on GPIOLIB && GENERIC_GPIO
	select INPUT_POLLDEV
	help
	  Say Y here if you want support for the S1 button built into
	  Mikrotik's Routerboard 532.

	  To compile this driver as a module, choose M here: the
	  module will be called rb532_button.

config INPUT_DM355EVM
	tristate "TI DaVinci DM355 EVM Keypad and IR Remote"
	depends on MFD_DM355EVM_MSP
	help
	  Supports the pushbuttons and IR remote used with
	  the DM355 EVM board.

	  To compile this driver as a module, choose M here: the
	  module will be called dm355evm_keys.

config INPUT_BFIN_ROTARY
	tristate "Blackfin Rotary support"
	depends on BF54x || BF52x
	help
	  Say Y here if you want to use the Blackfin Rotary.

	  To compile this driver as a module, choose M here: the
	  module will be called bfin-rotary.

config INPUT_WM831X_ON
	tristate "WM831X ON pin"
	depends on MFD_WM831X
	help
	  Support the ON pin of WM831X PMICs as an input device
	  reporting power button status.

	  To compile this driver as a module, choose M here: the module
	  will be called wm831x_on.

config INPUT_PCAP
	tristate "Motorola EZX PCAP misc input events"
	depends on EZX_PCAP
	help
	  Say Y here if you want to use Power key and Headphone button
	  on Motorola EZX phones.

	  To compile this driver as a module, choose M here: the
	  module will be called pcap_keys.

config INPUT_TM1668
	tristate "TM1668 LED/Keyboard controller"
	help
	  Say Y here if you want to enable driver for keyboard and LED
	  display controlled by GPIO-connected TM1668 chip. Note that
	  a related platform device must be defined in the board setup.

	  To compile this driver as a module, choose M here: the
	  module will be called tm1668.

endif