config STMMAC_ETH
	tristate "STMicroelectronics 10/100/1000 Ethernet driver"
	select MII
	select PHYLIB
	select CRC32
	depends on NETDEVICES
	help
	  This is the driver for the Ethernet IPs are built around a
	  Synopsys IP Core and only tested on the STMicroelectronics
	  platforms.

if STMMAC_ETH

config STMMAC_DA
	bool "STMMAC DMA arbitration scheme"
	default n
	help
	  Selecting this option, rx has priority over Tx (only for Giga
	  Ethernet device).
	  By default, the DMA arbitration scheme is based on Round-robin
	  (rx:tx priority is 1:1).

config STMMAC_TIMER
	bool "STMMAC Timer optimisation"
	default n
	help
	  Use an external timer for mitigating the number of network
	  interrupts. Currently, for SH architectures, it is possible
	  to use the TMU channel 2 and the SH-RTC device.

choice
        prompt "Select Timer device"
        depends on STMMAC_TIMER

config STMMAC_TMU_TIMER
        bool "TMU channel 2"
        depends on CPU_SH4
	help

config STMMAC_RTC_TIMER
        bool "Real time clock"
        depends on RTC_CLASS
	help

endchoice

endif