#
# STM specific device configuration
#

config STM_DRIVERS
	boolean
	default y if CPU_SUBTYPE_ST40
	default n

menu "STM specific devices"
        depends on STM_DRIVERS

config STM_MIPHY
	def_bool y
	depends on SATA_STM

config STM_MIPHY_TAP
	bool
	depends on STM_MIPHY
	default y if CPU_SUBTYPE_STX7105
	default y if CPU_SUBTYPE_STX7108
	default y if CPU_SUBTYPE_STX7141
	default y if CPU_SUBTYPE_STX7200
	default n

config STM_MIPHY_PCIE_MP
	bool
	depends on STM_MIPHY
	default y if CPU_SUBTYPE_STX7108
	default n

config STM_MIPHY_DUMMY
	bool
	depends on STM_MIPHY
	default y if CPU_SUBTYPE_STX7100
	default n

config STPIO
	bool "Legacy stpio API"
	default n
	help
	  Select this option to enable the legacy stpio interface. No
	  code within the kernel uses this API, it is retained only for
	  drivers outside the kernel which might still need it.

config STM_DMA
	bool "STMicroelectronics DMA API"
	select SH_DMA_API
	select LIBELF
	default y
	---help---
	  Selecting this option will provide support for STMicroelectronics'
	  custom DMA API. This API provides support for data transfers of
	  various dimensions and complex linked list operations. In addition
	  to these free-running operations it also allows management of the
	  paced-transfer peripherals on recent STM parts.

	  If you have a device from STMicroelectronics, then say Y here.
	  Otherwise say N.

config STM_DMA_DEBUG
	bool "STMicroelectronics DMA Debug"
	depends on STM_DMA
	default n

config STM_COPROCESSOR_SUPPORT
	bool "STMicroelectronics coprocessor support"
	default y
	depends on (CPU_SUBTYPE_STX7100 || CPU_SUBTYPE_STX7105 \
		|| CPU_SUBTYPE_STX7111 || CPU_SUBTYPE_STX7141 \
		|| CPU_SUBTYPE_STX7200 || CPU_SUBTYPE_STX7108 \
		|| CPU_SUBTYPE_STX5206)
	---help---
        Many of the ST system-on-chip devices have multiple CPUs, where a
        master CPU running Linux has control over a number of slave CPUs,
        which are usually used to run dedicated algorithms.
        Enabling this option will add support to the Linux kernel to
        control these slave CPUs, reserve memory for them, and thus allow
        code to be downloaded onto them and executed.
        Adding in the command line the following string:
        coprocessor_mem=[offset]:size0[,size1][,size2]...
        where:
        offset defines where the co-processors region starts.
               It's an offset from ST40 RAM start.
        size{n} defines the region size for the n.th slave core (max 16M).

        Example: coprocessor_mem=32m:16m,16m

config STM_NUM_COPROCESSOR
	int
	depends on STM_COPROCESSOR_SUPPORT
	default 2 if CPU_SUBTYPE_STX7100
	default 2 if CPU_SUBTYPE_STX7105
	default 2 if CPU_SUBTYPE_STX7111
	default 2 if CPU_SUBTYPE_STX7141
	default 2 if CPU_SUBTYPE_STX5206
	default 4 if CPU_SUBTYPE_STX7200
	default 3 if CPU_SUBTYPE_STX7108
	default 0

choice
	prompt "STM coprocessor loading strategy"
        depends on STM_COPROCESSOR_SUPPORT
        default STM_COPROCESSOR

config  STM_COPROCESSOR
	bool "STM coprocessor support"
	help
	  Select this option to enable support for the slave coprocessors
	  found on many ST system-on-chip devices.

config  STM_COPROCESSOR_FRMW
	bool "The new STM coprocessor firmware support "
	select FW_LOADER
	help
	  Select this option to enable support for the slave coprocessors
	  found on many ST system-on-chip devices.

endchoice

config  COPROCESSOR_DEBUG
        depends on STM_COPROCESSOR_SUPPORT
        bool "STM coprocessor debug"
        default n
        ---help---
        Enable this option to print out information about the slave CPUs
        addresses and operations you are using for coprocessor.

config STM_RNG
       bool "STM Random Number Generator Support"
       default y
       ---help---
         This option adds support for the hardware Random Number Generator
         (RNG) present on different STMicroelectronics SoCs.  It allows the
         RNG to feed /dev/random with entropy thereby ensuring real
         random numbers from this device.

         Without this option, /dev/random has little entropy and is not
         useful.  In fact, it may block for a long time while waiting for
         entropy.

         This option should always be enabled for relevant SoCs.

         This option can be used in conjunction with the /dev/hw_random
         driver found in the char drivers menu.

config STM_MALI
	depends on CPU_SUBTYPE_STX7108
	tristate "STM Mali GPU support"
	default n
	help
	  Enable this option to support Mali GPU Driver.

config PMS
	bool "Power Management Scheme"
	default n
	depends on PM
	select PM_RUNTIME
	help
	  This option enables the STMicroelectronics Power Management
	  Scheme (PMS).

	  This is a kernel framework based around power profiles (pms_state),
	  where the designer can specify devices power states and the
	  clock frequency rates.
	  Moving the system between pms_states the user application can
	  tune the power consumption according with what the system is doing.

config PMS_CHECK_GROUP
	bool "PMS always checks the state group"
	depends on PMS
	default n
	help
	  Enable this option if the state group has to be controlled.
	  When a group of pms_states are enabled in the same time, this option
	  forces the PMS to check that there is no conflict inside the group
	  itself. In case of conflict the group is rejected.

config PMS_DEBUG
	bool "PMS debug"
	default n
	depends on PMS
	help
	  Enable this option to print out information about the PMS

endmenu